keyence

Case Studies: Create A Fully Automated Process



Background:

For several years this particular company has been using a semi-automated process for their product assembly. An internal goal was move towards a fully automated process to speed up production, eliminate errors, and reduce the amount of human inspection. Blood Analysis

The Problem:

Each medical cartridge in the nest must contain only one bead of blood. What was happening is the cartridge would get by with no bead in it or more than one. All of these beads are forced down a tube by air.

Due to the speed at which the bead moving, it was often missed. In other situations the sensor would detect a bead but not recognize that there is more than one in the slot.

In order to help prevent this several operators would have to inspect these 100+ stations to help catch these errors. This was a very costly procedure and due to human error often-improper cartridges got by.

The Solution:

The KEYENCE FS-V30 series solved the problem.

By using this in high-speed mode with 33us response time they were able to detect almost 100% of the beads coming by. The speed was no longer an issue in detecting the bead.

Secondly, they were able to utilize the dual output model to detect double fed beads. Writing a simple PLC program allowed them to detect the bead, and determine if it was double fed

The Results:

The FS-V30 series solved all three of their issues. They now run a fully automated process. Production speed has increased with the sensor ability to detect the air forced bead. Operators are now able to spend their time on other areas of the process. Since the first system has been completed a second system is in the process of being built. Finally, other old stations have been retro-fitted to run on this new setup.



The FS-V30 series has been further improved upon with the New FS-neo series.
Download the catalog below.

 
  Request Now!
Digital Fiberoptic Sensor (32 pages)
 
 

     

Please send us your questions and a Keyence Salesperson will get back to you.
To complete your request, FIRST fill in the information below and then the form at the bottom.


   
 Please describe your application problem below.(required)
 What is your detect / measurement target?
 Detection / measurement type.(Choose one from the list below)
 Please check the item(s) you are interested in.




 Material:(optional)
Ex: Steel, plastic, rubber, etc.
 Accuracy:(optional)
Ex: High, Repeatabilitly
 Speed:(optional)
Ex: Char/sec, cycles, etc.
 output Type:(optional)
Ex: Digital, analog, etc.
 Optional Questions
 
Are you using a similar product(s)?

 
Any plans to purchase this product(s)?

 
Any questions about the product(s)?
 
How did you find us?
 
Notes:
[1] Your request has to be forwarded to the correct Keyence affiliate company or distributor responsible for your country / area. The question will then be given to the responsible engineer. Please be patient, we will try to respond to each and every request as soon as we can, however the response may not be immediate.

[2] Questions will be answered by a Keyence staff member if you live in the following areas : U.S.A, United Kingdom, Germany, France, Japan, Singapore, Malaysia, Thailand & Taiwan. If you are outside of these areas your question may be forwarded to a Keyence distributor.


To sign up please enable Javascript

topics_gry_JSNG

CE-Marking  |   Discontinued Products  |   Privacy  |   Terms and Conditions  |   Terms of Use  |   Purchasing Activity  |   Newsletter  |   Sitemap

Copyright (C) 2012 Keyence Corporation. All Rights Reserved.