keyence

Case Studies: Save $100K



Background:

A metal products manufacturer supplies a full line of product to thousands of customers worldwide. Thousands of these parts are manufactured on a daily basis at each plant across the United States.

There are multiple processes to produce each part. During the first process, the customer needs to control the thickness of powdered metallic material applied to a metal substrate. At some point during the process, an operator would use a contact caliper to measure the thickness of metal and coating. Each time a thickness problem was detected, the operator would adjust the rollers and then measure again until the optimum thickness was achieved.

The Problem:

The customer could not stop the line due to the sintering process or the time needed to cure in the oven. Due to the time interval in between the measurements, sometimes good product had to be thrown out along with the bad, costing production time and money. Calipers could potentially damage the product and the readings were inconsistent from shift to shift.

The Solution:

After consulting the customer, KEYENCE proposed the non-contact dual head LK-G32 as a solution due to its enhanced performance on specular and irregularly shaped/colored targets, including reliable measurement of metals. The customer designed a fixture to hold the LK-G units in place on the production line. Once set into place, the tolerance is simply programmed into the LKG unit. When the measurement rises above or falls below the tolerance, the screen turns red and a buzzer sounds to inform the operator that an adjustment to the rollers needs to be made. The LKG made it much easier for the operator to know when they had the correct thickness dialed in on the rollers, due its ability to continuously take dynamic measurements, and provide constant feedback. The customer still needs to conduct destructive testing, however the amount of material that actually needs to be discarded is minimal.

The Results:

The high-accuracy and repeatability of the dual head LK-G32 on the metal proved to be successful.

The customer liked the solution primarily because it allowed them to sample continuously on their products. They were no longer stopping production to perform a measurement. More importantly, the KEYENCE solution has saved them from disposing of over $100k worth of unusable product. They are now running a higher percentage of quality material with a much lower ratio of scrap.

  Request Now!
CCD Laser Displacement Sensor Selection Guide (22 pages).
 

     

Please send us your questions and a Keyence Salesperson will get back to you.
To complete your request, FIRST fill in the information below and then the form at the bottom.


   
 Please describe your application problem below.(required)
 What is your detect / measurement target?
 Detection / measurement type.(Choose one from the list below)
 Please check the item(s) you are interested in.




 Material:(optional)
Ex: Steel, plastic, rubber, etc.
 Accuracy:(optional)
Ex: High, Repeatabilitly
 Speed:(optional)
Ex: Char/sec, cycles, etc.
 output Type:(optional)
Ex: Digital, analog, etc.
 Optional Questions
 
Are you using a similar product(s)?

 
Any plans to purchase this product(s)?

 
Any questions about the product(s)?
 
How did you find us?
 
Notes:
[1] Your request has to be forwarded to the correct Keyence affiliate company or distributor responsible for your country / area. The question will then be given to the responsible engineer. Please be patient, we will try to respond to each and every request as soon as we can, however the response may not be immediate.

[2] Questions will be answered by a Keyence staff member if you live in the following areas : U.S.A, United Kingdom, Germany, France, Japan, Singapore, Malaysia, Thailand & Taiwan. If you are outside of these areas your question may be forwarded to a Keyence distributor.


To sign up please enable Javascript

topics_gry_JSNG

CE-Marking  |   Discontinued Products  |   Privacy  |   Terms and Conditions  |   Terms of Use  |   Purchasing Activity  |   Newsletter  |   Sitemap

Copyright (C) 2012 Keyence Corporation. All Rights Reserved.