keyence

CASE STUDIES: Eliminate Waste


New CMOS Sensor Eliminate Downtime and Waste on Production Lines

Background:

A printing company manufactures various types of materials for the gaming industry and distributes these games to a worldwide audience. This customer prints dozens of different types of cards, and deals with thousands of different colors and finishes on their printed materials.

The Problem:

The customer runs a continuous web of material through their printing presses and would like to run uninterrupted for a full 24 hours per day of manufacturing time. Ideally, the only downtime they expect is a manual change of rolled material when the previous roll is exhausted.

They needed a sensor that could constantly detect presence of the material running through the press without any failures.

To make matters more difficult, they could only use a one-sided sensor and could not mount any type of sensing element underneath the web of material. Due to the variety of color and finish on their printed materials, conventional diffuse and reflective sensors had consistently failed.

Furthermore, to avoid potential mechanical damage to the sensor it would need to be located at least four inches away from the web. This eliminated other detection options that could only operate within very close proximity to the printed material. Failure of all existing sensor options had caused thousands of dollars in damaged product due to false rejects and improperly spliced material.

They were also forced to employ an operator to oversee this line in the hopes of manually preventing damaged material, adding tremendous labor cost to their operation.

The Solution:

This customer’s local KEYENCE partner was aware of the previous problems with conventional reflective sensors and proposed the GV-H130 upon its release. The GV had the unique ability to detect the printed material based on the location rather than the surface color or finish. Pairing this aspect with its long-range sensing distance, the GV looked to be a perfect solution for the problem. The customer now had a “set it and forget it” approach to the sensing of their material and could eliminate damaged material as well as operator oversight on their lines.

The Results:

The customer initially purchased two sets of the KEYENCE GV-H130 for further testing in their facility. The primary test runs indicated that the sensor solved their issue and would allow them to eliminate downtime and waste on their production lines.

They have since purchased and implemented this solution on 18 lines across two different manufacturing facilities. They have drastically decreased their scrap rates and have been able to eliminate damaged product due to sensor failure.

Most importantly, the customer has been able to deploy the line operator to another part of the facility where their services were in more demand and reduced labor cost of the line as a result.
 

 

 

Please send us your questions and a Keyence Salesperson will get back to you.
To complete your request, FIRST fill in the information below and then the form at the bottom.


   
 Please describe your application problem below.(required)
 What is your detect / measurement target?
 Detection / measurement type.(Choose one from the list below)
 Please check the item(s) you are interested in.




 Material:(optional)
Ex: Steel, plastic, rubber, etc.
 Accuracy:(optional)
Ex: High, Repeatabilitly
 Speed:(optional)
Ex: Char/sec, cycles, etc.
 output Type:(optional)
Ex: Digital, analog, etc.
 Optional Questions
 
Are you using a similar product(s)?

 
Any plans to purchase this product(s)?

 
Any questions about the product(s)?
 
How did you find us?
 
Notes:
[1] Your request has to be forwarded to the correct Keyence affiliate company or distributor responsible for your country / area. The question will then be given to the responsible engineer. Please be patient, we will try to respond to each and every request as soon as we can, however the response may not be immediate.

[2] Questions will be answered by a Keyence staff member if you live in the following areas : U.S.A, United Kingdom, Germany, France, Japan, Singapore, Malaysia, Thailand & Taiwan. If you are outside of these areas your question may be forwarded to a Keyence distributor.


To sign up please enable Javascript

topics_gry_JSNG

CE-Marking  |   Discontinued Products  |   Privacy  |   Terms and Conditions  |   Terms of Use  |   Purchasing Activity  |   Newsletter  |   Sitemap

Copyright (C) 2012 Keyence Corporation. All Rights Reserved.