1. Home
  2. KEYENCE TV

KEYENCE TV

CV-X Series Camera Replication Function


Navigation to easily correct camera position, brightness and focus

The Camera Replication function of the CV-X Series can be used to easily guide the user to fix the vision camera position, brightness and focus back to the original stored condition if the camera gets bumped or moved. It compares the stored image to the current image condition. This can also be used to duplicate the same image conditions from one camera to another on duplicate production lines.

Download the catalog for more information: