Lenses (for Machine Vision)

CA-L series

LENS Selection Guide

Fixed focal length lens CA-LHR CA-LHE CA-LH CA-LHW CV-L

Macro lens CA-LMHR CA-LMHE CA-LM CA-LM CA-LM CA-LHW/CA-LHL/CA-LM Series

Camera model interaction chart
• The roundness of the lens series icons in the charts is a simple expression of the amount of TV distortion.
• WD indicates working distance when each lens is used at reference magnification, so the WD will be changed when magnification is adjusted.
• Select a lens whose resolution and image circle specifications exceed those of the camera. In more detail, select a lens whose supported image circle is larger than the image circle of the camera. Select a lens whose resolution is higher than the unit cell size of the camera.

VISION LIBRARY

  • General Catalog Request
  • Trade Shows and Exhibitions
  • eNews Subscribe

More Series In Vision Systems

Types In Vision / Auto ID

Vision / Auto ID