Ultra High-Speed, Multi-Camera, High-Performance Image Processing System

XG-8000 series

  • Ultra High-Speed, Multi-Camera, High-Performance Image Processing System

Ultra High-Speed, Multi-Camera, High-Performance Image Processing System

An image processing system with the ultimate camera selection

The XG-8000L Series is a highly flexible image processing system that has features to make line scan camera set up quick and easy

Supports line scan cameras

The interchangeable camera module type controller makes it easy to incorporate a line scan camera system that traditionally could only be done with complex, specialized machinery.

XG LINE SCAN SYSTEM

XG Series features

• Compatibility issues are eliminated since all the hardware is from the same manufacturer
• Simple connection of the camera to the controller allowing the user to obtain images quickly
• Robust solid state hardware design
• Minimal programming knowledge required

CONVENTIONAL LINE SCAN SYSTEM

Conventional problems

• Compatibility issues arise due to connecting multiple devices from different manufacturers
• A great amount of time and effort is needed in order to capture good images
• Concerns with freezing or crashes due to the PC-based design
• Specialized programming knowledge is typically necessary

Line scan image capture setup in 4 easy steps!

Simple camera connection and setting allows for quick image generation

Step1

Connect the camera to the controller

The camera is ready to capture images as soon as it is connected to the controller. This eliminates the work hours that are typically consumed with setting up image capturing on a conventional line scan camera.

Step2

Set image capture conditions

All parameters related to image capture are located in the Image Capture Unit of the XG program.
The detailed settings are configured in a straight-forward, top to bottom order.
 

Step3

Adjust focus and aperture

Adjust the focus and aperture of the lens utilizing the LED indicators located on the back of the camera for reference.
 

Step4

Correct for inconsistent image brightness

Misalignment of the light mounting position or workpiece position can cause uneven lighting in the captured image. Using the intensity waveform that has been generated in the waveform viewer as reference, correction can be performed before the image data is transferred to the controller.
 

  • Ultra High-Speed, Multi-Camera, High-Performance Image Processing System
  • New Function: LumiTrax

VISION LIBRARY

  • KEYENCE Information Network - XG-8000 Image Processing System
  • General Catalog Request
  • Trade Shows and Exhibitions
  • eNews Subscribe

More Series In Vision Systems

Types In Vision / Auto ID

Vision / Auto ID