A large steel processing manufacturer with multiple service centers throughout the US, prepares strips of metal rolls in order to provide metal forming, machining facilities, fabricators, and other miscellaneous parts for automakers and related heavy-industry appl
Gauging was performed using hand gauges, contact-type gauges, or some other less accurate indirect methods. Having no standard developed practice, workers at the plant were not taking reliable measurements.
A non-contact method from another brand was once used, but did not prove reliable due to the varying quality of the surface condition from a dozen different metal suppliers. The customer then tried nuclear gauges which gave them limited success, but were too expensive.
Implementing a highly invested gauging program was not in their plans because of the added cost and slower production.
Their application problem was solved by mounting a KEYENCE LK-G157 and LK-G37 directly over the mandrel measuring thickness accuracy to within 1/10 of a mil.
The dual-head LK-G37 would also be used for off-line gauging of sampled lots.

In the past, the shipment got rejected whenever the metal was not within tolerance and the cost became insurmountable. Using the KEYENCE LK-G as an in-line non-contact measurement device made a big impact on the company's production quality and costs.
It is now keeping their automotive customers happy since accurately gauged metal helps tooling last much longer.