Character size
Normal
Large
  1. Home > 
  2. KEYENCE Advantage > 
  3. Software Programming

KEYENCE Advantage Software Programming


Sample Marking

Problem:
Initial marks are faded/poor quality.
Parts are scrapped while trying different settings.

  • Generic Laser System

    1. STEP 1
      Estimate the settings needed to mark the part.
    2. STEP 2
      Change the settings and mark the part again.
    3. STEP 3
      Compare the settings and repeat these steps as many times as necessary.
    4. STEP 4
      Apply best setting to marking program.

    Hardware Additional Cost

    The cost of scrapped parts can vary by product.

    Labor

    4 hours: Time spent applying different settings and marking the part.

  • KEYENCE ADVANTAGE

    Sample Marking provides visual confirmation of optimum marking settings in as long as it takes to mark the parts.

    Hardware

    None

    Labor

    30 minutes: Run the sample marking program once or twice and pick the best mark from a matrix.


Test Marking

Problem:
Customer driven changes require additional data to be printed on a part before production can start.

  • Generic Laser System

    1. STEP 1
      Review PLC logic and disable all functions not needed for laser marking.
    2. STEP 2
      Disable laser safeties to allow manual marking operation.
    3. STEP 3
      Test mark the part.
    4. STEP 4
      Change the marking location and rerun the part as many times needed until mark is correct.
    5. STEP 5
      Return the system to its normal operating state.

    Labor Additional Cost

    1 hour: Time spent marking and readjusting the part's position.

  • KEYENCE ADVANTAGE

    Test Marking quickly verifies the marking location and mark quality.

    Hardware

    None

    Labor

    10 minutes: Quickly display the mark and move its position without scrapping product.


Communication Protocol: Profinet/EtherNet/IP/ActiveX

Problem:
You need to communicate with an EtherNet/IP PLC.

  • Generic Laser System

    1. STEP 1
      Select a communication module that will communicate with both the laser controller and the PLC.
    2. STEP 2
      Program and verify that the controller is working.

    Hardware Additional Cost

    $500 Cost of the communication module.

    Labor

    If there were a communication problem down the road you would have 2 different components to troubleshoot instead of just the laser marker.

  • KEYENCE ADVANTAGE

    The following are supported: EtherNet/IP, Ethernet TCP/IP, Profinet, and ActiveX.
    *MD-X1000/X1500 Series only

    Hardware

    None

    Labor

    None


2D Code Verification

Problem:
Application requires 2D code verification and/or grading.

  • Generic Laser System

    1. STEP 1
      Select a barcode reader.
    2. STEP 2
      Design the barcode reader into the machine.
    3. STEP 3
      Install the barcode reader.
    4. STEP 4
      Program the barcode reader.
    5. STEP 5
      Program the PLC and test during runoff.
      Troubleshoot the functionality of both devices until the line is running.

    Hardware Additional Cost

    $3,000 Barcode reader.

    Labor

    8 hours Programming and design time.
    $600 Based on the cost of engineering time.

  • KEYENCE ADVANTAGE

    The KEYENCE MD-X can mark, verify, and grade 2D codes in one system
    *MD-X1000/X1500 Series only

    Hardware

    MD-XA1D1 Software

    Labor

    None


TrueType Font

Problem:
A specific font is preferred for a particular product.

  • Generic Laser System

    1. STEP 1
      The customer must create DXF versions of individual characters using CAD.
    2. STEP 2
      The DXF files must be imported into the laser marker software (if possible).
    3. STEP 3
      The individual characters must be compiled into a list for the font.

    Hardware Additional Cost

    None

    Labor

    2 hours for an engineer who is familiar with CAD and that laser's software to create the DXF files, import them, and compile each font.
    $150 per font based on the amount of engineering time used.

  • KEYENCE ADVANTAGE

    Any Windows TrueType font can be used in Marking Builder 3.
    *MD-X1000/X1500 Series only

    Hardware

    None

    Labor

    None


Easy Interface

Problem:
Programming needs to be done by operators with very little programming experience.

  • Generic Laser System

    1. STEP 1
      New users must be trained on the interface.
    2. STEP 2
      Experience is gained through trial and error.
    3. STEP 3
      Making more difficult changes requires onsite support.
    4. STEP 4
      Any new employees will require continuing training.

    Labor Additional Cost

    $2,000 to $5,000 per session for basic training courses.

  • KEYENCE ADVANTAGE

    The KEYENCE Marking Builder software has an extremely user-friendly laser marking interface and mimics the latest Windows-style operating system.

    Hardware

    None

    Labor

    The user interface requires minimal time to learn and the majority of our services are free to customers (support videos, etc.).

Back to top

Other Pages

  • Download Technical Materials
  • Inquiries
  • Consultation
  • Test Marking
  • DEMO
  • Product Select
  • Price Request