• Font Size
  • Normal
  • Large

CHAPTER 2FLOW METER TYPES & PRINCIPLES
FLOATING ELEMENT FLOW METER

Principles and features of floating element flow meters

Various types of flow meters and flow sensors are available. This section summarizes the principles and features of floating element flow meters.

PRINCIPLES

This is classified as an area flow meter. Its mainstream method involves suspending a float in a tapered pipe (a pipe that progressively widens heading upwards). When the fluid is forced in between the tapered pipe and the float, a differential pressure is generated. When this happens, the float stops at an area where the upward force caused by differential pressure and the downward force caused by the weight of the float have been equalized. The resulting display is the instantaneous flow.
Commonly, the tapered pipe is manufactured from transparent materials calibrated for flow and measurements are read directly from the pipe. There are also types available that have a magnet built into the float and perform detection using a magnetic sensor.

FLOATING ELEMENT FLOW METER

FLOATING ELEMENT FLOW METER

FEATURES OF A FLOATING ELEMENT FLOW METER

PROS ・Able to detect gases, liquids, and vapors
・Generally low priced
・Comparatively low pressure loss
CONS ・Does not offer very high accuracy
・Not suited for fluids that include solids (clogging will occur)
・With the directly-read type, the float cannot be seen if the tapered pipe becomes dirty (frequent maintenance required)

Back to INDEX

Back to page top

To solve the problem related to the Flow Sensor!