America

About software updates

Print Page

Last updated on:

Nov 7, 2013

Version:

R2.00.00

Update file:

IV-M30_Update_R2_00_00_GB.exe

Checking the version number:
  • (1)Turn ON the menu on the run screen and touch the ”Monitor Settings" button.

  • (2)Touch the "System" button and then touch the "Monitor Information" button.

Necessary preparations:

USB memory

Note:

Do not turn of the power of the device while the update is being performed. Otherwise the device may be damaged.

The program settings will not be deleted.

Update process:
  • 1.Download the update file.

    • (1)Create a new folder on the hard disk drive.

    • (2)Click on the "download" button on the download site. A "File download" dialog will be displayed.

    • (3)Click on the "Save" button. A "Save as..." dialog will be displayed.

    • (4)Designate the folder you created in (1) as "save location" and click the "save" button. The update file will download.

    • (5)When you double-click the update file, a dialog opens asking you to enter the folder for file extraction. With the "browse" button specify the folder you just created and click "OK".

    • (6)Click on the "Extract" button to start the extraction.

    • (7)If the extraction completes normally, the following file will be created in the specified folder. The file extension may not be displayed depending on the settings of the PC.

    • ・IV_MONITOR_UPDATE_BIN

  • 2.Update the monitor.

    • (1)Copy the created file to a USB memory.
      ・Connect a USB memory to the PC and open it.
      Copy the created file (IV_MONITOR_UPDATE_BIN) to the root folder of the USB memory. The root folder is the folder immediately after you open the USB memory. If the USB memory is the E drive, it is "E:\".
      ・Detach the USB memory from the PC.

    • (2)Connect the USB memory to the IV-M30.

    • (3)Turn ON the menu on the run screen and touch the ”Monitor Settings" button.
      If no sensor is connected, proceed with step (4).

    • (4)Touch the "System" button and then touch the "Update Monitor" button.

    • (5)Confirm the current version number and a new version number displayed on screen.

    • (6)If there are no problems, touch the "OK" button. The update will start.

    • (7)A "Now Updating..." screen will be displayed. When "Monitor update complete" is displayed on screen, the update is complete.

    • (8)Detach the USB memory and touch the "OK" button.

Main changes/revision history:
  • [Changes from R1.02.00 -> R2.00.00] Dec 25 2012
    1. Added feature
    Compatibility with Italian / French / Spanish / Portuguese / Korean

  • [Changes from R1.01.01 -> R1.02.00] Mar 22 2012
    1. Added feature
    Now supports German language.

  • [Changes from R1.00 -> R1.01.01] Mar 22 2012
    1. Added feature
    Now supports Chinese language (simplified/traditional).

Close Window

Back to top