Dec 20, 2014
R3.00.40
IV-Navigator_R3_00_40_GB.exe
Log on as a user with administrator rights.
If the user account control screen is displayed during installation, click on the [Continue] button.
When you are logged on using a user account that does not have administrator rights, enter the user name and password of an account that has administrator rights. (For Windows 7)
1.Download the file.
(1)Create a new folder on the hard disk drive.
(2)Click the "Download" button in the download site. The "Download File" dialog is displayed.
(3)Click on the "Save" button. The "Save as" dialog is displayed.
(4)Specify the folder that you created in (1) as the "Save destination" and click on the "Save" button. The file is then downloaded.
(5)Double-click the downloaded file, and a dialog for specifying the extraction destination folder is displayed. Specify the folder you have just created using the "Refer" button and click "OK".
(6)Click on the "Install" button to start extraction.
(7)When the compressed file is extracted successfully, the extracted files appear in the specified folder.
2.Install IV-Navigator.
(1)Double click on “setup.exe” within the downloaded files to begin installation.
(2)The “Welcome to IV-Navigator Install Shield wizard” dialog is displayed. Follow the steps in the wizard to install the software.
(3)When the "Completion of Install Shield wizard" dialog is displayed, installation is complete.
[Changes from R2.00.10 ->R3.00.40] December 20, 2014
Direct connection (2 units or more) function added
[Changes from R1.10.00 ->R2.00.00] December 25, 2012
1.Added features
Compatibility with Italian / French / Spanish / Portuguese / Korean
IVP-Convertor added
[Changes from R1.02.00 ->R1.10.00] August 21, 2012
1.Simulator function added
2.Image capture function added
[Changes from R1.01.01 ->R1.02.00] March 22, 2012
1.Added features
German language support added.
[Changes from R1.00.00 ->R1.01.00] March 5, 2012
1.Added features
Chinese (simplified/traditional) language support added.