United States

About software updates

Last updated:

Nov 7, 2013

Version:

R2.00.00

File available for download:

IV-Navigator_Update_R2_00_00.exe

Note:

Log on as a user with administrator rights.

If the user account control screen is displayed during installation, click on the [Continue] button.

When you are logged on using a user account that does not have administrator rights, enter the user name and password of an account that has administrator rights. (For Windows 7)

It cannot be installed to a PC which does not have the former IV-Navigator installed.

How to upgrade:
  • 1.Download the file.

    • (1)Create a new folder on the hard disk drive.

    • (2)Click the "Download" button in the download site. The "Download File" dialog is displayed.

    • (3)Click on the "Save" button. The "Save as" dialog is displayed.

    • (4)Specify the folder that you created in (1) as the "Save destination" and click on the "Save" button. The file is then downloaded.

    • (5)Double-click the downloaded file.

    • (6)The “Welcome to IV-Navigator Install Shield wizard” dialog is displayed. Follow the steps in the wizard to install the software.

    • (7)When the "Completion of Install Shield wizard" dialog is displayed, installation is complete.

Main Changes/Revision History
  • [Changes from R1.10.00 -> R2.00.00] December 25, 2012
    1.Added features
    Compatibility with Italian / French / Spanish / Portuguese / Korean
    IVP-Convertor added

  • [Changes from R1.02.00 -> R1.10.00] August 21, 2012
    1.Simulator function added
    2.Image capture function added

  • [Changes from R1.01.01 -> R1.02.00] March 22, 2012
    1.Added features
    German language support added.

  • [Changes from R1.00.00 -> R1.01.00] March 5, 2012
    1.Added features
    Chinese (simplified/traditional) language support added.

Close Window

Back to top