America

About software downloading

Print Page

KV COM+ for Excel (English version)

Restrictions on the trial version of KV COM+ for Excel
  1. There are no restrictions during setup.Communication is possible for up to a total of 60 minutes.
  2. Additionally, when communication begins or when a restriction has been reached, a message window giving notice of said item will be displayed on the screen.
Supported OS

PC pre-installed with an English language version of Windows 7/Vista/XP/2000

Supported Excel version

Microsoft Office Excel 2010/2007/2003/2002/2000

Operating environment

Windows 7/Vista:
Processor recommended by Microsoft Corporation
Memory recommended by Microsoft Corporation

Windows XP/2000:
Pentium 800MHz or higher (Pentium 1GHz or higher recommended)
Minimum of 256MB of memory

Requires 200MB or more of free hard disk space

Installing the trial version of KV COM+ for Excel
  1. Download desired software to any directory.
  2. When you run the downloaded file, the installation screen appears automatically.
    For subsequent operations, follow the on-screen instructions.

* This software can be uninstalled.

Close Window

Back to top