'14/5/26
R2.11
Confirm the first line in the “version information” dialog by clicking “help” on the menu.
If THERMO PRO V R2.11.00 is displayed, update is not necessary.
PC for installing THERMO PRO V
・Make sure to confirm the version number of TR performance software before updating.
After the update is completed, the soft will properly operate in the combination with the TR main unit from the version below.
TR-H/TR-W :From version R2.00
TR-V :From version R1.66(R1.56)
If creating backup copies of measurement display, device, alarm instruction, and check list settings before updating, make sure to use THERMO PRO V which is not updated yet.
After updating, connecting with TR main unit which is not updated may be difficult.
In such a case, use USB memory for making backup. The measurement data and setting files saved in PC before updating can be opened in THERMO PRO V after updating.
The measurement data file (extension .krd) saved in THERMO PRO V(from version R2.00)can’t be read out with the version prior to R2.00 and TR-V Series.
For example, after reading out the measurement data saved in TR-V Series with THERMO PRO V(From version R2.00), the named and saved file can’t be read out with “Load ref waveform” in TR-V Series.
When reading out the measurement data file(extension .krd) saved in TR-V with THERMO PRO V(From version R2.00), overwrite save can’t be done. Save under a new file name.
Download the update files.
(1)Create a new folder on the hard disk.
Click the right mouse button on desktop. Choose “folder” in “new document” from pull-down menu, and “a new folder” is created. Name the “new folder” discretionally.
(2)Click “Download” button on download site, and the dialog indicating “File download” will be displayed.
(3)Click” Save” button in “File download” and the dialog indicating “Save As…” will be displayed.
(4)Specify the folder that was created in step (1) in “save location” and click “Save” button. Then TPV21100.EXE will be downloaded.
Install the update software.
(1)Execute the downloaded TPV21100.EXE, and the dialog “THERMO PRO V Install Shield Wizard” will be displayed. Proceed to install as following the instructions.
(2)Installation is completed when the dialog “Completion of Install Shield Wizard” is displayed.
(3)Start up THERMO PRO V and Confirm the first line in the “version information” dialog by clicking “help” on the menu. If THERMO PRO V R2.11.00 is displayed, update is successfully completed.
[Changes from R2.10 to R2.11 ] '14/5/26
Function addition
Chinese (Traditional Chinese/Simplified Chinese) PDF manual was supplied
[Changes from R2.00 to R2.10] '13/10/30
Function addition
THERMO PRO V
Icon for reading serial number file was added
FileViewer4
Mark search function was integrated with file search function.
File search was accelerated.
[Changes from R1.63 to R2.00] '13/6/17
Function addition
Compatible with TR-H Series and TR-W Series
THERMO PRO V
Function for choosing the method of reading serial number file was added.
Function for reading out the measurement serial data file is added.
Icon for starting FileViewer4 is added.
FileViewer4
“Ending data time” box was added.
[Changes from R1.52 to R1.63] '12/8/24
Function addition
Function for printing a list of channel name on a separate sheet was added. (Channel condition printing function)
Alternation was made to print channel name on the right side of the chart up to 8 letters in full-width character. (Only at the time of printing)
Fixed bugs
The problem that PRINT TOOL sometimes did not work was modified.
[Changes from R1.51 to R1.52] '11/6/3
Fixed bugs
On the “Comment history” screen, the problem that jumping couldn’t be properly done when clicking “Jump” was modified.
The problem that jumping to the “Comment history” screen could not be done properly when right-clicking on the comment of the measurement data or hand-writing title was modified.
[Changes from R1.41 to R1.51] '10/7/15
Function addition
Compatible with performance software R1.50
Compatible with Windows7
Fixed bugs
The problem that the file couldn’t be saved by specifying the name was modified.
[Changes from R1.40 to R1.41] '10/1/15
Function addition
Compatible with performance software R1.40
LANTOOL2
SMTP authentication function was added to mail delivery function.
[Changes from R1.30 to R1.40] '09/11/10
Function addition
Compatible with performance software R1.40
THERMO PRO V
Display setting template function was added.
Image copying function on comment history screen was added.
Sorting function on comment history screen was added.
Compaction display of unit number and channel number
Fileviewer4
Routine comment or comment title search function was added.
Function for date and time search was added.
LANTOOL2
Setting range of FTP file transfer cycle was modified.
Date and time of updating and creating FTP transfer file was modified.
[Changes from R1.02 to R1.30] '09/03/17
Function addition
Compatible with performance software R1.30