America

About software downloading

Print Page

VT STUDIO (VT-H5J)(Japanese version)

Updating VT STUDIO (VT-H5J)

  1. Supported operating systems*1

    Windows 8/7/Vista (SP2 or later)/XP (SP3 or later)

  2. Required free space on hard disk*2

    VT-H5J (Japanese version): 3 GB min.

  3. Required display

    1024 × 768 pixels min.
    High colour (16-bit) or higher

  4. Graphic hardware requirements

    VRAM video card with 128 MB or higher memory that supports Microsoft DirectX® 9.0 c or higher*3

    *1 32-bit version only for Windows Vista/XP operating system
    *2 When using the speech synthesis database, maintain the following additional free space on the hard disk:
    English: 1.2 GB or higher, Japanese: 1.5 GB or higher, Chinese: 600 MB or higher, Korean: 1.3 GB or higher, Spanish: 1.3 GB or higher
    *3 The VT simulator requires a VRAM video card with 256 MB or higher memory.

  5. Install the software update using the following procedure:

    (1) All the files downloaded to the same directory.
    (2) When you specify an installation destination folder name during the installation, specify the folder in which VTSHpUpdate510.exe was installed.
    (3) Install the software update according to the on-screen instructions.

Close Window

Back to top