United States

Green LED Ensures High Performance

Built-in CMOS Monitor Camera Enhances Usability

High-Accuracy CCD Micrometers LS-7000 Series

High-speed & High-accuracy [ Double the conventional ability ]

2400 samples/second, 0.002 Mil (±0.06 μm) repeatability

The continuous exposure measurement using HL-CCD enables high-speed sampling, which doubles the conventional speed and accuracy. Unlike the laser scanning method, there is no void in detection. This allows for wider applications that require more precision due to finer product designs, or faster line speed due to shorter manufacturing times.

Measurement with continuous exposure by CCD

Measurement with continuous exposure by CCD

The measurement uses the average value within the exposure time. Even an instantaneous change can be detected reliably.

Measurement by laser-scanning method

Measurement by laser-scanning method

A change that occurs between the laser scan paths cannot be detected.

High-durability[ Best in its class ]

CCD without moving parts & Long-life LED

The laser scanning data gathering method was thoroughly reviewed and resulted in a new design combining a Green LED and HL-CCD. This solved the problem of motor durability, which was the weakest point of the laser-scanning method. A long-life LED also provides greater reliability over a long period of time.

HL-CCD

HL-CCD

Green LED

Green LED