Machine Vision
- Presence/Absence
- Measurement
- Flaw Detection
- Positioning/Alignment
- Character and Barcode Reading
- Line Scan
- 3D Inspection and Measurement
- 3D Vision-Guided Robotic and Bin Picking
- Weld Inspection
- Position Correction
- Advanced Color and Product Type
- Quantity Inspection
- Appearance Inspection
- Dimension Measurement
- Identification & Connector Inspection
- Aerospace
- Automation Equipment/Machine Building
- Automotive
- Commodities
- Defense
- Electric Vehicles
- Electronic Device
- Fabric/Textile
- Food/Beverage Packaging
- Logistics
- Machine Tools
- Marine
- Medical Device Manufacturing
- Mining/Metals
- Paper Manufacturing
- Pharmaceuticals
- Printing
- Semiconductor/Manufacturing Electronics
- Solar
- Tobacco
- Vision-Guided Robotics
What is Machine Vision?
Machine vision, or computer vision, is a technology that enables computers to analyze and interpret visual data from images or videos. It’s an automated system designed to "see" and understand surroundings to perform tasks.
These systems use high-resolution cameras and algorithms to analyze data like shape, color, texture, and size. They detect patterns, trigger actions, and perform advanced tasks such as 3D modeling, motion tracking, and object recognition.
This technology offers diverse applications of machine vision systems across industries. In manufacturing, they optimize automated inspection and quality control. In healthcare, they support medical imaging and diagnostics, and for self-driving vehicles, they enhance object detection and navigation.
How Does Machine Vision Work?
Machine vision mimics the human visual system using cameras for image capture and advanced software for interpretation. It consists of four key components: lighting, optics, image sensors, and processing algorithms. Each element is crucial for capturing high-quality images and accurate interpretation.
Lighting
Lighting is crucial in industrial machine vision, affecting image quality, contrast, color fidelity, and texture. Proper lighting ensures images have enough contrast and detail for accurate analysis by the system. Types of lighting used include ambient, area, backlights, ring lights, and infrared.
Optics
The second component of a machine vision system is optics, which includes lenses or mirrors that focus light onto the image sensor. Optics selection affects the field of view, focal length, and depth of field. A larger field of view captures more data at once, while a smaller one offers higher magnification but less information per frame. Focal length dictates the detail visible, and depth of field pertains to the range of distances in focus.
Image Sensors
Image sensors are electronic components that act as the visual interface of a machine vision system, converting light into electrical signals processed by algorithms to create images. The two main types are complementary metal-oxide-semiconductor (CMOS) sensors and charge-coupled devices (CCDs). CCDs are more sensitive and faster, while CMOS sensors generally offer better image quality.
Processing Algorithms
The final component of a machine vision system is a suite of processing algorithms for analyzing images and extracting valuable information. These use mathematical techniques like pattern recognition, edge detection, and segmentation to identify objects, measure dimensions, detect defects, or make decisions based on criteria. The complexity varies with the application of the machine vision system and desired outcomes.
The Benefits of Machine Vision
Machine vision technology uses cameras, computers, and software to automate visual tasks in industrial settings. It offers significant benefits to manufacturing, such as improved product quality, increased efficiency, reduced labor costs, and minimized waste.
- Improving Product Quality: Manufacturers can detect minor defects during production, allowing for real-time adjustments and reducing the number of defective products.
- Increased Efficiency: As machines take over repetitive visual inspection tasks, production becomes more efficient and consistent, reducing human error and improving accuracy.
- Reduced Labor Costs: Machine vision automates manual tasks, allowing workers to focus on complex tasks needing human decision-making.
- Minimized Waste: Real-time visual feedback allows machines to adjust during production, minimizing scrap and conserving time and resources.
Industries That Use Machine Vision
There are many industries using machine vision, with applications broadening as technology advances and becomes more cost-effective. From automotive manufacturing to logistics, it demonstrates value in enhancing efficiency, accuracy, and productivity across various sectors. Below is a closer look at how machine vision is being utilized.
Applications of Machine Vision Systems
Machine vision system applications have transformed how industries handle inspection and quality control. Their rapid image capture, data analysis, and decision-making capabilities have made them essential in many industrial applications:
Machine Vision in Automated Manufacturing
In automated production environments, inspection must keep pace with throughput. Machine vision systems support automation by inspecting parts directly as they move through the production line, allowing every unit to be evaluated without slowing the process.
Rather than relying on sampling or manual checks, machine vision integrates inspection into the flow of manufacturing. Cameras capture images of each part at defined points, and software evaluates those images in real time to verify quality, alignment, and correct assembly. Inspection results are available immediately, allowing issues to be identified before defective parts move further downstream.
Because inspection occurs inline, automated machine vision systems help maintain consistent quality while improving efficiency. Every part is evaluated using the same criteria, reducing variation caused by manual inspection and supporting stable, repeatable production processes.
Machine vision systems are also designed to handle the natural variability of automated lines. As parts shift slightly in position, orientation, or appearance, vision systems evaluate each part as it appears rather than relying on fixed mechanical assumptions. Inspection data can be shared with downstream equipment—such as robots or positioning systems—allowing processes to adjust based on the actual condition of each part.
By combining inspection and feedback within a single system, machine vision plays a critical role in modern automated manufacturing, helping manufacturers increase throughput, reduce scrap, and maintain reliable quality at scale.
Latest Machine Vision Technologies
Pattern Projection Lighting
Simultaneous 2D and 3D imaging for all standard vision applications.
LumiTraxTM Lighting
Directional lighting enhances height features and reduces glare, while minimizing the effect of ambient light.
Multi-Spectrum Lighting
Versatile lighting with 8 available colors to account for part variation with LumiTraxTM compatibility in all colors.
LED Lighting
High-intensity lighting to ensure high quality image capture every time.
3D Vision-Guided Robotics
Automated, high performance 3D bin picking. Quick and easy to deploy with Auto-Calibration, Robot Path Planning, and Picking Simulator.
2D Vision-Guided Robotics
Machine vision systems for pick and place applications, with direct connection and automatic calibration for most major robot manufacturers.
Inline 3D Cameras
High-accuracy appearance and dimension inspection for products and materials of all types.
Line Scan Cameras
High-speed cameras for inspection and defect analysis on large parts, continuous webs, and cylinders.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
Related Products
Related Downloads
Related Information
- Presence/Absence
- Measurement
- Flaw Detection
- Positioning/Alignment
- Character and Barcode Reading
- Line Scan
- 3D Inspection and Measurement
- 3D Vision-Guided Robotic and Bin Picking
- Weld Inspection
- Position Correction
- Advanced Color and Product Type
- Quantity Inspection
- Appearance Inspection
- Dimension Measurement
- Identification & Connector Inspection
- Aerospace
- Automation Equipment/Machine Building
- Automotive
- Commodities
- Defense
- Electric Vehicles
- Electronic Device
- Fabric/Textile
- Food/Beverage Packaging
- Logistics
- Machine Tools
- Marine
- Medical Device Manufacturing
- Mining/Metals
- Paper Manufacturing
- Pharmaceuticals
- Printing
- Semiconductor/Manufacturing Electronics
- Solar
- Tobacco
- Vision-Guided Robotics