Even when the depth-of-field is shallow and the overall focus is poor, some areas of a target are still in-focus. As the distance between the lens and the object change, the area of focus also changes. By moving the lens throughout the different focal planes on a target, the VHX captures every pixel that comes into focus at each level and combines them into a single, fully-focused image.
The advancement of depth composition technology also extends to processing speed in addition to image quality. No matter how brilliant a technique can be, it is not practical if the operation or calculation takes too long.
The high-speed processing technique of the VHX-6000 advances the technology to benefit users' analysis tools.
The real-time depth composition function allows you to display fully-focused images, in real-time, simply by moving the stage to the area of interest.
High-quality depth composition images can be generated in UXGA resolution with high-speed calculations and position/magnification correction.
Glossary