Table of Contents
- Key Takeaways
- Making Sense of AI in Business Automation
- RPA As the Starting Point for Automation
- How AI Improves Everyday Automation
- A Simple Way to Think About AI + RPA Together
- Where This Approach Works Best
- Why You Don’t Need to Start Over
- A More Flexible Approach to Automation
- Turning Automation Into Something You Can See in Action
- See How AI and RPA Work Together in Your Environment
- Related Downloads
- Latest Content
Key Takeaways
- AI enhances RPA by interpreting unstructured data like emails, while RPA executes the subsequent structured tasks.
- You can integrate AI into specific steps of existing RPA workflows without needing a complete system overhaul.
- Combine AI and RPA to automate complex processes involving unstructured data, moving beyond simple data entry tasks.
- This approach is most effective for workflows with mixed data, such as processing invoices and handling email requests.
Integrating AI with RPA doesn't have to be complicated or require a total system overhaul. By combining these tools, you can move beyond simple data entry to automate complex tasks that involve emails, documents, and messy data. This approach allows your team to improve efficiency at any stage, making your existing workflows smarter and more flexible without starting from scratch.
Making Sense of AI in Business Automation
Many businesses want to use AI but are not always sure where it fits into daily work. At the same time, teams are under pressure to reduce repetitive tasks, improve accuracy, and speed up operations.
This often creates a gap between interest in AI and practical automation that can be implemented today. Most organizations do not need to choose between AI and existing automation tools. Instead, they need a practical way to combine them so they can improve workflows without disrupting current systems.
RPA As the Starting Point for Automation
RPA is commonly used to handle routine, repeatable tasks across different systems. These tasks often include copying information between applications, processing forms, and updating records.
RPA is effective because it works with existing systems without requiring major changes. This makes it a practical starting point for automation in many environments.
However, many real workflows include unstructured inputs such as emails, documents, or variable data formats. These situations are where traditional RPA alone may require manual support.
To see how RPA can fit into your workflows, visit our RPA Overview Page.
How AI Improves Everyday Automation
AI helps extend what RPA can do by handling information that is not structured or consistent.
For example, AI can interpret text in emails, extract key data from documents, or categorize incoming requests. This reduces the need for manual review at early stages of a process.
Once the information is structured, RPA can continue the workflow automatically. In this way, AI supports RPA by preparing and enriching data rather than replacing automation steps.
A Simple Way to Think About AI + RPA Together
A practical way to understand the relationship is:
RPA executes tasks, while AI helps interpret and prepare information for those tasks.
When combined, they allow automation to handle a wider range of real-world processes. This includes both structured tasks and workflows that involve variability or decision-making.
Rather than replacing existing automation, AI enhances what is already in place.
Learn more about the differences between RPA and AI technology here!
Where This Approach Works Best
AI-enhanced RPA is most effective in workflows that include both structured and unstructured elements.
This often includes processes such as:
- Handling incoming requests sent by email
- Processing documents like invoices or forms
- Categorizing or routing information before system entry
- Supporting approval workflows that require basic classification or decision support
These types of workflows are common in many business environments and often involve manual effort even when partial automation already exists.
Why You Don’t Need to Start Over
A common misconception about AI adoption is that it requires replacing existing systems or rebuilding automation from the ground up.
In most cases, AI can be introduced into existing RPA workflows in a targeted way. This allows organizations to improve specific steps without changing the entire process.
This approach reduces implementation risk, shortens time to value, and makes automation more accessible to teams at different stages of maturity.
A More Flexible Approach to Automation
Instead of treating automation as a single transformation project, it is often more effective to view it as a gradual evolution.
Some processes may remain fully RPA-based. Others may benefit from AI support in specific steps. Over time, organizations can adjust and expand based on where the greatest operational value is found.
This flexibility allows automation to grow alongside business needs rather than forcing a complete redesign.
Turning Automation Into Something You Can See in Action
Understanding how AI and RPA work together is one thing. Seeing how they apply to your actual workflows is where the value becomes clearer.
Every organization structures processes differently, and even similar tasks can vary depending on systems, data formats, and approval steps. Because of this, the most effective way to evaluate automation is not in theory, but in practice.
See How AI and RPA Work Together in Your Environment
Explore how automation can be applied to your existing workflows without redesigning your systems or changing how your teams operate today.
A KEYENCE specialist can walk through your processes and demonstrate how RPA can handle routine tasks while AI supports areas that require interpretation or analysis. This helps identify practical opportunities for automation based on your current setup and goals.
Request a demo to see how AI-powered RPA can be applied to your business at any stage of automation maturity.