About software updates

About software updates

MAJOR CHANGES/REVISION HISTORY

CHANGES FROM 3.44 TO 3.45

2. Fixed bugs
  • We have corrected the following defect: When Combine multi measurement is started at specific time, measurement results on appropriate dates cannot be extracted from "Statistics/Analysis”. This may happen when Time Zone is set other than to "(UTC+09:00) Osaka, Sapporo, Tokyo"

CHANGES FROM 3.30 TO 3.40

1. Added Functions
  • Added selection check box to enable/disable the Inspect Sink Marks and Flash function in the Save Consolidated Measurements Data confirmation dialogue box
2. Fixed bugs
  • Fixes made to prevent the selection of a focus indicator when performing a positioning search with the IM-6140
  • Fixed bug that causes an error when the size of the dimension line arc in the Angle Measurement Results is very small
  • Changed to specifications to allow the Z stage to maintain its focus position when auto-focus is used with Multi Measurement
  • Fixed bug that sometimes causes the misalignment of the Image and Edge Point Trail Display when performing Consolidated Measurement

CHANGES FROM 3.04 TO 3.30

1. Added Functions
  • Added language switching function (Japanese/English/German/French/Italian/Simplified Chinese/Traditional Chinese/Korean/Thai)
2. Fixed bugs
  • Changed calculation method for Length of Internal Processing Time During Measurement when Virtual Line is unlimited

CHANGES FROM 3.03 TO 3.04

2. Fixed bugs
  • Changed specifications to automatically return the Z-stage to the point of origin when returning to the menu screen from Measurement Settings or Multi Measurement. Z-stage height is maintained during measurement.

CHANGES FROM 2.95 TO 3.03

1. Added Functions
  • Supports IM-6120/6025/6015
  • Added Average No. of Measurements Settings function
  • Added Pattern Search Active Region settings
  • Added function that allows the Z-stage to be manually adjusted for measurement (IM-6120/6140 only)
  • Added Manual Measurement function
  • Added Automatic Transition Settings function to Combined Settings
  • Added Adjust Scan Interval function to Profile Extraction Elements

CHANGES FROM 2.92 TO 2.95

1. Added Functions
  • Added Data Output function to IM-H1T IM Data Transfer Software
  • Reduced measurement time when a large quantity of measurement objects are measured in succession

CHANGES FROM 2.81 TO 2.92

1. Added Functions
  • Added Italian and Thai to the Language Switching function

CHANGES FROM 2.71 TO 2.81

1. Added Functions
  • Added French and Traditional Chinese to Language Switching function

CHANGES FROM 2.62 TO 2.71

1. Added Functions
  • Added German and Chinese to Language Switching function

CHANGES FROM 2.53 TO 2.62

1. Added Functions
  • Added Language Switching function (Japanese/English)

CHANGES FROM 2.33 TO 2.53

1. Added Functions
  • Added "Peak Line", "Peak Circle", "Peak Arc", and "Gauge Line" to Element Tools
  • Added "Linear Pitch Angle", "Circular Pitch Width", "Area Measurement", and "Thread Measurement" to Application Tools
  • Added "Tolerance Judgement" selection function to all pitch measurements
  • Added "Inscribed and Circumscribed Circle" to Virtual Line
  • Added a function that can specify other measurement results in the radius specification for "Parallel Lines" and "Auxiliary Circle"
  • Added "Output Pattern" selection to "Auxiliary Circle"
  • Supports Maximum/Minimum Material Tolerance in "Straightness", "Perpendicularity", "Parallelism", "Point Position", and "Concentricity"
  • Possible to select a custom folder to save CSV files
  • Improved the order of numbering for Batch Measurements
  • Added Specify Pattern search direction
  • Added Measurement Results Sorting function when performing Batch Measurements
  • Improved auto-focus performance for the IM-6140
  • Added DXF Export function
  • Possible to select up to four decimal places for the angle display digits
  • Possible to perform direct input in the entry field for "Manager" from the Multi Measurement screen
  • Batch Depth Composition Image Display supported
  • Added Clear All Tolerances
  • Added "Consolidated Measurement Settings" to Password Protection in the Security Settings. Separated "Measurement Settings" and "Single Measurement"
  • Removed the Save Measurement Settings function in "Single Measurement"
  • Changed design value for "Profile Line Output" to dashed line
  • Increased File History Display in Multi Measurement Mode and Measurement Settings Mode to 50 items
  • Set lighting conditions at the end of Multi Measurement to lighting conditions when the Measurement Settings Data has been saved

CHANGES FROM 2.22 TO 2.33

1. Added Functions
  • Added French and Traditional Chinese to Language Switching function

CHANGES FROM 2.20 TO 2.22

2. Fixed bugs
  • Fixed Profile Line Output Display bug from the Statistics/Analysis screen

CHANGES FROM 2.10 TO 2.20

1. Added Functions
  • Added German and Chinese to Language Switching function
  • Changed the minimum area size in Pattern Registration
  • Added Expand Screen function in the Pattern Registration dialogue

CHANGES FROM 2.08 TO 2.10

1. Added Functions
  • Added Language Switching function (Japanese/English)
  • Added Time Zone Settings function

CHANGES FROM 2.07 TO 2.08

1. Added Functions
  • Added "Speed Priority"/"Accuracy Priority" selection to Pattern Image Registration

CHANGES FROM 1.58 TO 2.07

2. Fixed bugs
  • Reduced processing time when Reference Coordinates are being set

CHANGES FROM 1.58 TO 2.06

1. Added Functions
  • Supports IM-6140 measurement head
  • Added "Point Position" and "Perimeter Length" to Application Tools
  • Added Individual Dimension Display to Pitch Measurement
  • Supports the creation of elements in Application Tools
  • Added "Profile" to GD&T (geometric dimensioning and tolerances)
  • Added "Profile Extraction" and "Automatic Generation" to Element Tools
  • Changed the layout of the Element Tools Edit Screen
  • Added π, ARC functions, and CRD functions to Calculations
  • Added Batch Measurement (Pattern Search No. Settings) function
  • Added Consolidated Measurement Settings function
  • Added Layer Control function
  • Added Profile Statistics to Statistics/Analysis
  • Added File Search function to Statistics/Analysis
  • Added Element Batch Edit/Sort function
  • Added Folder Settings function
  • Supports network folders
  • Network sharing and FTP servers made always accessible
  • Added Device Identification Name Settings function
  • Added CSV file Auto-creation function
  • Added Serial Counter function
  • Added Auto-save Image when NG/Fail Occurs function
  • Changed Display Digits Settings function
  • Added Batch Auto-focus function
  • Added Switch Results Display function
  • Added Depth Composition function
  • Added Copy Reference Point function, Rotate&Copy function, Invert Horizontally& Copy function, and Invert Perpendicularly&Copy function for elements
  • Added Expand/Reduce Element function
  • Added Overlapping Guide

CHANGES FROM 1.56 TO 1.58

2. Fixed bugs
  • Fixed bug that prevented measurement values from being updated directly after switching to the Details Display from the Expanded Display in Multi Measurement
  • Fixed bug that sometimes displayed the message, "Perform edge extraction and then save" in error when saving measurement settings
  • Fixed bug that sometimes would cause freezing when overwriting the "Measurement/Settings Data Specification Area" display when saving measurement settings

CHANGES FROM 1.52 TO 1.56

2. Fixed bugs
  • Fixed bug that caused switching to Expanded Display when performing Multi Measurement
  • Fixed bug that did not allow measurement when setting reference coordinates based on an Auxiliary Circle
  • Fixed bug related to the transfer of data when overwriting a save with Save As

CHANGES FROM 1.38 TO 1.52

1. Added Functions
  • Added Measurement Direction Specification function to "Point-Point", "Circle-Point", and "Circle-Circle" in Basic Measurements
  • Added "Point (on an Arc)" and "Maximum/Minimum Point (Circle/Arc) to Element Tools
  • Added Edge Extraction Parameters Auto-adjustment function to Element Tools
  • Added "White Centre" and "Black Centre" to Edge direction in Element Tools
  • Added "Maximum Circle" and "Minimum Circle" output function to Circle in Element Tools
  • Supports custom axis for "Line Passing through Point" in Virtual Line
  • Supports two-point specification for "Auxiliary Circle" in Virtual Line
  • Supports Print All for the Label Printer
  • Changed maximum number of setting elements to 650 items
2. Fixed bugs
  • Applied .NET Framework, SP2 (Fixed bug that sometimes causes problems in which .NET Framework bugs would cause a forced exit or freezing.)
  • Fixed bug that sometimes causes insufficient memory errors

CHANGES FROM 1.32 TO 1.38

2. Fixed bugs
  • Fixed bug that sometimes causes unexpected errors (OMP abort:)
  • Fixed bug that sometimes causes exceptions when the remove button has been pressed on the Import/Export screen

CHANGES FROM 1.20 TO 1.32

1. Added Functions
  • Optimised execution parameters for Edge Intensity "Auto"
  • Added function that can copy original statistics data when performing Save As
  • Added Compatibility Mode

CHANGES FROM 1.14 TO 1.20

1. Added Functions
  • Added "Diameter Cross Measurement" to Applied Measurement
  • Added Edge Intensity Graph Display function
  • Added Data Backup function
  • Added Statistics Data List Column Switching function