SZ-V Solution Site

Troubleshooting Connection with the SZ-V Configurator

Cannot communicate with the SZ-V(Cannot log-in).

The power is not supplied to the SZ.

Supply power to the SZ.

For USB connection
The USB cable is not connected to the SZ-V, or is disconnected.

Check the USB cable and USB port on the computer.

For USB connection
The USB driver is not installed on the computer.

Double-click the "DPInst" file to execute it. Installation of the USB driver starts.
The "DPInst" file is in the folder where the SZ-V Configurator is installed.
(C:\Program Files\KEYENCE\SZ-V Configurator\Driver\)

For USB connection
In cases where NPN is selected in PNP/NPN Select, the SZ-V with positive grounding is connected to the PC with negative grounding through the USB cable.

Before connecting the SZ-V and computer with a USB cable, either the SZ-V or the computer should not be grounded. The brown wire and shielded wire need to be grounded in order to start normal operation.

For Ethernet connection (for the SZ-V32N type only)
The Ethernet cable is not connected to the SZ-V, or is disconnected.

Check the Ethernet cable and the Ethernet port on the computer.

For Ethernet connection (for the SZ-V32N type only)
The SZ-V network is not correctly configured.

Check the SZ-V network settings.

For Ethernet connection (for the SZ-V32N type only)
Which SZ-V to communicate with is not selected.

Select the SZ-V to communicate with through the SZ-V Configurator

Cannot transfer the configuration.

The model specified in the SZ-V Configurator mismatches the actual SZ-V model.

Check the SZ-V model in "Properties" on the Settings tab.
If the SZ-V model does not match, create new settings.

Configured number of scanner heads is different from the actually connected number of scanner heads.

Check the number of connected scanner heads.

All configurations are not completed.

Check that all settings have been configured

The specified protection zone or warning zone is configured beyond the specification.

Check the configuration of the protection zone, warning zone, and minimum detectable object size.

You do not have the authorization level to transfer settings.

If transferring settings that have not been approved, log in as the responsible personnel.
If transferring settings that have been approved, log in as the responsible personnel or maintenance personnel.

The power is not supplied to the SZ-V.

Supply power to the SZ-V.

Cannot perform the monitoring on the SZ-V.

The settings in the software do not match the settings in the SZ-V.

Match the settings between the SZ-V Configurator and the SZ-V before starting monitoring.
Run the settings on the SZ-V Configurator and to monitor the SZ-V operation, transfer the settings to the SZ-V. On the other hand, retrieve the configuration in the SZ-V to monitor the SZ-V operation according to the current configuration in the SZ-V. In this case, all settings in the SZ-V Configurator are deleted. Save the file as required.

The configuration is not completed.

Start monitoring after transferring the configuration to the SZ-V.