SZ-V Solution Site

Other States

(Nothing is displayed)

The power is OFF or the voltage is insufficient.

Ensure that the voltage is within the rated range.
Check the wiring. “Examples of wiring”

The SZ-V is in “Power Saving Mode”.

Turn power saving mode off

The SZ-V may be broken.

Replace the Display unit.

SZ-V Series Start Up

This is the start screen displayed after the power is turned on.

In approximately 8 seconds, the screen will transition to normal operation.

Waiting for Configuration

  • The SZ-V is not configured.
  • The settings are not approved yet.
  • Transfer the settings.
  • Approve the settings.

Normal Operation

The SZ-V is under normal operation.

None.

Normal Operation ON Delay

The on-delay function is operating,
OSSD is OFF.

For details, see "SZ-V Series User's Manual".

Normal Operation Laser Shutdown

The laser shutdown bank is selected.

Switch to a bank other than the laser shutdown bank.

The laser off input is ON,OSSD is OFF.

For details, see “SZ-V Series User's Manual”

Interlock

The interlock function is operating, OSSD is OFF.
The SZ-V has detected a person or an object in the protection zone.

Terminate the interlock function by returning the SZ-V to a state in which it does not detect an object in the protection zone, and then perform reset operation using the reset input.

Interlock Reset Ready

The interlock function is operating, OSSD is OFF.
Perform the reset operation to restart the SZ-V because the conditions for disabling the interlock are met.

Terminate the interlock function by performing the reset operation using the reset input.

Interlock Reset Ready 1/2

The interlock function is operating, OSSD 1/2 is OFF.
Engage reset input 1/2 to restart the SZ-V because the conditions for terminating the interlock are met.

Terminate the interlock function by performing the reset operation using the reset input.

Interlock Reset Ready 3/4

The interlock function is operating, OSSD 3/4 is OFF.
Engage reset input 3/4 to restart the SZ-V because the conditions for terminating the interlock are met

Terminate the interlock function by performing the reset operation using the reset input.

Ref. Point Undetected

One of the scanner heads does not detect a reference point(s), OSSD is OFF

Ensure that the scanner head detects the reference points.

Muting

Muting state.
The safety function has been temporarily disabled and OSSD is ON.

None.

Override

Override state.
The safety function has been temporarily disabled and OSSD is ON.

None.

Waiting for Bank Input

Waiting for bank input state.
A bank has not been selected, OSSD is OFF.

Check that the bank input is correct.

History Saving

The detection history is being saved.
The next detection history will not be saved until saving of the detection history is complete.

The SZ-V returns to the Normal Operation screen once the detection history has been saved.
Videos take about 30 seconds to save.

History Saving Suspended

In preparation of saving the detection history.
The next detection history will not be saved until preparation is done

The SZ-V returns to the Normal Operation screen once the preparation is done.

PC Connection

The SZ-V is under normal operation.
Communicating with SZ Configurator

If the connection with SZ Configurator is terminated, the SZ-V returns to the Normal Operation screen.

Operations, such as transferring settings from the SZ Configurator are being performed.
OSSD is fixed to OFF

Once the operations from the SZ
Configurator are complete and the connection is terminated, the SZ-V returns to the Normal Operation screen.