1. Home
  2. RPA Blogs
  3. 10 Oil and Gas Workflows Companies Are Automating with RPA

Blogs 10 Oil and Gas Workflows Companies Are Automating with RPA

Key Takeaways

  • Oil and gas companies use RPA for the administrative work around operations, including environmental reporting, inspection reports, permit tracking, production reports, contractor compliance, and invoices.
  • The AI Navigation RPA RK Series works at the user interface level, connecting ERP platforms, maintenance systems, production databases, regulatory portals, and spreadsheets without replacing them.
  • Permit expirations, inspection deadlines, and renewal dates are tracked automatically, with alerts sent to the responsible person.
  • Daily production data from several sources is consolidated into standard reports and distributed on a defined schedule.
  • The RK Series uses a floating license shared across teams, sites, and divisions, with no per bot pricing.

The Administrative Load Behind Oil and Gas Operations

Whether operating well sites, pipeline networks, compressor stations, terminals, refineries, or processing facilities, oil and gas organizations generate a significant amount of administrative work every day.

Inspection reports must be reviewed and distributed. Environmental data must be compiled for regulatory submission. Maintenance records must be updated across multiple systems. Contractors must be verified before accessing job sites. Production data must be consolidated into daily and monthly reports.

These workflows are essential to safe, compliant, and efficient operations, but they are often managed through spreadsheets, email, PDFs, and disconnected enterprise systems. As a result, teams spend a substantial amount of time moving information between systems rather than focusing on operational performance.

Unlike traditional software projects that require significant development effort or system replacement, RPA automates repetitive tasks across existing applications, helping teams reduce manual work while improving data accuracy and process consistency.

In many oil and gas organizations, this makes RPA a practical approach to improving efficiency without disrupting established systems or workflows.

Why Oil and Gas Is a Strong Fit for RPA

Oil and gas operations are built on a complex mix of interconnected but often disconnected systems. ERP platforms, maintenance management systems, production databases, regulatory portals, contractor management tools, and spreadsheets typically evolve independently across departments and sites.

While each system serves a specific purpose, they rarely exchange data seamlessly. This creates a dependency on manual data transfer to keep operations running smoothly. Employees frequently copy information between systems, reconcile records across platforms, and re-enter data into multiple applications to maintain consistency.

At the same time, many of the underlying workflows are highly structured. Regulatory reporting, inspection documentation, maintenance tracking, production reporting, and compliance processes follow defined rules and repeatable formats across the industry.

This combination of fragmented systems and standardized workflows creates strong conditions for RPA adoption.

Unlike integration projects that require system replacement or custom development, RPA operates at the user interface level. It interacts with existing applications in the same way an employee does, allowing organizations to automate repetitive tasks without changing underlying systems.

This is particularly valuable in environments where legacy platforms remain in place for long periods, regulatory compliance requires consistent documentation, and reporting must be repeated across multiple sites and systems.

In many organizations, these workflows still depend on skilled personnel spending significant time on data movement, reconciliation, and documentation rather than analysis or operational decision-making.

1. Air Emissions and Environmental Reporting

Environmental reporting is one of the most data-intensive responsibilities in oil and gas operations.

Organizations must regularly collect and report information related to air emissions, water discharge, waste handling, environmental monitoring activities, and regulatory compliance obligations. This data often originates from multiple systems and operational teams, making consolidation a manual and time-consuming process.

RPA can automate the collection of environmental data, populate reporting templates, validate required fields, and prepare submissions for review. It can also help ensure that reporting follows consistent formats across sites and reporting cycles.

This reduces administrative effort while improving consistency and accuracy in regulatory submissions.

2. HSE Incident Documentation and Investigation Tracking

Health, Safety, and Environmental teams manage a continuous flow of incident reports, corrective actions, observations, and investigation records.

When an incident occurs, information is often gathered from multiple stakeholders, including field personnel, supervisors, contractors, and operations teams. This information then needs to be entered into tracking systems, documented, and distributed to relevant parties.

RPA can automate the capture of incident data, creation of records, routing of notifications, and updates to tracking systems. It can also help maintain consistent audit trails across all incident-related documentation.

This improves speed and consistency in incident handling while reducing administrative overhead.

3. Field Inspection Report Processing

Inspections are conducted regularly across pipelines, well sites, processing facilities, storage tanks, and other critical infrastructure.

These inspections generate reports that must be reviewed, categorized, and entered into maintenance or compliance systems. In many organizations, this is still a manual process that creates delays between field activity and operational response.

RPA can extract inspection data from forms and documents, update centralized systems, route findings to appropriate teams, and generate summary reports for management review.

This enables faster visibility into field conditions and reduces delays in addressing issues.

4. Asset Integrity Documentation

Asset integrity programs generate continuous documentation throughout the lifecycle of critical infrastructure.

This includes inspection results, corrosion monitoring data, testing records, corrective actions, and maintenance history. Managing this information manually across multiple systems can lead to inefficiencies and inconsistencies.

RPA can standardize the collection and updating of asset integrity records, ensuring that information is consistently captured, organized, and stored across systems.

This supports more reliable asset tracking and improved operational oversight.

5. Permit and Regulatory Compliance Tracking

Oil and gas facilities operate under a wide range of permits and regulatory obligations that must be tracked continuously.

These include expiration dates, renewal requirements, inspection schedules, and documentation requirements. Managing this manually across multiple sites can create compliance risk.

RPA can monitor permit records, generate alerts for upcoming deadlines, update tracking systems, and notify responsible personnel when action is required.

This helps ensure regulatory obligations are consistently met and properly documented.

6. Daily Production Reporting

Production reporting is a core operational requirement across upstream and midstream operations.

Data is often sourced from production systems, field reports, SCADA platforms, and spreadsheets. Consolidating this information manually into daily reports requires significant effort and is prone to delays.

RPA can automate the collection of production data, consolidate inputs from multiple sources, populate standardized reporting formats, and distribute reports to stakeholders on a scheduled basis.

This improves reporting speed and consistency while reducing manual workload.

Related solution: Automating Report Generation

7. Contractor Qualification and Compliance Management

Contractors play a critical role in maintenance, construction, inspection, and turnaround activities across oil and gas operations.

Before beginning work, contractors are often required to submit insurance documents, safety certifications, training records, and other compliance materials. Tracking and validating these documents manually can slow onboarding and increase administrative burden.

RPA can automate the collection, validation, and organization of contractor documentation, while updating internal systems and notifying stakeholders when requirements are met.

This streamlines onboarding and improves compliance control.

8. Turnaround and Maintenance Documentation Management

Turnarounds and major maintenance events generate large volumes of documentation across planning, execution, and closeout phases.

Work orders, inspection records, contractor documentation, safety reports, and progress updates must be tracked and processed efficiently to avoid delays.

RPA can automate document routing, status updates, system entry tasks, and reporting activities during maintenance cycles.

This improves coordination and reduces administrative bottlenecks during high-intensity operational periods.

9. Vendor and Procurement Administration

Procurement operations involve continuous processing of vendor data, purchase requests, approvals, and supplier communications.

Many of these tasks require repetitive data entry and movement between email, ERP systems, and procurement platforms.

RPA can automate vendor onboarding, purchase order creation, approval routing, and supplier record updates while maintaining consistent process controls.

This increases efficiency and improves data consistency across procurement systems.

10. Invoice Processing

Oil and gas organizations process large volumes of invoices from suppliers, contractors, and service providers.

Invoice handling typically involves manual review, data entry into accounting systems, and matching against purchase orders or contracts.

RPA can automate invoice capture, data extraction, validation, system entry, and exception routing for review when discrepancies occur.

This reduces processing time, improves accuracy, and strengthens financial control.

Related solution: Invoice Processing Automation

Benefits of RPA in Oil & Gas Operations

Across these workflows, organizations typically see improvements in several key areas:

  • More consistent regulatory compliance and documentation
  • Reduced manual effort across repetitive administrative tasks
  • Improved accuracy in operational and financial data
  • Faster reporting cycles across departments and sites
  • Greater consistency in multi-system processes
  • Improved traceability for audits and operational reviews

How KEYENCE RPA Supports Oil and Gas Automation

Oil and gas organizations often operate across a combination of legacy systems, modern enterprise platforms, and specialized operational tools that do not naturally integrate with one another.

This creates a reliance on manual data transfer between systems to keep processes aligned.

KEYENCE RPA enables organizations to automate these repetitive workflows across existing applications without requiring system replacement or extensive development. By interacting directly with user interfaces, it allows teams to automate tasks such as reporting, documentation, data entry, and approvals while maintaining current systems and infrastructure.

This makes it suitable for environments where operational continuity, regulatory compliance, and system stability are critical.

Automating Oil and Gas Workflows with RPA

Oil and gas operations depend on structured processes that generate large volumes of administrative work across production, compliance, maintenance, and contractor management.

While these workflows are essential to safe and reliable operations, many remain highly manual and repetitive.

RPA provides a practical approach to automating these processes across existing systems, helping organizations reduce administrative burden, improve consistency, and increase operational efficiency across the enterprise.

Discover more about this product.

Click here to book your demo.