1. Home
  2. RPA Blogs
  3. How to Build an RPA Business Case

Blogs How to Build an RPA Business Case

Key Takeaways

  • An RPA business case documents which process will be automated, what it costs today, what the automation costs, and how results will be measured.
  • Leadership objections are usually specific and predictable, and most can be addressed directly in the document.
  • Finance, operations, and IT each evaluate the proposal against different criteria.
  • A well-chosen first process matters more to approval than a well-written argument.
  • A limited pilot with defined success criteria reduces perceived risk and produces internal data for the next request.

Getting approval for an automation project depends less on explaining the technology than on answering the questions decision-makers are already asking. Those questions tend to be consistent across organizations. This page outlines how to structure a business case that addresses them, which stakeholders to account for, and how to scope a pilot that produces evidence for a broader rollout.

If you are still evaluating whether the technology fits your operation, What Is Robotic Process Automation (RPA)? covers the fundamentals.

What Is an RPA Business Case?

An RPA business case is the document that justifies an automation investment to decision-makers.

At minimum, it identifies the process to be automated, establishes what that process costs the organization today, states the expected cost of the automation, defines when the investment is expected to return, and specifies how success will be measured after deployment.

The purpose is narrower than a general argument for automation. A business case addresses one process, one budget request, and one set of measurable outcomes. Proposals that argue for automation broadly tend to generate discussion rather than decisions.

What Leadership Actually Objects To

Resistance to automation proposals usually reflects specific concerns rather than general reluctance. Identifying which concern applies allows the document to address it directly.

Cost Beyond the License Fee

Decision-makers who have reviewed technology proposals before generally know that software licensing represents a portion of total cost. Implementation support, infrastructure, internal configuration time, training, and ongoing maintenance all contribute.

Business cases that present licensing alone tend to face scrutiny on this point. Presenting a complete cost of ownership, including internal hours valued at fully loaded rates, is generally more effective than presenting a lower number that later requires revision.

Disruption to Working Operations

Automation projects touch processes the organization currently depends on. Leadership concern here centers on what happens if the automation fails partway through a cycle, or if requirements surface during testing that were not visible during planning.

Addressing this usually means describing the fallback. If the automation stops, the manual process resumes, and stating that plainly reduces the perceived risk.

Skepticism from IT

IT teams often evaluate automation proposals against a different standard than finance or operations. Their concerns typically involve system access, credential handling, integration with existing infrastructure, and who maintains the workflow once it is built.

These concerns are worth resolving before the proposal reaches a budget discussion. A proposal that IT has already reviewed carries more weight than one that arrives unexamined.

A Previous Automation Attempt That Failed

Organizations that have attempted automation without success apply additional scrutiny to subsequent proposals. This is reasonable, and the business case is stronger when it acknowledges the earlier attempt rather than avoiding it.

The useful approach is to identify what differs. A previous project may have targeted a process with too many exceptions, lacked a defined owner, or attempted broad deployment before establishing a working example. Naming the difference addresses the objection more effectively than asserting that this attempt will go better.

Uncertainty About Measurable Return

Some automation benefits are straightforward to quantify, including recovered labor hours and reduced rework. Others, such as improved consistency or reduced dependence on individual employees, are harder to price.

Business cases hold up better when they quantify what can be documented and identify the remainder as benefit that has not been counted. Proposals that assign values to every benefit tend to attract questions about the values themselves.

What Each Stakeholder Needs to Hear

Approval frequently requires agreement across several functions, each evaluating the proposal against different criteria.

Stakeholder Primary Concern What the Case Should Provide
Stakeholder
Finance
Primary Concern
Cost, return, and payback timing
What the Case Should Provide
Complete cost of ownership and a defined measurement period
Stakeholder
Operations
Primary Concern
Continuity and workload during transition
What the Case Should Provide
Fallback plan and expected staff time during setup
Stakeholder
IT
Primary Concern
Access, security, and long-term maintenance
What the Case Should Provide
Systems involved, credential handling, and named workflow owner
Stakeholder
Process owner
Primary Concern
Accuracy and exception handling
What the Case Should Provide
Which steps automate, which remain manual, and who handles exceptions
Stakeholder
Executive sponsor
Primary Concern
Whether this scales beyond one process
What the Case Should Provide
Criteria for expansion and what the pilot is intended to prove

Not every proposal requires all five. Identifying which apply, and addressing each in the document, generally reduces the number of review cycles.

Choosing the Process Your Case Rests On

The process selected for a first automation affects approval more than the quality of the argument. A process that produces a clear result within a short period supports the case on its own.

Processes that tend to support a strong business case share several characteristics:

  • Repetitive and rules-based, with limited exceptions
  • High volume, or performed frequently
  • Stable, on systems that change infrequently
  • Measurable, with existing data on time spent or error rates
  • Owned by a team willing to participate

Processes that tend to weaken a business case include:

  • Work that requires judgment or interpretation at multiple points
  • Low-volume or seasonal tasks
  • Processes undergoing planned system changes
  • Work with no clear owner
  • Processes that are poorly documented or performed inconsistently

Invoice processing is frequently selected as a first project because it reflects most of the supporting characteristics and because organizations often already track its volume and error rates.

What Belongs in the Document

Business cases vary by organization, though most include the same core components:

  • A description of the current process, including who performs it and how often
  • The measured cost of that process at fully loaded rates
  • Which portion of the process the automation will handle
  • Which portion will continue to require staff involvement
  • Total cost of ownership, including internal configuration and maintenance time
  • Expected return and the time period used to calculate it
  • Success criteria and how they will be measured
  • A fallback plan if the automation stops functioning
  • The named owner responsible for the workflow after deployment

The last two items are frequently omitted and frequently asked about. Including them reduces review cycles.

Structuring a Pilot That Survives Review

A pilot converts an argument into evidence, which is generally more persuasive than projections. It also limits exposure, which addresses the disruption objection directly.

A pilot that supports a broader request typically has:

  • A single defined process rather than a category of work
  • Baseline measurements taken before the automation is built
  • Success criteria agreed to in advance by the approving stakeholders
  • A defined end date at which results are reviewed
  • A named owner responsible for building and maintaining the workflow

The baseline measurement is the component most often skipped and the one that most affects the outcome. Without a documented starting point, results after deployment become a matter of interpretation.

What to Measure After Launch

Measurement determines whether a second automation gets approved. Selecting metrics before deployment and reporting against them consistently is generally more effective than assembling evidence afterward.

Metrics commonly used include:

  • Time required to complete the process, before and after
  • Volume processed within a defined period
  • Error and rework rates
  • Exceptions requiring manual handling
  • Time spent maintaining the workflow

Reporting the maintenance figure alongside the savings figure tends to strengthen credibility rather than weaken it, since decision-makers generally expect that cost to exist.

Where KEYENCE’s RK Series Fits

The AI Navigation RPA RK Series is KEYENCE's no-code robotic process automation platform. The RK Series is intended for teams building workflows without developer support.

That characteristic affects two of the objections described above. When workflows are configured visually rather than programmed, the build work can sit with the team that already understands the process, which changes both the internal cost estimate and the resourcing question IT is likely to raise.

The costs involved do not disappear under this model. Their location within the organization changes, and a business case is more accurate when it states where configuration and maintenance time will come from.

When comparing platforms, it is worth documenting who performs configuration, who maintains the workflow afterward, and what each requires internally. Those answers often affect total cost of ownership more than the license fee does.

The Bottom Line

An RPA business case succeeds when it answers the questions decision-makers were going to ask anyway.

That means presenting a complete cost rather than a favorable one, naming which portion of the process remains manual, identifying the workflow owner, and defining in advance what a successful result looks like.

Selecting a first process that is repetitive, high volume, and already measured generally does more for approval than any element of the written argument.

Ready to Explore Automation Opportunities?

Explore how KEYENCE helps businesses automate repetitive workflows using no-code RPA software and workflow automation tools.

Explore KEYENCE RPA Software

Contact us to learn more about how our advanced technology can help take your business to the next level.

Frequently Asked Questions About RPA Business Cases

A complete business case identifies the process to be automated, the measured cost of that process today, the total cost of the automation including internal time, the expected return and the period used to calculate it, defined success criteria, a fallback plan, and the person responsible for maintaining the workflow.

Address the specific objection rather than presenting general benefits. Most resistance relates to total cost, operational disruption, IT resourcing, a previous failed attempt, or uncertainty about measurable return, and each can be answered directly within the document.

Acknowledge it and identify what differs in the current proposal. Earlier attempts often involved processes with too many exceptions, no defined owner, or deployment at scale before a working example existed.

Long enough to produce results that can be compared against a documented baseline, which depends on how frequently the process runs. A daily process generates comparable data considerably sooner than a monthly one.

Approval requirements vary by organization, though proposals commonly involve finance, operations, IT, the process owner, and an executive sponsor. Identifying which functions apply before drafting the document reduces review cycles.

In most cases, yes. IT concerns typically involve system access, credential handling, and long-term maintenance, and resolving those before a budget discussion generally strengthens the proposal.

We're here to provide you with more details. Reach out today!

Discover more about this product.

Click here to book your demo.