1. Home
  2. RPA Blogs
  3. How to Calculate RPA ROI

Blogs How to Calculate RPA ROI

Key Takeaways

  • RPA ROI compares the annual value of the work an automation handles against what that automation costs to build and run.
  • Accurate estimates begin with measuring the current process, including the cost of errors and rework.
  • Total cost of ownership includes internal configuration and maintenance time, not licensing alone.
  • ROI and payback period answer different questions, and most business cases require both.
  • High-volume, rules-based processes typically return value faster than complex or low-volume ones.

Calculating the return on an automation project does not require specialized financial modeling. It requires a clear baseline of what a process costs today, a realistic view of how much of that process can be automated, and an accurate total for what the automation itself will cost over the same period. This page outlines a practical method for building that estimate.

What Is RPA ROI?

RPA ROI is the financial return an organization earns from a Robotic Process Automation (RPA) project, measured against what the project costs to build and operate. Over a defined period, it answers whether the automation saves more than it costs.

Two related measures are often confused with RPA ROI.

Hours saved are an input to the calculation rather than a result. Those hours become a return once they are converted into a cost figure and weighed against the cost of the automation.

Payback period measures duration rather than magnitude. ROI indicates the size of the return, while payback indicates how long the organization waits before that return arrives. Most business cases include both figures.

What to Measure Before You Calculate

A return cannot be calculated without a baseline. Before applying any formula, organizations generally need four pieces of information about the specific process under consideration.

It is usually best to evaluate a single process rather than a department. A defined, repetitive task with a clear beginning and end produces a more reliable estimate than a broad category of work.

Time Spent on the Process Today

Measured time tends to be more accurate than estimated time. Estimates often understate the total, because the surrounding work is easy to overlook.

A complete measurement typically includes:

  • The core task itself
  • Time spent locating files, logins, or records
  • Switching between applications
  • Reviewing work for errors
  • Correcting work when errors occur
  • Waiting on another person or system

That total is then multiplied by how often the task runs and by how many people perform it.

Fully Loaded Cost of That Time

An hourly wage generally understates what an hour of work costs an organization.

Fully loaded cost accounts for the additional expenses attached to each employee hour:

  • Payroll taxes
  • Benefits and insurance
  • Paid time off
  • Equipment, software licenses, and workspace
  • Management overhead

Finance or HR teams can usually provide this figure for the roles involved. Using an internal number produces a more defensible estimate than applying a general rule of thumb.

With that figure available, the process can be expressed as a cost: hours per period multiplied by fully loaded hourly cost.

Error and Rework Volume

Manual data handling introduces errors, and those errors often carry costs elsewhere in the business.

Common examples include:

  • Corrections made after the fact
  • Duplicate or mismatched records
  • Late payments and missed early-payment discounts
  • Shipments delayed by inaccurate data
  • Audit findings and compliance cleanup
  • Time spent investigating discrepancies

Some of these costs are difficult to price precisely. A common approach is to quantify the costs that can be documented and to note the remainder as benefits that have not been counted. Business cases that identify their own exclusions tend to hold up better under review.

Cost of the Automation Itself

This figure represents total cost of ownership, which extends beyond the license fee.

Components typically include:

  • Software licensing
  • Infrastructure the automation runs on
  • Internal time spent configuring and testing the workflow
  • Outside implementation support, where required
  • Ongoing maintenance when a source system changes
  • Internal training

The weight of each component varies considerably between platforms. A no-code tool configured by internal staff carries a different cost profile than a platform requiring developer resources. Figures gathered from the vendors under consideration produce more accurate estimates than assumptions.

The RPA ROI Formula

The calculation itself is standard and is not specific to automation.

ROI (%) = [Total Benefits − Total Cost of Ownership) ÷ Total Cost of Ownership] × 100

Total benefits represent the annualized value of what is saved, including recovered labor cost and any error or rework cost that could be quantified.

Total cost of ownership includes all components described above, measured over the same period.

Two practices improve accuracy. The same time window should be applied to both sides of the equation, and that window should be stated explicitly. First-year figures carry setup cost, while later years generally carry only licensing and maintenance, so the two produce noticeably different results.

Calculating ROI Step by Step

The steps below use labeled inputs. Organizations substitute their own figures at each stage.

Step 1. Annual cost of the process today

(Hours per week) × (Fully loaded hourly cost) × (Number of people) × 52 = A

Step 2. Portion of the process that can be automated

Few processes automate completely, and exceptions generally continue to require human handling.

A × (Percentage of the process the automation handles) = B

Step 3. Recoverable error cost

(Annual cost of errors and rework) × (Portion the automation prevents) = C

Step 4. Total annual benefit

B + C = D

Step 5. Total cost of ownership, year one

(Licensing) + (Infrastructure) + (Configuration time at fully loaded cost) + (Maintenance) + (Training) = E

Step 6. First-year ROI

[(D − E) ÷ E] × 100

For subsequent years, E is rebuilt using recurring costs only and the calculation is repeated. The resulting figures differ substantially, which is why each should be labeled with its time period.

How to Find Your Payback Period

Payback period identifies the point at which cumulative savings equal the amount invested.

Payback (months) = Total implementation cost ÷ Average monthly savings

Monthly savings equal D divided by twelve. Implementation cost represents the one-time portion of E, covering setup, configuration, and training, and excluding recurring licensing.

Payback is often the figure that carries the most weight in budget discussions, since it describes how long the organization operates without a return.

Manual Cost vs. Automated Cost

Manual and automated processes accumulate cost differently, which is why estimates based on intuition are frequently inaccurate.

Manual Process Automated Process
Manual Process
Cost scales with volume
Automated Process
Cost is largely fixed once built
Manual Process
Paid per hour worked
Automated Process
Paid per license period
Manual Process
Capacity limited by staffing
Automated Process
Capacity limited by run time
Manual Process
Error rate varies with fatigue and workload
Automated Process
Behavior is consistent across every run
Manual Process
Added volume requires added staff
Automated Process
Added volume often requires added run time
Manual Process
No upfront build cost
Automated Process
Upfront configuration cost
Manual Process
Knowledge remains with individuals
Automated Process
Steps are documented in the workflow

Volume accounts for most of this difference. A manual process that doubles in volume generally doubles in cost, while an automated process often absorbs the increase without a proportional cost change.

What Makes ROI Arrive Faster or Slower

The same automation produces different returns depending on the process it is applied to.

Returns tend to arrive faster when a process is:

  • High volume
  • Rules-based, with limited exceptions
  • Performed by multiple people or across multiple sites
  • Stable, on-source systems that change infrequently
  • Creating a bottleneck that delays other work

Invoice processing reflects most of these characteristics, which is one reason it is frequently selected as a first automation project. Organizations modeling that workflow can use its component steps, including data extraction, approval routing, matching, and duplicate checks, to itemize the baseline measurement.

Returns tend to arrive more slowly when a process is:

  • Low volume or seasonal
  • Dependent on judgment calls and frequent exceptions
  • Built on systems that change frequently
  • Reliant on unstructured or inconsistent inputs
  • Already partially automated

This has implications for sequencing. Selecting the first automation based on speed of return, rather than on how disruptive the process feels, generally produces measurable results sooner.

Where ROI Estimates Go Wrong

Estimates tend to break on one of the two sides of the formula.

The benefit side is often overstated. The most common cause is counting time saved as money saved, when recovered hours only produce a financial return if they are redirected to other work or absorb growth that would otherwise require additional staff. Business cases are stronger when they specify which outcome applies. Assuming that a process automates completely has a similar effect, since exceptions continue to require staff time. Vendor averages introduce the same problem, as those figures reflect other organizations' processes and volumes rather than a forecast of local results.

The cost side is often understated, generally by excluding work that generates no invoice. Configuration hours represent real cost at fully loaded rates, and maintenance follows the same pattern, since source systems change and workflows require updating when they do.

A third issue relates to presentation rather than calculation. Second-year ROI appears stronger than first-year ROI because setup costs have been removed. Presenting that figure is reasonable, provided the time period is labeled.

Where the KEYENCE’s RK Series Fits

The AI Navigation RPA RK Series is KEYENCE's no-code robotic process automation platform. The RK-10 is intended for teams building workflows without developer support.

No-code configuration affects the ROI calculation through its impact on total cost of ownership. When workflows are built visually rather than programmed, the configuration work can sit with the team that already understands the process, rather than with developers or an external implementation engagement.

Two components of the model are affected. Configuration cost in the first year and maintenance cost in subsequent years both shift, since the team that built a workflow can generally adjust it when a source system changes.

These costs continue to exist in either case. Their location within the organization changes.

When comparing platforms, it is worth asking each vendor who performs the configuration work, who maintains it afterward, and what that requires internally. Those answers frequently affect total cost of ownership more than the license fee does.

The Bottom Line

RPA ROI is calculated from an organization's own process rather than drawn from published figures.

The method involves measuring what the work costs at fully loaded rates, determining realistically how much of it can be automated, accounting for total cost of ownership including internal time, and stating the time period used. Applied consistently, it produces a figure that holds up in a budget review.

Starting with a single high-volume, rules-based process generally produces the fastest return and provides measured data for evaluating additional automation opportunities.

Contact us to learn more about how our advanced technology can help take your business to the next level.

FAQs

Subtract total cost of ownership from total annual benefit, divide the result by total cost of ownership, and multiply by one hundred. Total benefit includes the fully loaded labor cost of the automated work along with any quantifiable error and rework cost.

Payback period equals one-time implementation cost divided by average monthly savings. Process volume influences this figure more than any other factor, so frequently repeated tasks generally pay back sooner than occasional ones.

A complete business case includes licensing, infrastructure, configuration time valued at fully loaded cost, any outside implementation support, ongoing maintenance, and training. Omitting internal time is a common reason estimates prove optimistic.

It can, provided the cost of those errors can be documented. Quantifying the costs supported by evidence and noting the remainder as uncounted benefit produces a more defensible estimate.

Process volume matters more than team size. A small team performing a high-frequency repetitive task may see a faster return than a larger team performing an occasional one.

Published benchmarks reflect the processes and volumes of the organizations that reported them, which limits their usefulness as a comparison. A calculated return is more meaningful when compared against local alternatives, including additional hiring, maintaining the current process, or other projects competing for the same budget.

Discover more about this product.

Click here to book your demo.