Quick Delivery and Comprehensive Support Most products are in stock and ready for same-day shipping - contact us to get your order started
  1. Home
  2. Products
  3. Measurement Sensors
  4. Spectral Interference Displacement Sensor
  5. Spectral-Interference Wafer Thickness Meter
  6. Principles

Spectral-Interference Wafer Thickness Meter

SI-F80R series

Principles

Dispersion unit

Dispersion unit

SLD

The infrared light of the wide wavelength band that has been emitted from the SLD (Super Luminescent Diode), passes through the sensor head via the polarization maintaining fiber optic cable, and is then irradiated on the surface of the wafer. Once this is done, some of the light is reflected and the remaining light passes through the wafer and is then reflected by the reverse side.

Light interference

2 reflected beams of light interfere with each other's wavelengths and then return to the spectrum unit. The intensity of the interference light is defined by the distance from the reference surface to the target and it takes an extremely large value when the distance is equal to an integral multiple of the wavelength.

Spectral analysis

Interference light is finely dispersed into individual wavelengths, and the light intensity spectral distribution is acquired from the CCD received light waveform. Additionally, wafer thickness is calculated by performing wavelength analysis such as FFT.

Tips of Measurement

  • General Catalog Request
  • Trade Shows and Exhibitions
  • eNews Subscribe

Measurement Sensors