United States

Complete Setup in Just One Click [New Concept]

An Entirely New Concept In Setup Ease. Just One Click Calibrates The Sensitivity And Resets The Display.

Point 1: Easy to detect changes (preventive maintenance)

The FS-neo provides an easy-to-read indication when the light intensity drops due to dirt or other environment related causes.

Conventional problem

Light intensity reduction is difficult to grasp.

Light intensity reduction is difficult to grasp due to individual differences in numeric values.

->

FS-NEO

All sensors initially display 100

All sensors initially display 100, making it easy to detect changes.

Point 2: The digital value resets to exactly 100

Conventional problem

The value easily shifted and the initial value of 2000 was arbitrary.

The value easily shifted and the initial value of 2000 was arbitrary.
Setting the value to an easier to read value of 1000 required a complicated operation. The ability to change the target value made it difficult to keep track of the original value.

->

FS-NEO

The numbers reset to exactly 100.

The numbers reset to exactly 100. The set values are reset to 50.
Resetting numeric values with one click offers unprecedented operating ease.

Point 3: Greater convenience when using multiple sensors

The preset function is even more useful when using multiple sensors.

The preset function is even more useful when using multiple sensors. Quickly and easily locate sensors that have become dirty or misaligned. Main and expansion unit sensors can be reset with one click by pressing PRESET on the main unit.

If the light intensity drops significantly it will not return to 100.0

If the light intensity drops significantly it will not return to 100.0, making it easy to detect the problem. The 2-output type can be used to provide a low light intensity signal to a PLC or similar controller.