[New Model]Streamline imaging and analysis with a single platform BZ-X800

Basics of Microscopes

Microscope Types & Principles

Microscope Abilities

Biological microscopes have multiple objective lenses with different magnifications to image samples with precision. The magnification of the microscope is the product of the objective and ocular lens magnifications.

The performance of a microscope, however, is not determined only by the magnification; the resolution is another important factor. Resolution is the ability to identify two light spots separately and is expressed as the shortest distance between two points that can still be distinguished as distinct entities. While a high magnification is needed in order to visualize small objects, the resolution will determine just how clearly they can be seen. For an optical microscope, the highest resolution is theoretically limited to approximately 100 to 200 nm due to the effect of the wavelength of visible light (400 to 800 nm). Consider using an electron microscope if you need higher resolution.

The numerical aperture (NA) is an important factor when considering the performance of the objective lens. As the NA increases, the resolution and brightness of the lens improves. When selecting a microscope, the user must check the NA of the lens, the magnification, and the resolution based on the samples intended for imaging.

Aberration, the distortion or blurring of an image caused by imperfections in the lens' shape, is another factor that influences lens performance. The more thoroughly the aberration is corrected, the higher the performance of the lens.

Latest developments in Microscope technology 4-part guide / Click here to download

For Your Support
Request demo
Price request
Trial unit request
Free sample testing

[New Model]Streamline imaging and analysis with a single platform BZ-X800

Catalog

Back to top

For details, please download the catalog.

Download