Recent Searches
    Series ( results)
      Models ( results)
        Keywords
          1. Home
          2. Microscope Glossary
          3. Lateral illumination

          Lateral illumination

          ILLUMINATION METHODS FOR MICROSCOPES

          There are generally two types of lighting that can be used for microscopes: transmitted and reflected illumination.
          With transmitted lighting, light shines from behind an object (usually a transparent target) to illuminate the features within that target, while reflected light is used to illuminate the surface of an object. Reflected light can be coaxial (brightfield) or from an angle (darkfield). Coaxial lighting travels along the same direction as the optical path of the lens and is used to view flat surfaces. Lateral illumination reflects off of the angled surfaces of an object and is usually used for imaging objects with textured or irregular surfaces.

          Transmitted Illumination Coaxial Illumination Lateral Illumination

          Back to top

          KEYENCE CORPORATION OF AMERICA 500 Park Boulevard, Suite 200, Itasca,
          IL 60143, U.S.A.
          Phone: 1-888-KEYENCE [1-888-539-3623]
          E-mail: tech@keyence.com
          Career Opportunities: KEYENCE Career Site