Q: What is the repeatability of the CV series?
A: CV series is repeatable to 1 pixel
Q: How does one connect a push button switch to the CV-110 to be used as a trigger input?
A: Connect pin3 to pin26 and then connect one end of the push button to pin 5 and the other end to pin 28.
Q: Does CV-110 have any one shot outputs?
A: No, there are no one shot outputs. Outputs are NPN open collector or 9 bit binary outputs.
Q: What is the length of the camera to controller cable?
A: it is 3 meters in length.
Q: Is the camera to controller cable extendible?
A: Yes, a 7m extension cable is available. (Part # OP-25525)
Q: What type of monitors should be used. Under scanning or over scanning?
A: Please use an under scanning monitor.
Q: How do I connect window output to a relay? e.g. W01
A: Please connect COM1 to 0VDC and connect W01 to relay. The other side of relay is connected to 24VDC.
Q: Is it possible to capture an image from the CV on a VHS cassette and save it?
A: Sure. Connect CV video out put to the video input of the VCR. Connect video output from the VCR to the video input of the monitor.
Q: Is it possible to save an image on the computer and place it in the CV's EEPROM?
A: No, that is not possible. CV's EEPROM is not accessible to external devices.
Q: What is the service life of the ring lamp?
A: 2000 hours approx.
Q: How long does the output remain on after CV is triggered?
A: It remains on till the next trigger input.
Q: When CV110 is switched from one program to the other, is it required to re-register the image.
A: In the CV110 it is required. But in the CV-130 it is not required as it can store multiple images. |