Summary: Chart recorders are mechanical or electromechanical devices that record an analog property onto paper charts, while data loggers are electronic devices that convert measurements into digital form for storage and analysis. Data loggers offer much higher resolution — accurate to 0.1°F or 0.056°C — react faster to temperature change, store data on high-capacity flash memory, and cost less to operate because they need no paper or ink. Chart recorders retain an advantage only in environments where electronic devices aren't desirable. Provided by KEYENCE.
Chart recorders are mechanical or electromechanical devices that typically measure an analog property and record it on paper charts as data points over time. The recording mechanism converts the input signal into an output, which then controls a pen that marks data points or variations on a rotating or linear-moving paper.
The data is captured in its analog form and is directly visible as a physical trace on paper, which is also used for storage and subsequent analysis. The movement of the pen across the paper directly corresponds to the changes in the variable being measured, producing a continuous representation of data over time.
Modern data loggers are electronic devices that measure temperature using external temperature sensors — usually thermocouples, resistance temperature detectors (RTDs), thermistors, or infrared sensors. The temperature measurement is converted into digital form, which allows a wide range of data processing, analysis, and storage.
The data can be viewed in real time and retrieved for future analysis. Digital storage eliminates the need for physical storage space, and digital loggers are typically less susceptible to different environmental conditions.
| Aspect | Data logger | Chart recorder |
|---|---|---|
| Size | Typically more compact | Usually bulkier, due to component size and the materials needed for measurement |
| Ease of use | Capable of real-time feedback, but requires some computer skills to extract data into a presentable form | User-friendly; provides immediate feedback without requiring additional steps |
| Resolution | Much higher resolution and highly accurate — up to 0.1°F or 0.056°C; reacts to temperature much faster | Lower resolution; slower response to sudden variations |
| Data storage | Onboard or removable high-capacity flash storage, in a format that is easy to transfer, back up, or analyze | Paper charts; capacity limited by the size of the paper roll, and data requires manual analysis plus additional storage space |
| Cost | Varies by features and specifications | Operational costs are much higher due to paper rolls and more frequent maintenance, which adds significantly to the initial device cost |
The choice typically comes down to application requirements. The pharmaceutical industry demands precise temperature control to maintain product quality, safety, and regulatory compliance. The same applies to food, beverages, and cosmetics, which can expire quickly when exposed to temperatures outside the safety range.
Inaccurate temperature readout and collection could result in spoilage, safety hazards, and regulatory non-compliance. The demand for high-resolution, accurate measurements tips the scale in favor of digital data loggers due to their accuracy, reliability, and versatility. KEYENCE's multi-input data loggers are capable of recording different measurements simultaneously and operate well in harsh environments.
Chart recorders have an advantage in environments where electronic devices aren't desirable.
Chart recorders rely on physical paper charts to record and store data, which limits the amount of data that can be recorded on a single paper roll. Data analysis has to be done manually through visual inspection, which can be time-consuming and prone to human error.
Chart recorders also contain moving parts and mechanical elements, all of which are susceptible to wear and tear over time. This can lead to inaccurate readings, as well as maintenance issues and occasional parts replacements.
The transition is usually driven by the need for higher accuracy, efficiency, and greater reliability. Thanks to their integrability with other computer systems, data loggers can not only record and store data but also provide automated analysis, remote monitoring, and alerts, allowing users to access data at any time from nearly any place.
Because they have fewer moving parts and no need for consumables like paper and ink, data loggers require less maintenance and cost significantly less to operate.
Most data recording methods involve measuring an analog property of an object or environment — such as dimensional measurements, temperature, pressure, humidity, and light intensity, all of which are inherently analog.
Automated analog recording captures data in physical form, typically as traces on a paper chart. Automatic digital recording measures the analog property via a sensor and converts it into digital form for storage in digital memory. Unlike analog recording, digital methods allow easier storage, transfer, and analysis of large amounts of data, since it can be processed by computers and represented as charts, graphs, or reports.
Source: KEYENCE, "Data Loggers vs Chart Recorders: What's the Difference?" https://www.keyence.com/products/daq/data-loggers/resources/data-logger-resources/data-loggers-vs-chart-recorders-what-is-the-difference.jsp