Continuous Inkjet Printers / Case Coder
Materials and Products
Production Machines
Printing Applications
Challenges in Glass Bottle Coding
Key Takeaways
- Glass is non-absorbent, smooth and often curved, causing slow ink drying, smears, and print inconsistency.
- Manufacturers in food, beverage, and pharmaceutical sectors face regulatory requirements for traceability, including batch codes, expiration dates, and barcodes.
- Efficient coding is vital for compliance, traceability, and consumer trust; CPG manufacturers must meet strict standards to avoid fines or recalls due to illegible or missing codes.
- Continuous inkjet (CIJ), laser, and UV printers each suit different needs; CIJ is most versatile for high-speed lines.
Beverage, medicine, cosmetics, spices, and even cleaning products are often stored in glass and plastic bottles for distribution. And what do all of these products have in common? As perishable goods, these products must have an expiration date clearly labeled on the packaging.
Ice cream
Cheese (cup container)
Pasta
Companies that package these goods must adhere to industry standards and federal regulations that mandate certain date codes on the packaging. That typically isn’t the issue when it comes to plastic or even metal containers, but glass can potentially be very challenging to print on, barring adequate equipment and proper ink selection.
In this guide, we’ll discuss the challenges of printing on glass bottles and introduce continuous inkjet printers (CIJ) as viable solutions for businesses that have to print on a large number of glass bottles with great speed.
Introduction to Date Coding on Glass Bottles
As stated above, date coding on glass bottles is essential for industries that produce and package perishable goods, as it conveys important information about the product. This information is useful to both the manufacturer, who uses batch numbers for quality control and logistics purposes, and to consumers, as it clearly states the product’s expiration date. In addition to expiration dates, barcodes and batch numbers are commonly required for traceability and compliance with regulatory standards.
However, as in any mass production, glass bottle coding, or coding on any type of glass container, is all about the volume and the ability to print on as much glass in as little time as possible. It may sound unreal, but it’s not uncommon for bottling companies to date code print on 100,000 bottles every hour. This means that the coding process has to be reliable and fast on top of being legible, ensuring the right data—such as expiration dates and barcodes—is printed clearly for compliance and traceability.
Direct-to-container coding technologies allow manufacturers to apply compliance information directly onto glass bottles, ensuring regulatory marking requirements are met while also supporting sustainability efforts.
Glass bottle coding isn’t as easy as it sounds due to inherent challenges associated with printing on glass.
Printing Challenges on Smooth, Curved Surfaces
Printing on glass has its own set of challenges due to the material properties of glass. Many consider glass to be fragile, implying a lack of strength, but that’s far from true. Glass isn’t fragile; it’s brittle and often used for its strength and recyclability. Glass bottles are considered challenging substrates because their non-porous surface and ability to be molded into various shapes make reliable marking difficult.
What makes glass bottle coding so challenging is the fact that glass is a non-absorbent material with a relatively smooth surface and a frequently curved form. This makes the material very hard to print on, as the non-absorbance means that the ink takes longer to dry and cure, the smooth surface might promote smears, and the curved surface area might affect the consistency of the print. The right equipment and technology are critical for effective marking on glass bottles, especially in varied production environments where dust, hygiene, and equipment specifications can impact code quality.
This issue of non-absorbency is mostly solved by using fast-drying inks, while modern printers have their way of dealing with glass bottle curvature, such as using specialized print heads. However, ink selection is also an issue, especially when printing on returnable bottles, which rely on a special, washable ink. The ink has to be durable enough to withstand the rigors of bottling, storage, distribution, transport, and use by the end consumer without being erased in the process. Surface pre-treatment methods like flame or plasma treatment can increase the surface energy of glass, thus improving ink adhesion.
However, once the bottles are collected and returned to the bottling company for reuse, replacing the glass bottle coding with a new expiration date and lot number is necessary.
On high-speed bottling lines, which can process up to 100,000 bottles per hour, features such as instant-drying inks and high-resolution marking are essential to ensure legibility and prevent smudging, maintaining consistent print quality even at rapid production speeds.
Properties of Dye Ink
- No precipitation when mixed with liquid
- Absorbed by print targets
- Short-term fade resistance
-
1Dye ink
-
2Target
-
3Dye ink sinks into targets easily
How to Print on Glass Bottles Effectively
Printing on glass bottles isn’t always straightforward. Especially when dealing with different surfaces and environmental factors. Getting good results comes down to using the right equipment, choosing the right ink, and accounting for the environment the bottles are in.
Cosmetics
Glass jar
Common Printer Types
Most operations use one of the following:
- Continuous Inkjet (CIJ) printers
These are the most flexible option. They can run different ink types and work well across a variety of surfaces, which makes them a go-to for many production lines. - Laser printers
These don’t use ink at all. Instead, they mark directly on the surface, giving you very clean, precise codes. They’re a good fit when you want to avoid ink altogether. - UV inkjet printers
These use inks that cure instantly under UV light. They’re more specialized, but they offer strong adhesion and durability on glass.
Ink Matters More Than You Think. Even with the right printer, the ink choice can make or break your results:
- Contrast is key
The code has to stand out against whatever’s inside the bottle. Pigmented inks are usually better for this. - Adhesion to glass
Glass is slick, so the ink needs to bond properly or it’ll smear or fade. - Handling condensation
Bottles often have moisture on them, especially in colder environments. The ink needs to either cut through that moisture or still hold up once condensation forms after printing. - Ongoing maintenance
Some inks (like pigmented ones) can settle if the printer sits too long, so regular circulation or use is important.
To sum it up, getting consistent, readable codes on glass bottles comes down to three things: choosing the right printer for your setup, using ink that sticks well and stays easy to read, and making sure everything holds up in real production conditions like moisture, condensation, and handling. When all three work together, you get reliable bottle coding that keeps production running smoothly.
Where Standard Options Fall Short
Even with the right equipment, standard inks can struggle with adhesion and durability on glass and similar surfaces. That’s where specialized inks like KEYENCE’s MK-13 come in.
- Stronger adhesion to smooth materials like glass, plastics, and clear films
- Improved durability with resistance to heat, abrasion, and handling
- Consistent performance thanks to a more robust binding mechanism
This means that our ink can ensure clear and long-lasting codes on glass bottles, helping brands protect product integrity, maintain compliance, and build consumer trust.
Reliable Adhesion to All Materials
Ink doesn't fade from materials that conventional ink does not adhere to. Increased adhesiveness, heat tolerance, and durability for rubbing can stick well to poly films and plastic containers.
Standard Ink
PP material film
Strong Adhesive Ink
PP material film
Date Coding on Glass Bottles: Why CIJ Printers work best
- Fast, consistent printing at high production speeds
- Good adhesion and quick drying on glass surfaces
- Lower maintenance since constant ink flow helps prevent clogging
Glass bottle coding is typically done at high speeds on production lines, which makes continuous inkjet (CIJ) printers one of the most common choices. They’re reliable, flexible, and designed to keep up with fast-paced bottling operations.
As their name implies, continuous ink printers rely on the continuous flow of ink mixed with a solvent from a reservoir. The ink is pumped from an ink reservoir through a nozzle and is broken into a large number of ink droplets through high-frequency vibration.
From there, the process is controlled internally:
- Select droplets are given an electrical charge
- Charged droplets are directed by an electrostatic field onto the bottle to form the code
- Unused droplets are recirculated back into the system
This continuous flow is a key advantage—it keeps the system running smoothly without interruption.
Circulation path
- Solvent tank: Supplies solvent to control viscosity when the ink in the main tank becomes too thick.
- Ink tank: Supplies ink to the main tank when it is empty or when the ink is too thin.
Circulation Principle
-
1Main tank: Stores the ink used in printing. Ink recovered from the gutter is also returned here.
-
2Pump: Pressurizes and feeds the ink from the main tank to the print head.
-
3Pressure-reducing valve: Adjusts the ink pressure.
-
4Piezoelectric element: Oscillates the ink stream discharged from the nozzle to separate into ink particles.
-
5Nozzle: Discharges the ink.
-
6Electrostatic electrode plates: Applies a negative electric charge to the ink particles created from the ink stream.
-
7Electrostatic sensor: Monitors whether the ink particles have the proper electrostatic charge in them.
-
8Deflecting electrode plates: Generates a magnetic field between the electrode plates to deflect ink particles according to their charge. This directs ink particles onto the print target.
-
9Gutter: Collects the ink particles that are not used in printing.
-
10Pump: Retrieves the ink particles from the gutter and feeds them to the main tank.
Summary
If you’re interested in glass bottle coding and are in the market for glass bottle coding printer equipment, don’t hesitate to contact KEYENCE and inquire about our line of continuous inkjet printers.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
Related Products
Related Downloads
-
Continuous Inkjet Printer Application Guide
This guide explains continuous inkjet (CIJ) printer applications together with pictures and illustrations. It contains many installation examples in various industries divided into food, medicine, and cosmetics; electrical machinery and electronics; and automotive, metal, and others. These examples show printing on targets specific to each industry.
Scroll
Related Information
Materials and Products
- Glass Bottles
- Plastic Bottles/Containers
- Cans
- Wires, Cables, & Pipes
- Pouches
- Metal Parts
- Corrugate Boxes
- Packaging Film
- Kraft Packaging
- Folding Cartons
- Building Materials
- PCBs
- Cartons
- Pallets & Lumber
- Corrugate Trays
Production Machines
- Paper Bag Packaging
- Box Conveyor
- Automatic Palletizer
- Sealer/Taping Machine
- Bottle Filling Machine
- Flow Wrapper
Printing Applications