Recent Searches
    Series ( results)
      Models ( results)
        Keywords
          1. Home
          2. Products
          3. Measurement Sensors
          4. Laser Displacement Sensors
          5. CMOS Multi-Function Analog Laser Sensor
          6. Applications

          CMOS Multi-Function Analog Laser Sensor

          IL series

          An Even Wider Range of Applications

          A Variety of Uses at Low Cost

          Height difference measurements of a plastic extrusion

          Height difference measurements of a plastic extrusion

          Provides constant monitoring by measuring the height using 2 sensors simultaneously, then calculates the height difference using the calculation function in the amplifier. Reliable detection is possible even if the product type or color changes.

          Warpage detection in ceramic boards

          Warpage detection in ceramic boards

          As the sensor head is compact, multiple point measurements of small-scale boards are possible. By calculating the measurement data externally, simultaneous measurements of positioning and warpage are possible.

          Thickness/width measurements of building material boards

          Thickness/width measurements of building material boards

          Thickness and width can be simultaneously measured immediately after the extrusion process. In addition, man-hours for setup and product changeovers are reduced using the thickness calibration function.

          Packaging material counting

          Packaging material counting

          Even in targets with a large amount of shape changes, reliable counts can still be achieved by detecting rising edges. The output signal is then sent to a counter or other device.

          Accuracy checks on an automotive door assembly

          Accuracy checks on an automotive door assembly

          When assembling automotive doors, by simultaneously measuring multiple points, the assembly accuracy can be evaluated. Reliable detection is possible regardless of body color.

          Position control of welding beads

          Position control of welding beads

          Through external calculations of height data from the sensor, the device detects the position of the weld seam. Welding accuracy can be improved via measurement data feedback to the welder.

          Heat processing inspection of cans

          Heat processing inspection of cans

          By observing the expansion of a can after heat processing, the results of heat processing can be evaluated. Reliable differentiation can still be conducted even if there are color changes in the cans.

          Height controls of a web material

          Height controls of a web material

          By using a long range sensor head, it is possible to control height of web materials such as steel plates and sheet materials even during transportation. The sensor head
          can be installed at a distance of up to 3500 mm 137.80".

          Differentiation of different types of plastic components

          Differentiation of different types of plastic components

          Reliable detection of small targets, can be accomplished with high precision. Part changeover is simplified using the tolerance bank function.

          Stacker counting and stack uniformity

          Stacker counting and stack uniformity

          The IL Series detects how many items are being transported along a conveyor. In addition, reliable inspection can be maintained regardless of color changes in the targets.

          Wire winding process

          Wire winding process

          Prevents irregular winding by monitoring the traverser position. In addition, feedback control to the device is possible by measuring wire height in relation to the bobbin.

          Height controls of a PC board

          Height controls of a PC board

          Controls the PC board height in the mounting and drilling processes. Various kinds of targets can be reliably controlled without being affected by the surface color.

          Detect the position of the workpiece on a pallet being carried on a conveyor

          Detect the position of the workpiece on a pallet being carried on a conveyor

          Detect the position of the workpiece that was stacked on a pallet by a palletizer. The stable detection is enabled despite of the color change and the slant of the workpiece.

          Detect whether or not the workpiece remains in the die

          Detect whether or not the workpiece remains in the die

          Confirm whether or not the workpiece is removed from the die, which prevents the die from being damaged in advance. Using the ultralong type enables the stable detection without concern for installation distance.

          Aluminum melt level detection

          Aluminum melt level detection

          Using the ultra-long type enables installation at a maximum distance of 3500 mm 137.80" without worry for the ambient temperature.

          Detection of stage inclination prior to furnace transportation

          Detection of stage inclination prior to furnace transportation

          Identifies the inclination by measuring multiple points on the stage prior to transferring to the furnace. Transferring the product after correcting the inclination allows for consistent temperature control.

          Behavior detection in an operational unit

          Behavior detection in an operational unit

          Measures the behavior of each unit in the device. Due to the small head footprint, the IL series can be installed in compact spaces. This means that the IL series can be installed even after the machinery has been set up.

          Misalignment measurement and presence detection of a wafer/glass in a cassette.

          Misalignment measurement and presence detection of a wafer/glass in a cassette.

          Measures the presence and protrusion of glass in a cassette. Stable detection is possible even if positional misalignments occur in the cassette itself by utilizing analog processing.

          Measuring the height of a chip after bonding

          Measuring the height of a chip after bonding

          Measures the height of the board pre-bonding and the chip postmounting, allowing control of the post processing suction nozzle and dispenser nozzle feedback.

          Back to top

          KEYENCE CORPORATION OF AMERICA 500 Park Boulevard, Suite 200, Itasca,
          IL 60143, U.S.A.
          Phone: 1-888-KEYENCE [1-888-539-3623]
          E-mail: tech@keyence.com
          Career Opportunities: KEYENCE Career Site

          Measurement Sensors