Manage Busbars at Two Points: Gap/Flatness Before Welding and Peak Height After Welding
Busbars are the actual current paths of battery modules. The two points of gap after assembly and peak height after welding are quantified using the LJ-X8000 Series to perform 100% inline inspection.
Three Key Points to Keep in Mind for Busbar Inspection
Rather than increasing the number of inspection items, the process can be stabilized more effectively by focusing on the two points that determine joint quality and the precautions for optical inspection.
Welding With a Gap at the Joint Surface Results in Insufficient Strength
If there is a gap between the joint surfaces of the busbar and the terminal, heat input escapes during laser welding, resulting in shallow penetration, which makes it impossible to secure sufficient joint strength and current-carrying cross-sectional area. Busbars are thick metal parts, and warpage can occur due to residual stress from pressing or bending. If a warped busbar is placed on a terminal, some part of it will remain raised even after fastening. Even if a defect is detected after welding, the module is already assembled, which increases the scope of rework. It is effective to measure the amount of gap from the terminal surface after assembly and before welding, and to reject out-of-specification parts beforehand.
Variation in Peak Height Causes Interference in Subsequent Processes
A weld bead is formed on the busbar after welding. If this peak is too high, it will interfere with the cover or insulating members placed on top, leading to assembly defects or insufficient insulation distance. If it is too low, it may be a sign of insufficient penetration. The peak height must be managed in units of several hundred micrometers, which cannot be determined by visual inspection or 2D image inspection. It is necessary to measure the height immediately after welding to detect any deviation in welding conditions.
Densely Packed Metal Components Make Optical Inspection Unstable
Busbars inside a module are located in a densely packed area of terminals, insulating members, and housings. Because shiny metal surfaces are adjacent to each other, reflections and shadows from neighboring parts can cause false detection in 2D image inspection. Methods that judge based on color or brightness will produce varying results depending on differences in plating or the degree of oxidation. If judgment can be made using the physical quantity of height, it is less likely to be affected by differences in surface conditions, allowing the same standard to be maintained.
Inline Implementation for Managing Busbars at Two Points
By placing measurements before and after welding, deviations in conditions can be detected within the process.
- 1 Position Correction and Measurement Start – Implementation ①. The 3D position correction function automatically corrects misalignment and tilt, and the automatic target detection function starts measurement. This reduces dependence on the positioning accuracy of the jig.
- 2 Gap Measurement Before Welding – Implementation ②. The terminal surface and the top surface of the busbar are captured in the same cross-section with a single image. The gap amount is calculated from the relative height of the top surface of the busbar with respect to the reference plane fitted to the terminal surface using the least squares method. Targets with gaps can be rejected before welding.
- 3 Peak Height Measurement After Welding – Implementation ③. The peak height and cross-sectional area are calculated from the cross-sectional shape of the weld bead. Even on densely packed metal surfaces, the stray light suppression function suppresses multiple reflections to accurately represent the shape.
- 4 Judgment, Recording, and Feedback – Implementation ④. NG products are rejected based on the judgment output, and measured values and images are output and saved to an FTP server. Outputting measured values to upstream equipment via PLC link can also be used to correct welding conditions.
Comparison of Busbar Inspection Methods
For height-direction management items such as gap and peak height, the differences between methods are clear. Cross-sectional area and warpage, which can also be obtained, are also summarized.
| Management Items / Installation Requirements | LJ-X8000 Series (3D cross-section profile) |
2D Vision Sensor (Grayscale/Planar Inspection) |
Contact Height Gauge | CMM (Offline) |
|---|---|---|---|---|
① Gap after assembly (before welding) |
LJ-X8000 Series (3D cross-section profile)
◎ Calculates the gap amount based on the terminal surface
|
2D vision sensor (grayscale/planar inspection)
× Cannot determine lifting in the height direction
|
Contact height gauge
△ Limited to measuring only a few points
|
CMM (offline)
○ Measurable, but offline
|
② Peak height after welding |
LJ-X8000 Series (3D cross-section profile)
◎ Quantifies the peak from the cross-sectional shape
|
2D vision sensor (grayscale/planar inspection)
× Height cannot be determined
|
Contact height gauge
△ Difficult to target and contact the peak
|
CMM (offline)
○ Measurable, but cannot match the cycle time
|
③ Cross-sectional area of weld bead |
LJ-X8000 Series (3D cross-section profile)
◎ Understands penetration trends using cross-sectional area
|
2D vision sensor (grayscale/planar inspection)
△ Can only judge by area
|
Contact height gauge
× Cannot measure
|
CMM (offline)
△ Shape measurement requires many man-hours
|
④ Warpage of individual busbar |
LJ-X8000 Series (3D cross-section profile)
◎ Calculates flatness from the height distribution of the entire length
|
2D vision sensor (grayscale/planar inspection)
× Cannot detect
|
Contact height gauge
△ Limited measurement points
|
CMM (offline)
○ Measurable, but the number of targets is limited
|
Compatibility with shiny metal and dense areas |
LJ-X8000 Series (3D cross-section profile)
◎ Diffuse reflection is suppressed by the stray light suppression function
|
2D vision sensor (grayscale/planar inspection)
△ Lighting conditions must be carefully set up
|
Contact height gauge
△ The probe may not fit
|
CMM (offline)
○ Minimal effect
|
Necessity of positioning |
LJ-X8000 Series (3D cross-section profile)
◎ Not required due to the 3D position correction function
|
2D vision sensor (grayscale/planar inspection)
× Positioning is a prerequisite
|
Contact height gauge
× A jig is required
|
CMM (offline)
× Setup is required
|
Inline 100% inspection |
LJ-X8000 Series (3D cross-section profile)
◎ 100% inspection is possible during transfer
|
2D vision sensor (grayscale/planar inspection)
△ Condition setup is required
|
Contact height gauge
× Cannot match the cycle time
|
CMM (offline)
× Offline is a prerequisite
|
Inspection records and traceability |
LJ-X8000 Series (3D cross-section profile)
◎ Save and output measured values and images
|
2D vision sensor (grayscale/planar inspection)
○ Image saving is possible
|
Contact height gauge
× Relies on manual recording
|
CMM (offline)
○ Records are kept, but the number is limited
|
Reasons for Choosing the LJ-X8000 Series for Busbar Inspection
Because the LJ-X8000 Series can capture the terminal surface and the top surface of the busbar in the same cross-section with a single scan, the amount of gap based on the terminal surface can be evaluated as is. After welding, the peak height and cross-sectional area can be calculated from the cross-sectional shape using the same configuration, allowing two-point management to be completed with a single controller. The stray light suppression function ensures stability even for targets with densely packed metal, and inline 100% inspection can be configured without the need for positioning.
Products for Measuring Busbar Gap, Flatness, and Peak Height
This inline profile measuring instrument quantifies the gap after assembly and the peak height of the weld bead using the same configuration.
Supports Gap After Assembly and Peak Height After Welding — LJ-X8000 Series
2D/3D Laser Profiler
With ultra-high-definition measurement of 3200 points/profile, the cross-sectional shape is expressed in detail, and the busbar is quantified using indicators such as height, step, width, and cross-sectional area. The terminal surface and the top surface of the busbar can be captured in the same cross-section with a single scan. The height data of the terminal surface acquired during transfer is fitted to a plane using the least squares method to serve as the reference plane, allowing the amount of busbar gap based on the terminal surface to be evaluated as is. After welding, the peak height and cross-sectional area can be calculated from the cross-sectional shape of the bead using the same configuration.
Because height images are not easily affected by differences in metal surface color, plating, or the degree of oxidation, judgment can be continued using the same criteria even if the appearance varies. The stray light suppression function works against multiple reflections and diffuse reflections that occur on targets with densely packed shiny metal, accurately representing shapes. The 3D position correction function automatically corrects for misalignment and tilt of the target, eliminating the need for positioning. When combined with the automatic target detection function, inline 100% measurement and inspection can be achieved. Inspection can be set up simply by choosing from a wide variety of measurement tools such as step, width, cross-sectional area, and angle. It also supports discharging NG products via judgment output, and outputting/saving images and measured values to an FTP server.
Obtain Detailed Materials for the LJ-X8000 Series
You can download a free catalog summarizing the sensor head specifications, measurement tools, and system configuration.
Examples of Inspection Applications Around Busbars and Terminals
Used in the busbar connection process for batteries of various shapes.
Busbar Height and Position Measurement (Cylindrical)
A single unit performs height inspection of the busbar before welding and XY position inspection after welding. While inspection of only the X and Y positions was possible with conventional image processing, processing 3D data allows height data to be acquired as well, enabling simultaneous inspection of height and position.
Bead Shape Inspection After Busbar Welding (Prismatic)
Inspects the busbar weld joint shape with 3D images to support 100% inspection of battery module weld quality. It can be used directly for peak height management after welding.
Position Confirmation Before Busbar Welding (Pouch)
When modularizing pouch cells, the positions of tabs and busbars are measured, and the position information required for welding is output. Even when different colors and materials are mixed, profiles with suppressed noise can be acquired.
Frequently Asked Questions About Busbar Inspection and Measurement (LJ-X8000 Series)
Q What should be measured in busbar inspection?
A
It is practical to focus on two points that determine the joint quality. Before welding, this is the gap of the busbar from the terminal surface, and after welding, it is the peak height of the weld bead. By also looking at the cross-sectional area, changes in the penetration trend can be captured.
Q How do you evaluate the gap?
A
The terminal surface and the top surface of the busbar are captured in the same cross-section with a single scan. The height data of the terminal surface acquired during transfer is fitted to a plane using the least squares method to create a reference plane, and the gap amount is evaluated from the relative height of the top surface of the busbar with respect to that reference plane. Because it is viewed as a surface rather than measuring a few points, local gaps can also be captured.
Q With what level of accuracy can the peak height after welding be measured?
A
Since the Z-axis (height) repeatability can be selected from 0.3 µm depending on the sensor head, minute height changes of the bead peak can be handled as numerical values. The control range is set according to the requirements and the target.
Q Can measurements be made even in locations where metal is densely packed and reflections are strong?
A
Yes, they can. For multiple reflections and diffuse reflections, the stray light suppression function works to represent the accurate shape. Because judgment is based on height data, it is hardly affected by differences in appearance due to plating or oxidation.
Q Can inline 100% inspection be performed without positioning?
A
Yes, it can. The 3D position correction function recognizes misalignment and tilt to automatically correct them, eliminating the need for positioning. The automatic target detection function also eliminates the need for an external trigger.
Q Can it be used for feedback to welding conditions?
A
Yes, it can. In addition to discharging NG products based on judgment output, measured values can be output to upstream equipment via PLC link and utilized for correcting welding conditions. Measured values and images can be output and saved to an FTP server, which can also be used for trend management.