Measure Electrode Misalignment for Each Sheet: Quantify Overhang Inline

Whether stacking or winding, the key parameter to manage is the overhang amount, where the negative electrode covers the positive electrode. The LJ-X8000 Series acquires the edge position of each individual electrode to determine misalignment numerically.

View Catalog

Inquiries regarding electrode stacking/winding alignment measurement

Why Alignment Deviation Directly Affects Safety, and the Associated Challenges

The essence is not the apparent misalignment, but the physical condition of whether the negative electrode covers the positive electrode.

Insufficient Overhang Causes Lithium Deposition

In battery cells, the negative electrode is designed to be slightly larger than the positive electrode. This difference is the overhang, which provides a margin to receive lithium ions during charging. If misalignment occurs during stacking or winding and the overhang is insufficient, lithium coming from the edge of the positive electrode cannot be received by the negative electrode and deposits as metallic lithium. As deposition progresses, it penetrates the separator, leading to an internal short circuit. Because this directly affects safety, misalignment must be reliably prevented within the process.

Different Ways Misalignment Occurs in Stacking and Winding

In stacking using Z-fold or lamination, variations in the transfer position of each sheet accumulate, changing the direction of misalignment between the top and bottom. On the other hand, in jelly rolls produced by winding, tension fluctuations and winding core runout appear as positional deviations for each turn, accumulating toward the outer circumference. Since the occurrence mechanism differs even for the same “alignment defect,” the measurement location and timing must be designed to match the process.

Management Is Impossible Without Separating Each Individual Electrode

The end face of a stacked cell has a structure where electrodes and separators of several tens of micrometers are alternately stacked. Even if only the overall external dimensions are measured, it is impossible to know which layer is misaligned and by how much. Similarly, in winding, it is necessary to separate and view the position of each turn. Without the resolution to acquire the profile of each individual sheet, the overhang amount index itself cannot be quantified. The required resolution is determined by the thickness of the electrodes and separators to be separated.

4 Steps to Measure Stacking/Winding Alignment

Since the measurement target changes for each process, measurements are divided into cutting position, post-stacking, and post-winding.

  1. 1 Electrode cutting position before stacking – Measurement ①. The electrode cutting position is measured before stacking and fed back to the equipment. Since the edge position can be stably detected from the end shape, the cause of misalignment can be suppressed in the upstream process.
  2. 2 Stacking misalignment after stacking – Measurement ②. The edge position of each individual electrode is acquired from the end face profile after stacking. High X-axis resolution allows layers to be separated and the amount of misalignment to be quantified.
  3. 3 Winding misalignment after winding – Measurement ③. The end face after winding is measured, and the positional deviation for each turn is captured as the shape of each individual electrode. Winding misalignment caused by tension fluctuations can be detected.
  4. 4 Overhang amount determination and recording – Measurement ④. The overhang amount is calculated from the difference in position between the positive electrode edge and the negative electrode edge, and out-of-specification parts are rejected via judgment output. Measured values can be saved using the FTP server function.

Comparison of Alignment Measurement Methods

On the premise that each individual electrode can be separated, the deciding factor is whether 100% inspection can be performed at inline transfer speeds and whether feedback can be sent upstream.

Management items / Installation requirements LJ-X8000 Series
(3D cross-section profile)
2D intuitive vision system
(grayscale/surface inspection)
X-ray inspection system Sampling + microscope
① Edge position of each individual electrode
LJ-X8000 Series (3D cross-section profile)
◎ Separates layers with high X-axis resolution
2D intuitive vision system (grayscale/surface inspection)
△ Difficult to separate using the contrast of the end face
X-ray inspection system
◎ Can separate internal layers
Sampling + microscope
△ Can separate, but requires destructive sample inspection
② Quantification of overhang amount
LJ-X8000 Series (3D cross-section profile)
◎ Calculated from the difference in position between the positive and negative electrode edges
2D intuitive vision system (grayscale/surface inspection)
△ Depends on the appearance
X-ray inspection system
◎ Can be quantified
Sampling + microscope
△ Can be quantified, but the number of samples is limited
③ Stacking misalignment (Z-fold/lamination)
LJ-X8000 Series (3D cross-section profile)
◎ Inspect layer by layer using the edge profile
2D intuitive vision system (grayscale/surface inspection)
△ Only overall misalignment
X-ray inspection system
◎ Can determine misalignment
Sampling + microscope
△ 100% inspection is difficult
④ Winding misalignment (jelly-roll)
LJ-X8000 Series (3D cross-section profile)
◎ Acquires the position of each turn from the shape
2D intuitive vision system (grayscale/surface inspection)
△ Outer circumference only
X-ray inspection system
◎ Inside is also visible
Sampling + microscope
△ 100% inspection is difficult
⑤ Cutting position feedback
LJ-X8000 Series (3D cross-section profile)
◎ Inspects edge position from end shape
2D intuitive vision system (grayscale/surface inspection)
○ Edge detection is possible
X-ray inspection system
× Difficult to use in-process
Sampling + microscope
× Cannot provide feedback
Tact time
LJ-X8000 Series (3D cross-section profile)
◎ Supports inline transfer speeds
2D intuitive vision system (grayscale/surface inspection)
◎ High speed
X-ray inspection system
△ Imaging and analysis take time
Sampling + microscope
× Offline
Equipment cost and ease of installation
LJ-X8000 Series (3D cross-section profile)
◎ Easy to integrate into the line
2D intuitive vision system (grayscale/surface inspection)
◎ Easy to integrate
X-ray inspection system
△ Large-scale and requires shielding
Sampling + microscope
○ Small scale
Inspection records and traceability
LJ-X8000 Series (3D cross-section profile)
◎ Save and output measured values and images
2D intuitive vision system (grayscale/surface inspection)
○ Images can be saved
X-ray inspection system
○ Images can be saved
Sampling + microscope
× Relies on manual recording

Why Choose the LJ-X8000 Series for Alignment Measurement

Because the LJ-X8000 Series has high X-axis resolution, it can separate the profiles of individual electrodes, allowing the overhang amount index to be directly quantified. The end faces can be evaluated using the same principle for both stacking and winding, and the same configuration can be used to feed back the cutting position. Without requiring shielding equipment like X-rays, 100% inspection can be configured at inline transfer speeds.

Products Compatible With Stacking/Winding Alignment Measurement

This inline profile measurement system separately acquires the edge position of individual electrodes and quantifies the overhang amount.

Supports Quantification of Misalignment and Overhang Amount for Individual Electrodes — LJ-X8000 Series

2D/3D Laser Profiler

With ultra-high-definition measurement of 3200 points/profile, cross-sectional shapes are represented in detail, and the end faces of stacked electrodes are captured separately, one by one. By combining profile measurement tools such as edge position, step, and width, the position difference between the positive and negative electrode ends (overhang amount) can be directly quantified. Because height images generated from height data are not affected by the color or gloss of electrodes or separators, stable inspection is possible even at end faces where materials change. For multiple reflections and diffuse reflections from glossy foil, the stray light suppression function works to represent accurate shapes. The 3D position correction function automatically corrects misalignment and tilt of the target, eliminating the need for positioning, and when combined with the automatic target detection function, inline 100% measurement and inspection can be achieved. It supports the rejection of NG products via judgment output and real-time feedback to upstream processes, allowing you to configure operations that include cutting position correction. It also supports saving measured values and images using the FTP server function.

View Catalog

Click here for product information on the LJ-X8000 Series

Get Detailed Materials on the LJ-X8000 Series

You can download a free catalog summarizing sensor head specifications, measurement tools, and system configuration.

View Catalog

Inquiries regarding electrode stacking/winding alignment measurement

Examples of Use in Stacking/Winding Processes

It is used throughout the process, from cutting position inspection before stacking to stacking misalignment and winding misalignment inspection after winding.

Electrode Cutting Position Inspection

Feeds back the electrode cutting position before stacking to the equipment. Because the edge position can be stably detected from the end shape, the cause of misalignment can be suppressed in upstream processes.

Electrode Stacking Misalignment Inspection

Inspects stacking misalignment after stacking with high X-axis resolution. Because the edge position of individual electrodes can be captured separately, it enables direct management of the overhang amount.

Electrode Winding Misalignment Inspection

Inspects winding misalignment after winding as shape measurement of individual electrodes. Misalignment for each turn due to tension fluctuations or core runout can be detected.

Frequently Asked Questions Regarding Electrode Stacking/Winding Alignment Measurement (LJ-X8000 Series)

Q What is the overhang amount?

A

This is the amount that the negative electrode protrudes outward from the positive electrode. It corresponds to the margin for receiving lithium ions during charging, and if it is insufficient, it leads to the risk of metallic lithium deposition and internal short circuits. It is the key indicator for alignment management.

Q Does the measurement method change between stacking and winding?

A

Although the measurement principle is the same, the measurement location and timing differ. In stacking, misalignment appears as the accumulation of individual transfer positions, while in winding, it appears as misalignment for each turn. Therefore, measurement points are designed according to the process.

Q Can individual electrodes be measured separately?

A

Yes, they can. Because the cross-sectional shape is acquired at 3200 points/profile, even on end faces where electrodes and separators of several tens of micrometers overlap, the positions can be quantified by separating each layer. Since the required resolution varies depending on the thickness of the target, we will propose a head after asking about the specifications of your electrodes and separators.

Q How should this be used differently from X-ray inspection?

A

While X-rays can see inside, imaging and analysis take time, and shielding equipment is also required. This method is suitable for continuous monitoring within the process because end face shapes can be acquired inline for every unit at the transfer speed. The two have different roles.

Q Can the measurement results be used to correct the cutting position?

A

Yes, they can. By measuring the electrode cutting position before stacking and feeding it back to the equipment, the cause of misalignment can be suppressed in the upstream process. It also supports discharging NG products based on judgment output.

Q Is measurement stable even if the color and gloss differ between the electrode and separator?

A

Yes, it is stable. Because judgment is based on height data, it is not affected by differences in color or gloss, and the stray light suppression function works against multiple reflections and diffuse reflections that occur on glossy foil.

Q Why not quantify electrode misalignment within your process?

A

The measurement configurations for both stacking and winding can be confirmed in the catalog or via the inquiry form.

Related Products