Failure Analysis for Medical and Pharma Components: Document Root Causes and Support Complaint Investigations
Failure analysis is the systematic investigation of why a part fractured, cracked, or wore out. For medical and pharmaceutical components, it starts with non-destructive examination, including fractography (the study of fracture surfaces), under a digital microscope or 3D optical profiler so the evidence stays intact. This guide covers how to analyze damage and document findings for complaint investigations.
A surgical instrument comes back from the clinic with a fracture. An explanted implant shows cracking that shouldn't be there. A batch of injection-molded parts shows chipping along the parting line, and the supplier disputes the cause. The situations differ, but the demand is the same. You need a reliable conclusion about what happened, and you need documentation that withstands scrutiny.
That is what separates failure analysis from routine quality inspection. You usually have one part and one chance, and your first step cannot be one that destroys the evidence. The sections below follow the path a real investigation takes. They begin with how to look at a damaged part without harming it, move through the examination of fractures, cracks, and wear, and show when 3D measurement becomes necessary. They finish with how to document and compare findings so they hold up in a complaint investigation.
Key Takeaways
- Start non-destructive. With one part and no second chance, image and understand the failure before any sectioning or cutting.
- Overhead-only viewing limits what you can see. Stereo and USB microscopes look straight down and have limited depth of field. The VHX Series digital microscope allows users to tilt around a sample, focus stacking for fully focused imaging, and save settings captured with the image.
- 3D capture settles raised versus recessed. It distinguishes buildup from chipping and quantifies crack depth and step height as a profile or color height map.
- Credible documentation is traceable, repeatable, and unaltered. That means scale and visible measurement geometry, stored capture settings, and preserved original files.
- When a limit value is in play, quantify. A VK-X Series 3D optical profiling microscope measures height differences at the nanometer-to-micrometer level and roughness parameters such as Ra, Rz, and Sa.
Non-Destructive First Look: Where Magnifiers, USB Microscopes, and Stereo Microscopes Fall Short
Every investigation starts with a choice, what to look at the part with. In many labs, that first look uses whatever is within reach, whether it is a magnifier, a USB microscope from the shop floor, or a stereo microscope that has sat on the bench for years. That is enough for rough classification, but rarely for a reliable conclusion. Three limitations explain why.
The first is that the view only comes from above. A classic stereo microscope looks straight down at the sample, yet a fracture surface is rarely horizontal, and the interesting structure is often on a sidewall or in a recess. Users have to fixture the part and manually adjust to see the desired area since the stereo microscope can only view a sample looking straight down.
The second is that the depth of field is too shallow. Fracture surfaces are strongly three-dimensional, so at higher magnification only one plane is in focus at a time, and your brain has to assemble the rest. That doesn't make a usable report image.
The third is that documentation becomes an afterthought. A photo taken through a camera attached to an eyepiece, a scale added later from memory, and a file with no link to the capture settings all hold up poorly in a dispute with a supplier or customer. No measurement results are saved on an image.
A 4K digital microscope addresses all three. The camera and lens tilt, so sidewalls and undercuts become visible without fixtures or manually moving the sample. Multiple focus planes are combined into one fully focused image, no need to manually adjust focus throughout one view. And documentation is automatic with image capture, including scale, capture settings, and measured values. The table below shows how the three classes of tool compare in practice.
How the tools compare
| Magnifier, USB, or stereo microscope | VHX Series Digital microscope | VK-X Series 3D optical profiling microscope | |
|---|---|---|---|
|
Typical role
|
Magnifier, USB, or stereo microscope
Rough classification
|
VHX Series Digital microscope
Imaging the failure and proving the cause
|
VK-X Series 3D optical profiling microscope
Quantifying a defect against a limit value
|
|
Height information
|
Magnifier, USB, or stereo microscope
None
|
VHX Series Digital microscope
3D view from a focus stacking (profile section, color height map)
|
VK-X Series 3D optical profiling microscope
Quantitative height and depth values, nanometer-to-micrometer scale
|
|
Roughness values (Ra, Rz, Sa)
|
Magnifier, USB, or stereo microscope
Not available
|
VHX Series Digital microscope
Possible – micron level accuracy and material dependent
|
VK-X Series 3D optical profiling microscope
Measured in damaged vs. undamaged areas
|
|
Shiny, curved, or steep-sided surfaces
|
Magnifier, USB, or stereo microscope
Not addressed
|
VHX Series Digital microscope
Focus-based height measurement, special lighting adjustments are required for more reflective surfaces
|
VK-X Series 3D optical profiling microscope
Suited to these surfaces
|
|
Documentation
|
Magnifier, USB, or stereo microscope
Often manual, with an eyepiece photo and a scale added later
|
VHX Series Digital microscope
Captured with the image, including scale, settings, and measured values
|
VK-X Series 3D optical profiling microscope
Quantitative values ready for a report
|
Examining Fracture Surfaces, Cracks, and Wear at High Resolution and at an Angle
With a capable instrument in place, users can start to better understand the fracture surface. Beach marks, fatigue striations, dimple structures, smooth cleavage surfaces, and deformation zones each point to a different failure mechanism, but only if those features are visible in the image at all. For example, see our page on metallurgical failure analysis and fracture patterns. Four capabilities make the difference when inspecting fracture surfaces.
The first is focus stacking, also called depth composition. Capturing multiple focus planes and combining them produces an image that is sharp across an entire, heavily contoured fracture surface. Only then can you discuss the origin and propagation direction of a fracture in a single image.
Tilting and rotating comes next. An angled view reveals structure on sidewalls, in notches, and at edges that stay invisible from above. On small instruments and implant geometries, this is often the difference between suspicion and finding.
Lighting then changes what the image can show. Bright field, dark field, and ring or directional lighting brings out different features, and a fine hairline crack on a polished surface often stands out in dark field while disappearing in bright field.
Finally, when a deposit or discoloration sits on the fracture surface, the optional elemental analysis on the VHX Series digital microscope shows which elements are present.
Wear analysis asks a different question. Fine structure matters less than extent, meaning how large the worn area is, how deep the material loss goes, and how the condition has changed over the service life. For that, stored capture settings matter more than maximum magnification.
3D and Topography: Buildup vs. Chipping, Crack Depth, and Step Height
Even a sharp, fully focused image regularly leaves one question open. Is the conspicuous spot raised or recessed? A deposit and a chip of missing material can look alike under front lighting, yet the cause is completely different.
Three-dimensional capture answers that directly. A focus series produces height information that can be shown as a profile section, a color height map, or a perspective view, and that supports findings that carry weight in an investigation. It can show buildup or chipping with the corresponding height or depth value, the course of a scratch or groove as a profile section across the direction of travel, and the step height at a shoulder, coating edge, or offset. It can also show the volume or area lost from a worn zone.
For most damage patterns, the 3D view of the VHX Series digital microscope is enough to answer the question and prove it. When the focus shifts to the finest structures, such as very shallow steps or surface roughness at the nanometer scale, a VK-X Series 3D optical profiling microscope is the more precise tool. For examples on medical parts, see our page on instantaneous measurement of medical devices.
When a 3D Optical Profiling Microscope Quantifies the Defect
Not every failure analysis needs a number. Often an image that shows the cause is enough. But once a limit value is in play, the assessment becomes a measurement, and the question is which method fits.
A VK-X Series 3D optical profiling microscope is the right choice when one of these applies.
- You are dealing with height or depth differences at the nanometer-to-micrometer scale.
- You need a roughness parameter such as Ra, Rz, or Sa (profile parameters per ISO 21920, areal parameters per ISO 25178) from the damaged area to compare against an undamaged area.
- The surface is shiny, curved, or steep-sided, so a purely focus-based height measurement reaches its limits.
- The result has to go into a report as a quantitative value, not just an image.
For larger areas and contours on bigger parts, a VR-6000 Series wide-area 3D optical profiler completes the toolchain. Taken together, the practical sequence is to image the part non-destructively and understand it first, then quantify with a specific goal, and only last, if unavoidable, cut the part for a cross-section.
Traceable Image Documentation for Complaint Investigations
Whatever instrument produced the evidence, a failure analysis almost always ends in a document someone else will check, whether that is your own customer, the supplier, an insurer, or in the worst case an expert witness. The same record often feeds a CAPA or a supplier corrective action request.
Some labs argue that software-assisted image evaluation is weaker in a dispute than a classic inspection report. The concern is fair, but it points to a documentation discipline problem, not a software problem. Software-assisted records are only weaker when settings and raw data aren't preserved. When they are, the evaluation is easier to reproduce and audit than a handwritten report. Three properties make image documentation reliable.
- Traceable. Every image carries a scale, magnification, lighting type, and capture date. Every measured value comes with the image it was measured in, with the measurement geometry visible. If you can't show where a number came from, you have an assertion, not proof.
- Repeatable. If capture settings are stored with the image and can be reloaded identically, the measurement can be reproduced on the same sample months later. That is the property that carries an evaluation in a dispute, and a measurement made by hand on a stereo microscope doesn't have it.
- Unaltered. The original image is preserved and edits are saved separately. Contrast adjustments that can't be undone in the original are the fastest way to make documentation open to attack.
In regulated environments, these properties map to established expectations. Complaint handling falls under quality system requirements such as ISO 13485, electronic records fall under 21 CFR Part 11, and data integrity expectations such as ALCOA+ (attributable, legible, contemporaneous, original, accurate) apply. Put user management and an audit trail in the specification early. Add an organized filing structure for each case, and the report is also usable for audits and supplier ratings.
Checking Suspect or Nonconforming Supplier Parts: Marking, Dimensions, and Surface
The same documentation discipline carries over to a special case of failure analysis, parts of questionable origin. A shipment looks different than usual, the marking sits slightly off, or the surface feels different. Before that becomes an accusation, you need evidence.
What works in practice is a comparison against a known-good reference part across several features.
- Marking and identification. Typeface, edge quality of the engraving or print, position and orientation, and structure at the bottom of the mark.
- Dimensions at characteristic points. Radii, chamfers, groove widths, and wall thicknesses at the same positions on both parts.
- Surface condition. Machining marks, groove direction, polish or blast pattern, and coating edges.
- Material. Where an optical comparison isn't enough, elemental analysis shows whether the alloy components match the specified material.
Because different capture conditions create apparent differences, both parts should be imaged under identical lighting, magnification, and orientation, and those conditions should be recorded in the report.
From First Look to Defensible Conclusion
Return to the three situations that opened this guide. For the fractured instrument, focus-stacked and tilted images of the fracture surface make it possible to discuss where the crack started and how it grew. For the explanted implant, dark-field imaging can bring out a hairline crack, and elemental analysis can identify a deposit without preparing or shipping the sample. For the chipped molded parts, a height map separates chipping from buildup, and a documented comparison against a reference part gives the supplier discussion a factual footing.
In each case, the sequence is the same. Look without destroying the evidence, quantify when a limit value is in play, document so the result can be reproduced and audited, and cut the part only if nothing else answers the question.
Frequently Asked Questions
Q How do you analyze a fracture surface without destroying it?
A
Image the fracture surface under a digital microscope without cutting or coating it, combining several focus planes into one image that is sharp throughout. Tilting reveals sidewalls and notches hidden from above, and switching between bright field and dark field brings out different features. Only if this first analysis doesn't give a sufficient answer should the part be cut for a cross-section. The VHX Series digital microscope is capable of non-destructive inspection with it's ability to tilt and rotate around a sample, switch between lighting settings, and automatically save all settings and measurements with an image.
Q How can I tell whether a defect is buildup or chipping?
A
In a two-dimensional, front-lit image, a deposit and a chip often look alike. 3D capture adds height information and shows clearly, as a profile section or color height map, whether the spot is raised or recessed. That lets you document the cause unambiguously in a complaint investigation.
Q Does microscope image documentation hold up in a complaint investigation?
A
It supports the investigation when it is traceable, repeatable, and unaltered. That means scale, magnification, lighting type, and date on every image, visible measurement geometry on every measured value, stored capture settings for later repetition, and the original image preserved. Documentation built this way can be reproduced identically, unlike a measurement taken by hand on a stereo microscope. The VHX series digital microscope automatically documents image settings, measurements, and analysis findings at the click of a button.
Q When do I need a 3D optical profiling microscope for failure analysis?
A
As soon as the assessment turns into a measurement against a limit value. A VK-X Series 3D optical profiling microscope makes sense for height and depth differences at the nanometer-to-micrometer scale, roughness parameters such as Ra, Rz, or Sa, or very shiny and curved surfaces. To simply image the damage and clarify its cause, a digital microscope is often enough.
Q Can you identify deposits on a damaged part?
A
Yes. With the optional elemental analysis on the VHX Series digital microscope, you select the deposit in the image and analyze its elements at the instrument, with no need to prepare or ship the sample. That separates corrosion products from manufacturing residue, for example, and speeds up finding the cause considerably.
Q How do I compare a suspect supplier part with a reference part?
A
Image both parts under identical lighting, magnification, and orientation, then compare marking, characteristic dimensions, surface condition, and, where needed, material through elemental analysis. Different capture conditions create apparent differences and ruin the comparison, so record the conditions in the report to keep the comparison traceable.