Gap measurement between rollers

The LS-9000 Series can measure the gap between the photoconductive drum and the transfer roll. Conventionally, this has been measured with a thickness gauge and a reflective type displacement sensor, but these measurements required more time and effort. It was difficult to perform measurements with micrometers due to the influence of outer diameter fluctuations. With the LS-9000 Series, the user only has to set the workpiece in the jig to easily perform measurements.

High-speed optical micrometer

LS-9000 series

Back to "Product Selection by Industry and Application"