Grooved sleeve deflection and outer diameter measurement

The outer diameter and deflection of sleeves are incredibly important measurements that have an effect on the amount of toner that is transferred. Also, with conventional laser scan types, there were times when the measured value was not stable due to the effect of the diffuse reflection caused by the groove. The TM Series uses dual telecentric lenses, which enable stable measurements.

High-speed 2D Optical Micrometer

TM-3000 series

Back to "Product Selection by Industry and Application"