Checking of adapter type
-
Industry:
- Automotive, Electronic Devices
-
Products:
- Machine Vision
The positive and negative sides of the adaptor being reversed will cause defective soldering, so it is necessary to check in advance. Adapters are made of glossy materials and if their positions are slanted, the laser sensor will not be able to detect them stably. The image sensor, which is equipped with a unique AI learning function, is unaffected by the workpiece’s position or environment and can be easily configured. Stable detection is possible even when the adapter position changes.