Inductive Noise Troubleshooting: How to Prevent Sensor and PLC Malfunctions Near Inverters
Key Takeaways
- Inverters and AC servos generate switching noise that can induce unwanted signals in nearby cables.
- Inductive noise can cause sensor malfunctions, unstable analog readings, communication errors, and intermittent PLC issues.
- Installing ferrite cores on sensor cables can help reduce noise.
- Increasing the distance between noise sources and signal cables can significantly minimize interference.
- Proper cable routing and noise prevention should be considered early in machine design and troubleshooting.
What Is Inductive Noise?
Have you ever experienced a sensor that occasionally misses a detection, an analog signal that fluctuates unexpectedly, or a PLC input that seems to trigger for no apparent reason?
In many industrial environments, the root cause is not a faulty sensor or controller—it is electrical noise.
Inductive noise is commonly generated by equipment such as:
- Variable frequency drives (VFDs)
- Inverters
- AC servo systems
- High-power motors
These devices rapidly switch power on and off to control motor operation. While this switching is essential for performance, it creates electrical noise that can travel through nearby wiring and interfere with connected devices.
Common Symptoms of Inductive Noise
Noise-related problems can be difficult to diagnose because they often appear sporadically.
Typical symptoms include:
Sensor Malfunctions
- False triggers
- Missed detections
- Unstable measurements
Analog Signal Instability
- Fluctuating voltage outputs
- Incorrect analog input values
- Drifting measurements
PLC and Control Issues
- Unexpected input activation
- Communication interruptions
- Random system faults
If these issues occur only when motors, inverters, or servos are operating, inductive noise may be the cause.
How Inductive Noise Affects Industrial Systems
When an inverter controls a motor, switching noise is created and can be coupled into nearby signal wiring.
For example:
- An inverter power cable runs beside a sensor cable.
- Electrical noise is induced onto the sensor signal.
- The PLC receives a distorted signal.
- The system reacts incorrectly.
This type of interference is especially problematic for low-voltage analog signals and high-speed sensing applications.
Solution 1: Install Ferrite Cores on Sensor Cables
One of the simplest and most effective noise countermeasures is a ferrite core.
Ferrite cores work by suppressing high-frequency noise traveling along a cable. When installed on a sensor cable, they can help prevent noise from reaching the control system.
Does the Number of Turns Matter?
Yes.
Increasing the number of times the cable passes through the ferrite core improves noise reduction performance. Multiple turns effectively increase the suppression effect without requiring multiple ferrite devices.
Best Practice
- Install ferrite cores as close as possible to the vulnerable device.
- Increase cable turns through the ferrite core when practical.
- Select a ferrite core suitable for your cable size and application.
Solution 2: Separate Power and Signal Wiring
Another highly effective countermeasure is physical separation.
Increasing the distance between noise sources and signal cables reduces the effects of inductive noise. When signal wiring is routed directly alongside inverter or motor power wiring, interference becomes much more likely.
Good Wiring Practices
Avoid:
- Running sensor cables parallel to motor power cables
- Bundling control wiring with high-current wiring
- Routing analog signals alongside inverter outputs
Instead:
- Separate signal and power wiring whenever possible
- Cross power and signal cables at 90-degree angles when they must intersect
- Use dedicated cable trays or raceways for control wiring
Troubleshooting Checklist for Inductive Noise
If you're experiencing intermittent sensor or control issues, work through the following checklist:
Check Nearby Equipment
- Are inverters, VFDs, or servo drives operating nearby?
- Do problems occur only when motors are running?
Inspect Cable Routing
- Are signal cables routed next to power cables?
- Can wiring be separated?
Add Noise Suppression
- Install ferrite cores on signal cables.
- Increase the number of cable turns through the ferrite core.
Validate the Results
- Test the system under normal operating conditions.
- Compare signal stability before and after implementing changes.
Because every installation environment is different, noise reduction effectiveness should always be verified on the actual machine.
Reduce Noise Before It Becomes a Problem
Inductive noise is one of the most common causes of intermittent automation issues. Fortunately, the solution is often straightforward.
By combining proper cable routing with proven noise suppression methods such as ferrite cores, manufacturers can improve system reliability, reduce downtime, and eliminate difficult-to-diagnose control problems. Whether you're troubleshooting an existing machine or designing new equipment, addressing inductive noise early can prevent costly production issues later.
Frequently Asked Questions about Inductive Noise
Q What causes inductive noise in industrial equipment?
A
Inductive noise is typically generated by switching devices such as inverters, servo drives, and variable frequency drives (VFDs). These devices rapidly switch power to motors, creating electromagnetic interference that can affect nearby wiring.
Q Can inductive noise cause sensor failures?
A
While inductive noise may not physically damage a sensor, it can cause false readings, missed detections, unstable measurements, or communication issues that appear similar to a sensor failure.
Q How do ferrite cores reduce noise?
A
Ferrite cores absorb and suppress high-frequency electrical noise traveling through cables. This helps prevent interference from affecting connected devices.
Q How much distance should be maintained between power and signal cables?
A
The required distance depends on factors such as voltage, current, cable shielding, and the application. In general, increasing separation between power and signal wiring reduces the likelihood of electrical interference.
Q Which devices are most susceptible to inductive noise?
A
Analog devices, sensors, communication networks, PLC inputs, measurement systems, and other low-voltage electronic components are often more susceptible to electrical noise.