Invest in In-House Measurement Equipment or Use an External Lab? How to Choose

Whether a company does its measuring in-house or sends it to an external lab is not an either-or question. It is a question of the right split. As a rule of thumb, measurements that steer process decisions on a daily or hourly basis belong in-house. Reference measurements, calibrations, and rarely needed specialty methods are most efficiently done by an external lab, ideally an accredited one. The decision comes down to five criteria: turnaround time, cost per measurement as volume grows, confidentiality, flexibility, and the need for formal accreditation. This article goes through the criteria one by one, shows why modern optical measurement systems have lowered the barrier-to-entry for in-house measuring, and describes the hybrid model that has proven itself in practice.

Want to know how this could work in your production? Talk to one of our experts.

Key Takeaways

  • This is not an either-or question but a question of how to split the work: keep process-relevant measurements in-house, bring reference work to a lab.
  • The most important criterion is turnaround time. A result that arrives days later can no longer be used to help course-correct the current manufacturing process.
  • In-house pays off once the external cost per measurement x your annual volume exceeds the cost of your own equipment.
  • An external lab remains the right choice for accredited proof, rarely needed specialty methods, and the highest reference accuracy.
  • Modern optical systems have lowered the barrier-to-entry for in-house measuring, and a hybrid model has proven itself.

Why Is Turnaround Time the Most Important Factor?

Turnaround time is the most important factor because a measurement result that arrives days later cannot assist in diagnosing immediate problems in your current production process. It only documents what has already been produced. If you outsource measuring, you add packaging, shipping, the lab's queue, and report writing to the actual measuring time. Production keeps running in the meantime. If the process has drifted, several days of production may need to be scrapped or require rework by the time the report arrives.

In-house measuring shortens that loop to minutes. A suspicious first article, a tool correction, or a startup can be checked and adjusted right away. That is why the first question to ask is not "What does the measurement cost?" but "What decision is waiting on this result, and how expensive is the wait?" The more closely a measurement result is tied to a running process decision, the stronger the case for doing it in-house.

When Does In-House Measurement Pay Off?

In-house measurement pays off once the running cost of each external measurement multiplied by your annual volume exceeds the depreciation, maintenance, and staff time of your own equipment. With regular measuring needs, that point often comes sooner than expected when looking at the cost of measuring devices. External measurements scale linearly: every additional measurement costs another fee, more shipping, and more waiting. Your own systems scale on a declining curve. After the investment, the marginal cost per measurement drops to just labor and operating costs.

Here is an example. If an external measurement costs $150 including handling, and you need 20 measurements a week, that adds up to about $144,000 a year over 48 working weeks. That is service cost alone, without the value of the lost time. It is the benchmark to compare against the annual cost of your own measuring setup, including the operator's share. The calculation also has to include the in-house side costs: training, maintenance, climate control where needed, and regular monitoring of the measuring equipment.

Two more effects can't be put into numbers but are real. One is confidentiality: new developments and complaint-critical parts can't leave the building. The other is skill building. When you measure yourself, you understand your processes and tolerances better and can talk to customers and suppliers on equal terms.

In-House Measurement vs. External Lab: A Comparison

Criterion In-house measurement External lab
Turnaround time
In-house measurement
Minutes to hours
External lab
Days to weeks, including shipping and queue
Cost at high volume
In-house measurement
Declining; marginal cost falls
External lab
Linear; every measurement costs the same for each part
Cost at rare need
In-house measurement
You have a high inspection cost per part that is inefficient compared to a lab
External lab
Economical; no fixed costs
Confidentiality
In-house measurement
Parts and data stay in the building
External lab
Confidentiality must be settled by contract
Flexibility
In-house measurement
Immediate repeat and extra measurements
External lab
Every change is a new order and added cost
Accredited results
In-house measurement
Only with your own accredited lab
External lab
Labs accredited to ISO/IEC 17025 provide recognized proof
Specialty methods (such as CT or materials analysis)
In-house measurement
Only makes sense with enough utilization
External lab
Access to specialty equipment without the investment
Skill building
In-house measurement
Measurement know-how grows in your own team
External lab
Knowledge stays with the service provider

When Does the External Lab Become the Right Choice?

An external lab is the right choice when formally recognized proof, rarely needed specialty methods, and/or the highest reference accuracy are called for. Specifically:

  • Accredited proof. When customers, regulators, or disputes require results from a lab accredited to ISO/IEC 17025 (in the U.S., through accreditation bodies such as A2LA or ANAB), internal measuring equipment doesn't replace that proof, no matter how well it measures.
  • Calibration. It makes sense to trace your own measuring equipment back to national standards (NIST in the U.S.) through accredited calibration labs. Your own team measures for production, and the lab makes sure those measurements stay traceable.
  • Rare specialty methods. Computed tomography, reference roughness measurements, materials analysis, or first article inspection of exotic features rarely justify your own investment if they only come up a few times a year.
  • Referee measurements. When a customer and a supplier disagree on results, an independent, accredited lab provides the neutral party that internal measurements can't be in principle.

Has the Barrier-to-Entry Changed for In-House Measurement?

Yes. The barrier-to-entry has historically been the strongest argument against bringing your measurements in-house, but modern optical systems have lowered that barrier significantly. Traditional coordinate measuring requires trained metrologists for programming, fixturing, and evaluation. That staff is scarce, and operating errors show directly in the results.

With modern optical measurement systems and machine vision systems, much of that complexity is built into the system. Parts are placed with little alignment effort, measurement programs run automatically, and the dependence of results on the specific operator drops. An operator on the production floor can run measurements that once required being performed in a measuring room. That shifts the economic break-even point. Tasks that used to go outside for lack of staff are realistic to do in-house today. A proper rollout is still a requirement, including a measurement system analysis (MSA/GR&R), defined inspection instructions, and traceability through regular calibration. For an example, see this case study on bringing measurement in-house.

What Does the Proven Hybrid Model Look Like?

The proven hybrid model is this: routine measurements tied to the process stay in-house, and reference and calibration work goes outside to the accredited lab. In practice, that means:

  • In-house: measurements that accompany production, first articles in daily operation, tool corrections, startup support, and quick complaint analysis. In short, everything that needs fast feedback and comes up regularly.
  • External: calibration of your own measuring equipment, accredited proof for customers and regulators, referee measurements, and rare specialty methods.
  • Linking the two. Reference parts that were measured precisely outside serve as control standards inside. Regular comparison measurements confirm that your in-house systems measure correctly for their task.

Used this way, the two paths don't compete. They support each other. The external lab secures traceability, and your own measuring equipment delivers the speed for everyday production.

Frequently Asked Questions

Q Do I need accreditation for internal measurements?

A

No. Internal process and quality decisions don't require accreditation. What matters is a capable measurement system, shown for example through MSA/GR&R, and calibrated, traceable measuring equipment. Accreditation to ISO/IEC 17025 only becomes relevant when you want to use measurement results as formally recognized proof for third parties.

Q What does it mean for a lab to be accredited?

A

An accredited lab has been assessed by an accreditation body, such as A2LA or ANAB in the U.S., and confirmed to meet the ISO/IEC 17025 requirements for competence and quality assurance. Customers and regulators recognize results from an accredited lab as independent, reliable proof. For calibrations and referee measurements, that is the usual standard.

Q At what measurement volume does your own equipment pay off?

A

There is no fixed number. Compare the annual cost of outsourcing (fees, shipping, internal handling time) with the depreciation, maintenance, and staff share of your own solution, and also, put a price on the cost of waiting. In practice, the math often tips toward in-house at a regular weekly measuring need, especially when measurement results steer running processes.

Q Can an operator without metrology training measure reliably?

A

With modern optical measurement systems, in many cases yes, because alignment, measuring sequence, and evaluation are largely automated and the dependence on the operator is correspondingly low. The prerequisites are a properly built measurement program, a measurement system analysis at the point of use, and clear inspection instructions. For creating new programs and judging difficult features, measurement expertise in-house is still worthwhile.

KEYENCE can help you decide which measurement tasks to bring in-house economically, from image dimension measurement systems and digital microscopes to laser profilers, including feasibility tests on your real parts. Request a consultation with our measurement experts.

Related Products

Related Downloads