Pneumatic Components Video Manuals

Applicable models: CS-L / SP-C / SP-N / SP-V

We've compiled a video manual that clearly explains installation and wiring methods, as well as tips for pre-use setup.
This video manual will support you in resolving issues from installation to maintenance.

CS-L Series

Standard/Dual type

Cylinder Sensor Installation

Installation on round cylinders

Installation on CKD T-slot cylinders

Installation on tie rod cylinders

Cylinder Sensor Replacement

How to Teach the Sensor

How to Key Lock

USB Type-C Cable

Setting the 3rd Output

Changing the Output Width

Three Status Indicators

Gripper model

Installing the Cylinder Sensor

How to Use the T-Slot Conversion Bracket

How to Use the Plate Bracket

How to Configure the Sensor​

Configuring the Sensor via Panel​

Distinguish Between Workpieces

SP-C Series

Operation support video

Smart Cushion Valve - Piping and Wiring

Smart Cushion Valve How to Use the Bracket

Smart Cushion Valve Smart Guided Settings

Smart Cushion Valve Manual settings

Auto Stroke Control ~ Fixed stroke time ~

Smart Cushion Valve Valve Replacement Procedure

Performance verification

Smart Cushion Valve
~Speed Increase and Impact Reduction~

Smart Cushion Valve With vs. Without

SP-N/V Series

Operation support video

Unit Assembly (Screw Type)

Unit Assembly (Cam Lock Type)

Installing the Supply-Exhaust Unit Option

Setup Procedure for the External Manifold Connection Unit

Connection to the IO Unit

How to Configure Warnings

Predictive Maintenance Settings

Configuring Sensors from the Panel

How to Assemble the Connector

Settings Backup Procedure

Setting Write Procedure

Web Server Connection Procedure

Functionality

Registering a Reference State and Setting Warnings

Checking Each Parameter During Operation

Quickly Identify the Source When a Warning-Error Occurs

Valve Operation on the Panel

Adjust While Checking Speed and Time

Web Server

Performance verification

Value of Distributed Manifold

Product Lineup: