Non-Contact Measurement of Steel Sheet Thickness: Inline Measurement Using Coaxial Lasers on Both Sides
Non-contact measurement of steel and metal sheet thickness using the CL-3000 Series confocal displacement sensor. With a dual-head sandwiching configuration and optical axis alignment functions, thickness variations on rolling, straightening, and cutting lines are managed inline.
Three Reasons Why Thickness Measurement of Steel and Metal Sheets Is Difficult
Thickness variations directly affect strength, flatness, and formability in subsequent processes. Choosing the wrong measurement method leads to defects and losses.
Thickness Variation Directly Affects Quality and Yield Rate
If the thickness of steel and metal sheets varies, strength, flatness, and formability in subsequent processes become non-uniform, leading to winding defects, out-of-dimension issues, and complaints. In rolling and straightening, slight fluctuations in forming conditions appear as thickness unevenness, requiring management in both the width and longitudinal directions. Without stable thickness management, yield rates decrease and rework increases.
Limitations of Contact, Ultrasonic, and Beta-Ray Methods on Site
Contact methods such as calipers and micrometers make continuous measurement while moving difficult, resulting in measurement marks and reading errors. Ultrasonic thickness gauges are affected by couplants and surface conditions, and while the beta-ray method is non-contact, the reality is that it has high operational hurdles, requiring radiation source management, qualified personnel, and controlled areas. There is a need for a measurement method that can keep up with production speeds without being affected by regulations or contact.
Metallic Luster, Slant, and High-Speed Lines Make Measurement Difficult
Steel sheets have large variations in luster and reflectance, and with general laser triangulation, the detection position shifts, making errors more likely to occur. Furthermore, fluttering and slanting while moving, as well as high temperatures and vibrations on rolling lines, also make measurement difficult. A measurement principle that is less affected by target slant, steps, and glossy surfaces, along with the ability to keep up with high-speed conveying, is required.
Each Process of Steel and Metal Sheet Manufacturing and Thickness Measurement Points
By understanding the thickness in each process from rolling to shipping inspection, variations and defects can be detected at an early stage.
- 1 Rolling – Thickness measurement (1). The process of forming the thickness with rolls. The thickness is measured, and the roll gap and tension are fed back to converge to the target thickness.
- 2 Straightening/Leveling – Thickness measurement (2). The process of straightening warpage and waviness. The thickness before and after straightening is measured without contact to detect over-straightening and unevenness.
- 3 Cutting/Slitting – Thickness measurement (3). The process of cutting to specified dimensions. The thickness before and after cutting is checked to determine if it is within standard tolerances, preventing missed thickness measurements.
- 4 Shipping Inspection – Thickness measurement (4). Thickness profiles are acquired across the entire length and width. Synchronized measurement with up to 6 heads captures the distribution in the width direction, ensuring standards and traceability.
Comparison of Thickness Measurement Methods for Steel and Metal Sheets
Depending on the measurement method, there are large differences in non-contact capability, compatibility with glossy surfaces, legal regulations, and inline adaptability.
| Comparison Items | CL-3000 Series (Multi-color laser confocal, coaxial, non-contact) |
Micrometer (contact) | Ultrasonic thickness gauge (contact) | Beta-ray method |
|---|---|---|---|---|
Non-contact/Influence on target |
CL-3000 Series (Multi-color laser confocal, coaxial, non-contact)
○ Non-contact with no measurement marks
|
Micrometer (contact)
× Contact may cause measurement marks or local deformation
|
Ultrasonic thickness gauge (contact)
× Contact and coupling medium required
|
Beta-ray method
○ Non-contact
|
Resistance to metallic luster and tilted surfaces |
CL-3000 Series (Multi-color laser confocal, coaxial, non-contact)
○ Coaxial measurement is resistant to luster, tilt, and steps
|
Micrometer (contact)
△ Difficult to operate on large tilts, steps, or curved surfaces
|
Ultrasonic thickness gauge (contact)
△ Dependent on surface conditions
|
Beta-ray method
△ Dependent on material and density
|
Radiation and regulatory requirements |
CL-3000 Series (Multi-color laser confocal, coaxial, non-contact)
○ Not required
|
Micrometer (contact)
○ Not required
|
Ultrasonic thickness gauge (contact)
○ Not required
|
Beta-ray method
× Radiation source management, qualified personnel, and controlled areas are required
|
Inline continuous measurement |
CL-3000 Series (Multi-color laser confocal, coaxial, non-contact)
○ High-speed sampling allows measurement while moving
|
Micrometer (contact)
× Basically manual single-point measurement. Automation requires jigs or mechanisms.
|
Ultrasonic thickness gauge (contact)
× Not suitable for running lines
|
Beta-ray method
○ Possible
|
Multi-point/full-width measurement |
CL-3000 Series (Multi-color confocal, coaxial, non-contact)
○ Synchronous measurement of up to 6 heads with 1 controller
|
Micrometer (contact)
× Low practicality due to the need for mounting measurement jigs and scanning mechanisms
|
Ultrasonic thickness gauge (contact)
× Difficult
|
Beta-ray method
△ Large-scale scanning mechanism required
|
Measurement range (reference distance) |
CL-3000 Series (Multi-color confocal, coaxial, non-contact)
○ Select from a reference distance of 7 to 150 mm and a measurement range of ±1 to ±35 mm
|
Micrometer (contact)
△ Narrow range but high accuracy and high resolution
|
Ultrasonic thickness gauge (contact)
○ Compatible with thick materials
|
Beta-ray method
△ Range is determined by the radiation source
|
Reasons to Choose the CL-3000 Series
The CL-3000 Series uses multi-color confocal coaxial measurement, making it less susceptible to the effects of metal luster, tilt, and steps, and stably measures the thickness of steel and metal plates without contact. It suppresses thickness measurement errors with a dual-head sandwiching configuration and optical axis alignment function, and eliminates the need for radiation control. This enables inline plate thickness management while overcoming the limitations of contact and beta-ray methods.
CL-3000 Series for Steel and Metal Plate Thickness Measurement
With multi-color confocal coaxial measurement, this displacement sensor is highly resistant to glossy surfaces, tilt, and steps, making it ideal for measuring the thickness of steel and metal plates.
Compatible With Steel and Metal Plate Thickness Measurement - CL-3000 Series
Confocal Displacement Sensor
The multi-color confocal method measures the distance to the target coaxially. Because of the coaxial method, the measurement position does not shift even if the height changes, enabling stable measurement regardless of the material, even on metallic glossy surfaces, rough surfaces, or targets with tilts or steps. The plate thickness is calculated as “Reference Distance - (Upper Distance + Lower Distance)” by sandwiching the target between two heads. The dedicated jig and the optical axis alignment function (3 steps) of the PC software suppress errors caused by optical axis misalignment during sandwiching. The CL-S015 thickness measurement head features a zero-heat-generation structure and an athermal optical design, ensuring stable sub-micron measurement even when the ambient temperature changes, when mounted with a SUS jig. Up to 6 heads can be synchronously controlled with a single controller, allowing the thickness distribution in the plate width direction to be acquired. With sensor heads that can withstand heat up to 200°C and explosion-proof heads, it is also suitable for rolling lines and high-temperature/explosion-proof environments.
Get Detailed Materials on the CL-3000 Series
You can download a free catalog summarizing specifications, system configuration, and case studies.
Application Examples of Plate Thickness Measurement for Steel Plates and Metal Sheets
The CL-3000 Series is used for plate thickness measurement in various metal sheet processes, such as rolling, straightening, and cutting.
Non-Contact Thickness Measurement of Rolled Steel Plates
Measures steel plate thickness without contact. The athermal design minimizes the effects of ambient temperature, allowing easy and highly accurate plate thickness measurement even on rolling and transfer lines.
Thickness Distribution Measurement of Metal Foil
Using ultra-compact sensor heads with an outer diameter of 8 mm, thickness distribution measurement is performed in a space-saving manner through fully synchronized measurement of six sensor heads.
Plate Thickness Measurement on High-Temperature and Harsh-Environment Lines
With the 200°C heat-resistant head (CL-V) and athermal design, measurement values are less likely to fluctuate even on rolling and hot lines with large temperature changes, ensuring stable measurement.
Frequently Asked Questions About Plate Thickness Measurement of Steel Plates and Metal Sheets (CL-3000 Series)
Q Can plate thickness be measured even on glossy surfaces like steel plates?
A
Yes, it can. The multi-color confocal coaxial measurement method is less susceptible to the effects of metal gloss, tilt, and steps, allowing stable measurement of distance and plate thickness even on steel plate surfaces with fluctuating reflectance.
Q Can it replace contact-type or ultrasonic plate thickness gauges?
A
Yes, it can. Because it is non-contact, there are no measurement marks, and continuous measurement while moving is possible. Without depending on couplants or operator skill, you can transition to 100% inline plate thickness management.
Q How is the plate thickness calculated?
A
The target is sandwiched between two heads, and the plate thickness is calculated as "reference distance - (upper surface distance + lower surface distance)". The optical axis alignment function minimizes optical axis misalignment errors during sandwiching.
Q Can it be used in high-temperature environments such as rolling lines?
A
Yes, it can. With the 200°C heat-resistant head (CL-V) and athermal design (temperature compensation with SUS mounting), measurement values are less likely to fluctuate even on lines with large temperature changes, ensuring stable measurement.
Q Can multiple locations on a plate be measured simultaneously?
A
Yes, they can. A single controller can synchronously control all heads, and simultaneous measurement of up to six heads allows collective management of the plate thickness distribution in the width direction.
Q What is the measuring range (the range of plate thickness that can be measured)?
A
You can select by head model number. With a lineup of reference distances from 7 to 150 mm and measuring ranges from ±1 to ±35 mm, you can select according to the target and line configuration.
Q Please feel free to contact us regarding challenges in plate thickness measurement of steel plates and metal sheets
A
Measurement methods, installation configurations, and specifications can be confirmed in the catalog or via the inquiry form.