Non-Contact Measurement of Sheet Thickness: High Accuracy Without Optical Axis Misalignment Even in Dual-Sided Measurement
Measure the thickness of rubber sheets, urethane, and green sheets without contact using a multi-color confocal coaxial displacement sensor. The optical axis alignment function reduces errors in dual-sided measurement and enables inline management of continuous extrusion, calendering, and winding processes.
Three Reasons Why Sheet Thickness Measurement Is Difficult
Thickness variation in rubber, urethane, and green sheets directly affects strength, quality, and yield. Choosing the wrong measurement method leads to defects and losses.
Thickness Variation Directly Affects Quality and Yield
If sheet thickness varies, strength, insulation properties, and coating amount become non-uniform, causing processing defects in subsequent processes and variations in product performance. In extrusion and calendering, unevenness easily occurs in both the width and flow directions, and out-of-specification lots must be discarded entirely. In continuous production, a measurement method is required that can detect thickness variations on the order of several micrometers during operation and immediately reflect them in the operating conditions.
Limitations of Contact and Beta-Ray Methods on-Site
Contact methods such as micrometers make continuous measurement during operation difficult, and pressing them against soft rubber or urethane causes deformation and scratches. Although the beta-ray method is non-contact, it requires radiation source management, qualified personnel, and controlled areas, making the hurdles for introduction and operation high in reality. There is a need for a method that can measure without being affected by regulations or contact while keeping up with production speeds.
Black Rubber, Transparent Sheets, and Rough Surfaces Are Difficult to Measure
Black rubber absorbs light, and transparent/semitransparent sheets have mixed reflections from the front and back surfaces, making stable measurement difficult with general displacement sensors. With milky white resin or rough surfaces, the reflected light scatters, causing the measured values to fluctuate. Furthermore, when measuring from both sides by sandwiching, even a slight misalignment of the optical axes of the two sensors causes sheet fluttering or tilting to appear as large errors.
Each Process of Continuous Sheet Production and Thickness Measurement Points
By understanding the thickness in each process from extrusion to winding, thickness unevenness and defects can be detected at an early stage.
- 1 Kneading and extrusion – Thickness measurement (1). Raw materials are kneaded and continuously extruded into a sheet from a die. The total thickness immediately after extrusion is measured to provide immediate feedback on the discharge rate, reducing loss during startup.
- 2 Calendering (rolling) – Thickness measurement (2). The sheet is rolled to a specified thickness using rolls. The thickness after rolling is measured by sandwiching to adjust the roll gap and detect thickness unevenness caused by uneven wear on one side.
- 3 Drying and curing – Thickness measurement (3). The sheet is stabilized by solvent evaporation, vulcanization, or curing. The thickness after treatment is checked to manage dimensional changes due to shrinkage or swelling within reference values.
- 4 Winding and slitting – Thickness measurement (4). The sheet is cut to a specified width and wound. The final thickness before shipment is checked without contact to prevent the outflow of out-of-specification lots and guarantee quality.
Comparison of Sheet Thickness Measurement Methods
Depending on the measurement method, there are significant differences in non-contact properties, legal regulations, compatibility with difficult materials, dual-sided measurement accuracy, and inline suitability.
| Comparison items | CL-3000 Series (Multi-color Confocal/Coaxial) |
Beta-ray method | Contact method (micrometer, etc.) |
|---|---|---|---|
Non-contact / Impact on target |
CL-3000 Series (Multi-color Confocal/Coaxial)
○ Non-contact, no scratches or deformation
|
Beta-ray method
○ Non-contact
|
Contact method (micrometer, etc.)
× Deformation/scratches due to pressing
|
Radiation and regulatory requirements |
CL-3000 Series (multi-color confocal/coaxial)
○ Not required
|
Beta-ray method
× Radiation source management, qualified personnel, and controlled areas required
|
Contact method (micrometer, etc.)
○ Not required
|
Black rubber, rough surfaces, milky white resin |
CL-3000 Series (multi-color confocal/coaxial)
○ Stable measurement with Quad processing
|
Beta-ray method
△ Dependent on density and material
|
Contact method (micrometer, etc.)
△ Supported by pressing
|
Measurement of transparent/semitransparent sheets |
CL-3000 Series (multi-color confocal/coaxial)
○ Separate measurement of front and back surfaces (from 15 µm)
|
Beta-ray method
△ Dependent on density and material
|
Contact method (micrometer, etc.)
× Difficult
|
Thickness measurement by sandwiching (both sides) |
CL-3000 Series (multi-color confocal/coaxial)
○ Optical axis alignment function reduces errors
|
Beta-ray method
△ Transmission arrangement required
|
Contact method (micrometer, etc.)
△ Single-sided contact only
|
Inline continuous measurement |
CL-3000 Series (Multi-color confocal/coaxial)
○ Measurement during travel is possible with high-speed sampling
|
Beta-ray method
○ Possible
|
Contact method (micrometer, etc.)
× Stopping required
|
Stability against temperature changes |
CL-3000 Series (Multi-color confocal/coaxial)
○ Athermal design minimizes the effects
|
Beta-ray method
△ Depends on configuration
|
Contact method (micrometer, etc.)
△ Depends on configuration
|
Why Choose the CL-3000 Series
The CL-3000 Series uses a multi-color confocal method that does not require radiation control, and measures difficult-to-measure sheets such as black rubber, transparent sheets, and rough surfaces with high accuracy without contact. The optical axis alignment function suppresses optical axis misalignment errors even during opposed measurement, and the athermal design suppresses the effects of temperature changes. While eliminating the limitations of beta-ray and contact methods, it enables inline thickness management for extrusion, calendering, and winding.
CL-3000 Series for Sheet Thickness Measurement
This coaxial displacement sensor uses the multi-color confocal method and is suited for sheet thickness measurement of various surface conditions, such as black rubber, transparent sheets, and rough surfaces.
Sheet Thickness Measurement - CL-3000 Series
Confocal Displacement Sensor
The multi-color confocal method and Quad processing system enable high-accuracy measurement with a single unit regardless of surface condition or material, including black rubber, transparent materials, rough surfaces, and milky white resin. The thickness measurement model CL-S015 has a resolution of 0.003 µm and linearity of ±0.1 µm (high-accuracy range). Thanks to the athermal optical design, measured thickness values barely change even if the ambient temperature changes. The optical axis alignment function suppresses optical axis misalignment errors during opposed measurement, minimizing the effects of flapping and tilting. The dedicated adjustment jig OP-88864 is fully made of stainless steel (SUS) and is compatible with dry clean rooms, allowing close installation down to a 50 mm pitch. The controller CL-3050 can synchronously measure up to 6 heads, enabling collective thickness management for multiple points in the sheet width direction and both sides.
Get Detailed Materials on the CL-3000 Series
You can download the catalog containing specifications, system configuration, and case studies for free.
Examples of Sheet Thickness Measurement Applications
The CL-3000 Series is used in thickness measurement of various sheets, such as rubber, polyurethane, green sheets, and metal sheets.
Opposed Thickness Measurement of Rubber and Polyurethane Sheets
By sandwiching the sheet between two heads, the optical axis alignment function suppresses errors caused by optical axis misalignment. Even if the sheet flutters, the thickness after calendering can be measured with high accuracy and without contact.
Thickness Measurement of MLCC Green Sheets
Measures the thickness of the PET base material and the coated dielectric layer with a spot diameter of ø3.5 µm. The adjustable jig for sandwiching measurement enables ultra-high accuracy thickness measurement of green sheets.
Thickness Measurement of Steel Plates and Metal Sheets
Measures the thickness of steel plates without contact. The athermal design, which suppresses the effects of ambient temperature, enables easy and high-accuracy thickness measurement.
Frequently Asked Questions About Sheet Thickness Measurement (CL-3000 Series)
Q Can black rubber or milky white sheets also be measured?
A
Yes, they can. The multi-color confocal method and Quad processing system enable stable, high-accuracy measurement regardless of the material, such as black rubber, milky white resin, or rough surfaces, by suppressing the effects of minute surface irregularities.
Q Can thickness be measured by sandwiching the sheet?
A
Yes, it can. It supports double-sided measurement by sandwiching the sheet between two heads. The optical axis alignment function accurately aligns the optical axes of both heads, suppressing errors caused by sheet fluttering or tilting to measure thickness with high accuracy.
Q Can it replace beta-ray systems?
A
Yes, it can. Because the multi-color confocal method does not use a radiation source, controlled areas and qualified personnel are not required. High-accuracy inline thickness measurement can be continued without contact.
Q Can the thickness of transparent or translucent sheets and films also be measured?
A
Yes, they can. Because the multi-color confocal method can separate the reflected light from the front and back surfaces, the thickness of transparent and translucent objects from approximately 15 µm can be measured without contact.
Q Can multiple locations be measured simultaneously?
A
Yes. The CL-3050 controller can synchronously measure up to 6 heads, allowing collective management of multi-point and double-sided thickness in the sheet width direction. No programming on the PLC is required.
Q Can thickness be measured stably even if the ambient temperature changes?
A
Yes, it can. The CL-S015 thickness measurement model features an athermal optical design. When mounted using a jig made of the same SUS material as the sensor head, it is designed so that the measured thickness value barely changes even if the ambient temperature changes.
Q Please feel free to contact us regarding any challenges with sheet thickness measurement.
A
Measurement methods, installation configurations, and specifications can be confirmed in the catalog or via the inquiry form.