GS1 Sunrise 2027 Explained: Requirements, Timeline, and Preparation
GS1 Sunrise 2027 is changing how products are identified across the supply chain. As businesses transition from traditional 1D barcodes to GS1-compliant 2D barcodes, manufacturers and retailers must ensure their systems remain compatible throughout the transition.
This guide outlines what's changing, what it means for your operations, and how to prepare your production systems for compliance.
Timeline and Key Changes
GS1 Sunrise 2027 marks the transition to 2D barcodes as the new standard for retail point-of-sale. By the end of 2027, retailers are expected to be able to scan both traditional 1D barcodes and GS1-compliant 2D barcodes. During this transition period, manufacturers should support both barcode types to maintain compatibility across the supply chain. Common GS1-compliant 2D barcode formats include GS1 Data Matrix and GS1 QR Codes using GS1 Digital Link, depending on the application.
Why GS1 Sunrise 2027 Matters
2D barcodes can store more information, such as batch numbers, expiration dates, and serial numbers, within a smaller space. This improves traceability, product transparency, and supply chain visibility.
Who needs to prepare
Manufacturers, retailers, and logistics providers all need to update systems. Most importantly, manufacturers must ensure their production lines can reliably print and verify 2D barcodes.
What GS1 Sunrise 2027 means for your production line
- Existing printing systems may need upgrades or reconfiguration
- Product data must be prepared and standardized
- Barcode quality must meet industry grading standards
- Systems must support both 1D and 2D codes during the transition
Early evaluation helps avoid production delays and last-minute changes.
Why Printing Technology Determines GS1 Compliance Success
GS1 Sunrise 2027 is not just a data initiative; it depends on how reliably barcodes are printed and read in real production environments. Even with correct data, poor marking can lead to scan failures and compliance issues.
Print Quality and Barcode Scan Performance
Low contrast, smudging, or poor resolution can reduce barcode grading and cause scan failures at retail or in distribution.
Production speed and GS1 Implementation
Marking systems must keep up with line speeds while handling variable data. If printing cannot maintain performance, it can slow production or create inconsistencies.
Packaging Materials and Marking Technology
Different packaging materials require different marking methods. Selecting the right technology helps ensure codes remain readable throughout production, shipping, and retail handling.
Choosing the Right Marking and Coding Technology
Different technologies serve different production needs:
- Continuous inkjet supports high-speed lines and varied substrates
- Laser marking provides permanent codes on rigid materials
- Thermal solutions are suited for labels and flexible packaging
- Case coding supports higher resolution, large-format printing on corrugate
Selecting the right approach ensures reliable barcode quality without interrupting production.
Data Preparation and 2D Barcode Generation
Each product requires accurate and structured data before barcode generation. This typically includes:
- Product identification (GTIN)
- Batch or lot numbers
- Expiration dates
- Serial numbers (if required)
Well-prepared data helps ensure consistent barcode generation and reduces errors during implementation.
Barcode Verification and Quality Control
Barcode verification ensures that codes meet required quality standards before reaching the supply chain.
- Inline inspection checks every code during production
- Systems detect print or positioning issues in real time
- Failed codes can be corrected immediately
- Verification data supports compliance and traceability
This approach helps prevent defective barcodes from reaching retailers.
GS1 Sunrise 2027 Preparation Checklist
To ensure a smooth and successful transition of GS1 Sunrise 2027:
-
1.Assess current printing capabilities.
-
2.Determine which products require 2D barcodes.
-
3.Verify your data infrastructure.
-
4.Select the appropriate marking technology.
-
5.Implement inline verification.
-
6.Test with supply chain partners before deployment.
Conclusion
Preparing for GS1 Sunrise 2027 starts with understanding your current systems and making the right updates to your production process.
Reliable marking, accurate data, and effective verification work together to ensure successful implementation.
KEYENCE supports this process with integrated marking, verification, and inspection solutions designed to help maintain quality and compliance.
FAQs about Gs1 Sunrise 2027
Q Is GS1 Sunrise 2027 mandatory?
A
GS1 Sunrise 2027 is not a legal requirement, but it is a retailer-driven initiative. Manufacturers will need to comply to meet retailer expectations and maintain compatibility with point-of-sale systems.
Q What is the main goal of GS1 Sunrise 2027?
A
The goal is to introduce 2D barcodes at retail point-of-sale so businesses can store more product information, improve traceability, and support supply chain visibility.
Q Will 1D barcodes be eliminated?
A
Not immediately. During the transition, businesses will need to use dual marking by printing both 1D and 2D barcodes until all systems support 2D scanning.
Q Why is printing important for GS1 compliance?
A
Even with correct data, barcode readability depends on print quality. Poor marking, low contrast, or incorrect placement can lead to scan failures and impact compliance.
Q What changes are required on production lines?
A
Production lines may need updates to printing equipment, data systems, and verification processes to support 2D barcode generation and quality control.
Q When should businesses start preparing?
A
Preparation should begin as early as possible. Packaging updates, equipment changes, and data preparation can take significant time to implement before 2027.