Non-Contact Measurement of Glass Substrate Warpage: High-Accuracy Measurement of TTV and Flatness

The CL-3000 Series confocal displacement sensor performs non-contact measurement of warpage in glass substrates, cover glasses, and large panels. Combined with the SI-F Series, which uses the spectral interference method, it manages TTV and flatness with high accuracy.

View Catalog

Inquiries regarding glass substrate warpage and TTV measurement

Three Issues That Occur When Glass Substrate Warpage and TTV Cannot Be Measured Correctly

Warpage and thickness distribution (TTV) directly affect the yield rate of subsequent processes. Because transparent objects are difficult to measure, conventional methods have limitations on-site.

Warpage and Thickness Distribution Directly Affect the Yield Rate of Subsequent Processes

Warpage (Bow/Warp) and thickness distribution variation (TTV) of glass substrates, cover glasses, and wafers cause poor adhesion during bonding, film deposition, and transfer, as well as deformation and cracking during transfer. If not detected within the process, they manifest as defects in subsequent processes or final products, leading to material loss and complaints. Especially for large panels and thin glass, even slight warpage or deterioration in thickness distribution significantly pressures the yield rate and costs, making 100% surface inspection the key to quality.

Transparent Objects Are Difficult to Measure Because Reflections From the Front and Back Surfaces Mix.

Because reflection occurs on both the front and back surfaces of glass or coating films on glass, general displacement sensors mix the reflected light from both sides, making it impossible to stably obtain the height shape (warpage) of the target surface. If the front and back surfaces cannot be separated, warpage and thickness cannot be distinguished, reducing the reliability of the measured values.

Rough Surfaces, Mirror Surfaces, Tilt, and Contact Make Measurement Difficult.

Transparent objects have a mixture of mirror and rough surfaces, and differences in reflected light intensity, minute irregularities, and target tilt make measurements unstable. Contact-type methods and coordinate measuring machines (CMMs) measure at points and at low speeds, which can cause scratches and deformation, and their structure makes 100% inspection difficult.

Concept of Warpage and TTV Measurement

Warpage and thickness distribution (TTV) measure different characteristics. Measurements are performed using equipment suitable for each characteristic.

  1. 1 Define and separate warpage and thickness distribution – STEP 1. Warpage (Bow/Warp) is the waviness of the height shape of “one side” of the substrate, and TTV is the variation in thickness distribution. It is important to select equipment according to each measurement application.
  2. 2 Confocal Displacement Sensor CL-3000 Series – STEP 2. The multi-color confocal method accurately separates reflected light from the front and back surfaces, even for transparent objects. Select from a wide variety of sensor heads according to the installation environment.
  3. 3 Micro-head Spectral-interference Laser Displacement Meter SI-F Series – STEP 3. Using the spectral interference method, thickness and distance are measured with ultra-high resolution from the interference between light specularly reflected by the target and light from the reference surface inside the head.
  4. 4 Inline surface management at multiple points – STEP 4. Up to six sensor heads can be measured synchronously with a single controller, acquiring surface data at multiple points. Warpage and thickness distribution are managed inline within the process.

Comparison of Glass Substrate Warpage and TTV Measurement Methods

Depending on the measurement method, there are significant differences in front/back surface separation of transparent objects, warpage/thickness distribution measurement, non-contact, inline 100% inspection, etc.

Comparison items CL-3000 Series/SI-F Series (laser displacement, non-contact) Moire (grating projection) method Contact method (dial, stylus) Coordinate measuring machine (CMM)
Separation of front and back surfaces of transparent objects
CL-3000 Series/SI-F Series (laser displacement, non-contact)
○ Accurately separates reflected light from the front and back surfaces
Moire (grating projection) method
× Reflections from the front and back surfaces are easily mixed
Contact method (dial, stylus)
△ Contacts only one side
Coordinate measuring machine (CMM)
△ Probe contact on one side only
Warpage (one-sided height profile) measurement
CL-3000 Series/SI-F Series (laser displacement, non-contact)
○ Stable acquisition with the CL-3000 Series
Moire (grating projection) method
△ Error in height conversion
Contact method (dial, stylus)
△ Point measurement, slow
Coordinate measuring machine (CMM)
△ Highly accurate but slow/requires stopping
Thickness/thickness variation (TTV) measurement
CL-3000 Series/SI-F Series (laser displacement, non-contact)
○ High resolution with the SI-F Series
Moire (grating projection) method
× Cannot measure thickness
Contact method (dial, stylus)
△ Point measurement by clamping
Coordinate measuring machine (CMM)
△ Separate configuration required
Capability on rough, specular, and micro-uneven surfaces
CL-3000 Series/SI-F Series (laser displacement, non-contact)
○ Quad processing system eliminates the effects
Moire (grating projection) method
△ Depends on surface conditions
Contact method (dial, stylus)
× Risk of scratches/deflection
Coordinate measuring machine (CMM)
△ Probe, slow speed
Non-contact, 100% inline inspection
CL-3000 Series/SI-F Series (laser displacement, non-contact)
○ Non-contact, surface management with up to 6 synchronized units
Moire (grating projection) method
△ Depends on configuration and speed
Contact method (dial, stylus)
× Contact, stoppage, sample inspection
Coordinate measuring machine (CMM)
× Offline, slow speed
Role (area of expertise)
CL-3000 Series/SI-F Series (laser displacement, non-contact)
Warpage and thickness distribution of transparent objects (surface, non-contact)
Moire (grating projection) method
Understanding surface unevenness trends
Contact method (dial, stylus)
Point measurement of stationary surfaces
Coordinate measuring machine (CMM)
Offline precision measurement

Reasons to Choose the CL-3000 Series/SI-F Series

The CL-3000 Series uses the multi-color confocal method to separate reflected light from the front and back surfaces of transparent objects, stably acquiring the warpage of the target surface without contact. The SI-F Series uses the spectral interference method to measure the distance to the target and its thickness with ultra-high resolution. You can choose the model that best fits your installation environment and required accuracy.

CL-3000 Series/SI-F Series Supporting Warpage and TTV Measurement of Glass Substrates

With confocal displacement sensors that offer a choice of various installation distances and spectral interference laser displacement sensors capable of ultra-high resolution measurement of 1 nanometer, glass substrates can be measured without contact according to the application.

Supporting Warpage Measurement of Glass Substrates — CL-3000 Series

Confocal Displacement Sensor

The CL-3000 Series is a confocal displacement sensor that utilizes the multi-color confocal method. Due to coaxial measurement, it accurately separates the reflected light from the front and back surfaces of thin transparent films or coating films on glass, enabling stable, non-contact measurement of the height profile (warpage) of the target surface. The Quad processing system eliminates the effects of rough surfaces and microscopic unevenness, and optimizes and combines surfaces with different reflected light intensities, such as glass and mirror surfaces, for high-accuracy measurement. With a wide lineup of heads, including a long-range model with a reference distance of 150 mm and a measuring range of ±35 mm, and the ability to synchronize and measure up to 6 sensor heads with a single controller, it enables inline surface management of warpage (Bow/Warp) for large panels, cover glass, and wafers.

View Catalog

Click here for product information on the CL-3000 Series

Supporting Thickness and Thickness Distribution (TTV) Measurement — SI-F Series

Micro-head Spectral-interference Laser Displacement Meter

The SI-F Series is a laser displacement sensor that uses the spectral interference method. Light partially reflected by the reference surface inside the sensor head and light specularly reflected by the target that returns to the head interfere with each other, and this interference light is spectrally analyzed to calculate the distance to the target and its thickness. With ultra-high-accuracy measurement at a resolution of 1 nm, the flatness of transparent bodies and the thickness distribution (TTV) on surfaces can be captured with high resolution.

View Catalog

Click here for product information on the SI-F Series

Obtain Detailed Materials for the CL-3000 Series/SI-F Series

You can download a free catalog summarizing the specifications, measurement principles, system configuration, and application examples.

View Catalog

Inquiries regarding warpage and TTV measurement of glass substrates

Application Examples of Warpage and TTV Measurement for Glass Substrates and Transparent Bodies

These systems are used for warpage and TTV measurement of various transparent bodies, such as large glass panels and support glass.

Deflection and Height Measurement of Glass Substrates During Robot Transfer

Measure the height and warpage of glass during transfer with a robot arm to accurately capture deflection and position.

Simultaneous Measurement of Thickness and Warpage of Large Glass Panels

Simultaneously measure the thickness and warpage of large panels at multiple measurement points. Non-contact measurement allows for stable inspection within the manufacturing process.

Glass Thickness and Warpage Measurement

By installing sensor heads at the four corners and center of the target and simultaneously performing non-contact measurement and calculation of the distances to the front and back surfaces of the glass, thickness and warpage are calculated instantaneously.

Height and Thickness Measurement of Support Glass

Measure the height and thickness when bonding glass and wafers. Combined with a stage, the thickness distribution (TTV) is also managed.

Frequently Asked Questions About Warpage and TTV Measurement of Glass Substrates (CL-3000 Series/SI-F Series)

Q Can the warpage of transparent glass substrates be measured without contact?

A

Yes, it can. The CL-3000 Series uses a coaxial multi-color confocal method to separate the specular reflection light from the front and back surfaces, stably measuring the height shape (warpage) of the target surface without contact.

Q What is the difference between warpage and TTV, and which product is used to measure them?

A

Warpage (Bow/Warp) is the waviness of the height shape on one side, while TTV is the thickness variation within the surface (the difference between the maximum and minimum thickness values). The CL-3000 Series is mainly responsible for warpage, and the SI-F Series is mainly responsible for thickness and TTV, which are selected according to the installation distance and required accuracy.

Q How does it differ from the moire (grating projection) method or contact method?

A

The moire method is prone to errors in height conversion, and contact methods/CMMs involve stopping and scratching due to point measurement. The CL-3000 Series/SI-F Series can separate the front and back of transparent bodies without contact, allowing warpage and TTV to be managed on a surface basis.

Q Can measurement be performed through a case or glass?

A

Yes, it can. A long-range model supports specular reflection measurement from a distance, such as through a case or glass, with a wide range of 150 mm reference distance and ±35 mm measurement range.

Q Can all warpage and TTV be managed inline?

A

This is possible. Surface data can be acquired through multiple points, multiple heads, or scanning, and warpage and TTV can be recorded inline to be used for 100% quality control.

Q Please feel free to contact us regarding any challenges with glass substrate warpage and TTV measurement.

A

Measurement methods, installation configurations, and specifications can be confirmed in the catalog or via the inquiry form.

Related Products