Laser Marking Systems / Laser Markers
- Laser Etching vs Laser Engraving: Which to Choose?
- How Does Laser Cleaning Work?
- What Materials Can Be Marked with a UV Laser Machine?
- EV Laser Marking Applications
- Comparison of Different Types of Electric Vehicle Battery Cells
- Difference Between UV Laser and Fiber Laser Engraving Machines
- How to Choose the Right Laser Marker for Engraving
Laser Etching
Laser etching machines are revolutionary tools that open up amazing possibilities in creating, crafting, and even manufacturing objects with highly intricate and detailed designs. By harnessing the power of laser technology, many industries are transforming a wide variety of materials, ranging from organic products like wood to metals, into breathtaking pieces of art or useful industrial products.
In the following, we will learn about laser etching machines, the materials used, and the types of laser etching solutions KEYENCE provides to help improve processes.
What is Laser Etching
Laser etching is a process of using a laser to remove material from a surface by running the laser beam along the desired path, the workpiece is etched in the desired pattern. The etching depth and type of marking can also be controlled by changing the laser parameters. It can be used for a variety of purposes, including engraving, cutting, and marking. Laser etching is a very precise process, and it can be used to create detailed designs or patterns on a wide range of materials, including glass, wood, metal, and plastic.
Laser etching is becoming increasingly popular for a number of reasons. First, it is a very efficient and cost-effective way to produce high-quality results. In addition, laser etched designs are highly resistant to wear and tear, making them ideal for products that will be used frequently.
Laser Etching Process
During the laser etching process, the laser beam melts the material, vaporizing it or evaporating it, and then the material is blown away by a stream of gas. The process is quick and precise, making it ideal for creating high-quality marks on products.
To create a laser etched product, the first step is to create a design. This can be done using software such as Adobe Illustrator or Photoshop. Once the design is complete, it is saved as a vector file. This file is then imported into the laser etching machine. The machine will read the file and follow the vectors to create the desired shape or design.
The next step is to select the material that will be used for the project. This can be anything from wood to metal to glass. Once the material is selected, it is placed in the machine and secured in place. Then, the machine settings are adjusted according to the type of material being used and the desired results.
Finally, the laser is turned on and directed at the material. The beam will etch the material, following the path of the vector file. As the laser moves over the material, it will gently remove small amounts of material, creating text, images, or patterns on the surface. Laser etching is a quick and easy way to create high-quality products with a unique look.
Laser Etching Machine
A laser etching machine is the force and brains behind the process. These machines are widely used in manufacturing and throughout many of the top industries. Although a laser etching machine can be manufactured with different options and features, some have a few key benefits over others.
KEYENCE offers a variety of laser etching machines that can be used to improve processes and create designs or patterns on a variety of materials. Our laser etching machines are available in numerous sizes, wavelengths, and power levels to meet the needs of any business or application. We are dedicated to supplying laser etching machines that are easy to use and offer a variety of features to meet the needs of any business.
KEYENCE’s laser etching machines and laser marking systems are not only innovative but reliable, bringing you the latest in marking technology. Contact us today to learn more about laser etching equipment and how it can improve your operations.
Related Downloads

2D codes have become a near-universal standard for traceability. This must-read document covers everything from code scanning principles, laser installation, predictive maintenance, and more.

Some laser marking applications require integration with multiple devices. KEYENCE provides a total marking solution, from X/Y stages and indexing systems to head traversal systems. Learn more in this brochure.
Related Products
Application
Industries
Resources
- Laser Etching vs Laser Engraving: Which to Choose?
- How Does Laser Cleaning Work?
- What Materials Can Be Marked with a UV Laser Machine?
- EV Laser Marking Applications
- Comparison of Different Types of Electric Vehicle Battery Cells
- Difference Between UV Laser and Fiber Laser Engraving Machines
- How to Choose the Right Laser Marker for Engraving