RPA (Robotic Process Automation)
Taiheiyo Club Corporation
RK has enabled the automation of even technically complex tasks. This has allowed us to achieve a reduction of approximately 1,000 hours of work annually!
Taiheiyo Club Inc. introduced KEYENCE's RK, a user-friendly and highly accurate RPA (Robotic Process Automation) tool, seeking a solution accessible to anyone. Just one year after implementation, we realized an annual work reduction of about 1,000 hours. To share insights on the background, effects, and the appeal of RK as a tool, we interviewed Mr. Sugita, Executive Officer and Head of the Management Control Division, and Mr. Sato, Head of the Business Planning Department, who were deeply involved in the RK deployment.
About the Company
Taiheiyo Club Corporation
Taiheiyo Club Inc. operates one of the world's largest "shared membership clubs," with approximately 19,000 members. They manage 19 golf courses nationwide. In addition to hosting domestic tours like the "Sumitomo Mitsui VISA Taiheiyo Masters" and the "Japan Professional Golf Championship," they also hold international tournaments such as the World Cup and the Asia-Pacific Amateur Championship. They conduct over 200 competitions annually and run golf academies at five locations, significantly contributing to the promotion of golf.
We’re here to provide you with more details.
Reach out today!
The Dedicated PC for RK, Named "Bryson," Has Enabled About 20 Automation Processes
Please Tell Us About Your Use of RK
Our company introduced RK in February 2024 and has been utilizing it for about a year. We have one creator license. During the day, we develop scenarios (automation programs), and from 9 PM to 8 AM, we run these scenarios, switching usage based on time zones. Interestingly, the PC dedicated to running RK has been affectionately named "Bryson," after the strategic-minded pro golfer Bryson DeChambeau. Internally, it has become common to say "Let Bryson handle it" when referring to running scenarios (automated workflows within RK).
Currently, about 20 scenarios are operated by Bryson. Here are some main examples:
- Scenario Examples
-
- Sales Report Generation: Extract and aggregate sales data for each course from the core system overnight, compile the data into Excel, and send it to management by 7 AM each morning.
- Cancellation Data Preparation: Extract cancellation data from the core system, calculate a unique "index" for cancellations using our proprietary method, and send this information to the department that consolidates golf course data nationwide.
- Customer Data Management: When customer data in the core system is updated, download the data and update the customer information in a separate system called Kintone.
In this way, Bryson excels at handling daily routine tasks and system integrations.
Expectations for Development Without Programming Knowledge
Please Tell Us About the Background of RK's Adoption
Our operations include several tasks that must be performed daily without fail. Among them, the task of compiling data early every morning, like example 1, was quite burdensome for staff members. We were interested in automating with RPA and tried several solutions. However, the RPA tools we used before were difficult to operate and required experts for scenario development. Our Business Planning Department manages various systems, including 19 core systems, accounting, attendance, and network infrastructure, and with only two staff members there was no room to add this kind of RPA development to the workload. Ultimately, we concluded that implementing RPA with our current team was challenging.
However, at that time, our parent company Maruhan suggested, "Why not try RK?" After a brief pilot period, we found it to be a very capable tool. We thought that not only the Business Planning Department but also employees in other departments could create scenarios on their own. This led us to commit to adopting RK.
What Were the Key Factors That Encouraged You to Proceed With the Implementation?
The main point was that even people with little to no programming knowledge could develop scenarios easily through a simple UI. We believed this would reduce the burden on both the Business Planning Department and other departments when creating scenarios. Additionally, we checked the accuracy of button recognition. After testing, we confirmed that RK accurately recognizes buttons not only through image recognition but also via element recognition, which reassured us that as long as the UI of the system doesn't change, RK will continue to perform reliably.
Over 1,000 Hours of Annual Work Reduction and Benefits for More Than One Person
Please Tell Us About the Effects of the Implementation
We achieved a reduction of approximately 1,033 hours annually. Calculated at $14 per hour, this amounts to about $14.5k. This is cheaper than hiring an additional part-time staff member. As we plan to add more scenarios, these benefits are expected to grow further.
Another significant benefit is the reduction in system development costs. For example, consolidating and outputting reports from core systems previously required $7k to $14k in vendor development costs. With RK, we can do this task in-house, which means even greater cost savings than the numbers above suggest.
High Functionality and the Ability to Quickly Resolve Complex Tasks
Please Share What You Found Most Valuable About RK After About a Year of Use
There are three main points:
- Versatility, including executing SQL commands: RK can run SQL commands via command line. For tasks like extracting reservation data for each course, directly pulling raw data from the core system using SQL is faster. Currently, about 4-5 of the roughly 20 scenarios utilize SQL for data retrieval.
- Automating complex tasks in a short time: For irregular tasks like submitting reports covering the past year, RK has been very useful. By creating a scenario that can dynamically use the date of execution, the RK is able to complete the task at any time. Once familiar, creating this kind of scenario takes about an hour. Once completed, scenarios can be stored as assets for future reuse, enabling faster execution of similar tasks.
- Performing error-free work during early mornings and late nights: RK works 24/7 without mistakes or complaints. It handles data entry flawlessly, like a highly reliable assistant working early mornings, allowing us to focus on other priorities.
Support That Exceeds Expectations
Please Describe Your Experience With RK’s Support
The support team is impressively intelligent. When we ask questions, they don’t just give straightforward answers but also suggest ways to reuse components across scenarios, helping us develop more versatile solutions. They always respond with information beyond the questions we send. Additionally, both the support team and sales staff are quick to reply—unlike typical vendors that may take a day or two to respond or require weeks for investigations. This responsiveness makes it easy for us to consult with KEYENCE freely.
Desire to Expand Automation to Other Golf Course Sites As Well
Do You Think RK Can Be Recommended to Other Golf Course Operators?
Absolutely. Even companies managing fewer courses than ours can benefit. There are still many areas in golf course management that can be digitized. Since golf service is customer-focused, accuracy is crucial. Using RK eliminates mistakes and frees up time, ultimately leading to better service. In this sense, effectively leveraging systems like RK will become increasingly important.
Future Plans for RK
We believe there are many more tasks that can be automated. Our plan is to gather ideas and expand scenarios accordingly. We also want to increase RK’s use not only at the headquarters but also at each course site. Our goal is to make everyone’s work easier through automation.
To achieve this, we want to train more staff within the company to use RK. As part of this effort, we leave comments on each command in scenarios so that others can understand what automation is being performed, even if they are not familiar with programming. We hope KEYENCE will offer seminars, training sessions, and videos to help spread RK internally—ideally with beginner-friendly themes like "Introduction to RK" for employees who are not as skilled with computers.
Contact us to learn more about how our advanced technology can help take your business to the next level.
Contact Us
Related Products
Scroll