Application Solutions

Outer Diameter

Finding The Right Solution for Outer Diameter Measurements

When looking for the best way to measure outer diameter, there are a number of important factors to consider, including the shape of the target, the type of measurement system, and the installation environment. Selecting equipment that doesn't adequately meet your needs can lead to insufficient precision and increased man-hours during production, so choosing the right equipment is important. This site is designed to help you discover the best way to perform outer diameter measurements with confidence.

How to Measure Outer Diameter

Find the best measurement method and the right equipment to measure "Outer Diameter".

Measurement of outer diameter at one location on a thin target

Example Application: Outer diameter measurement of high-speed wires

Optimal measurement system

Optimal measurement systemThrubeam Optical Micrometer

The target is passed through a beam of collimated light to measure the size of its shadow.

A
Receiver
B
Measurement target
C
Transmitter
D
Focal distance
KEY POINTS
  • Outer diameter can be measured to high precision by selecting the measurement system best suited to the target diameter.
  • A faster sampling cycle ensures stable measurement even if there is target run-out.
  • 1D Telecentric Optical Method.
    Long service life design that is free of moving parts.
    Fastest sampling rate in its class at 16 kHz.

    LS Series

    View Catalog

Measurement of outer diameter at multiple locations on a thin target

Example Application: Outer diameter measurement of injectors at multiple points

Optimal measurement system

Optimal measurement system2D Thrubeam Optical Micrometer

The 2D optical projection method makes it possible to measure the outer diameter of multiple points as well as the minimum/maximum values over specified ranges.

KEY POINTS

Even if the target is tilted, outer diameter can be measured accurately by utilizing the position correction function.

  • 2D Telecentric Optical Method. Simultaneous measurement of up to 100 with calibrated high-speed measurement.

    TM-X Series

    View Catalog

Measurement of outer diameter on thick targets

Example Application: Outer diameter measurement of large steel pipes

Optimal measurement system

Optimal measurement systemThrubeam Optical Micrometer

Outer diameter is measured by placing a target between two sensor heads.

KEY POINTS

Parallel alignment of the sensor heads is important to prevent values from changing if the target moves to the left or right.

  • 1D Telecentric Optical Method.
    Long service life design that is free of moving parts.
    Fastest sampling rate in its class at 16 kHz.

    LS Series

    View Catalog

INDEX