Recent Searches
    Series ( results)
      Models ( results)
        Keywords
          1. Home
          2. Microscope Glossary
          3. Coaxial illumination

          Coaxial illumination

          OPTICAL ILLUMINATION TECHNIQUE
          - COAXIAL LIGHTING

          Viewing highly-reflective objects with flat surfaces, such as ICs and cross-sectioned samples, is typically difficult to accomplish using ring illumination. When light hits the surface, most of it will reflect away from the lens and result in a dark image. Instead, coaxial (brightfield) illumination is used to view these targets and produce a bright image. Generally, this type of lighting makes use of a half-mirror to match the optical axes of the illumination and lens.

          Back to top

          KEYENCE CORPORATION OF AMERICA 500 Park Boulevard, Suite 200, Itasca,
          IL 60143, U.S.A.
          Phone: 1-888-KEYENCE [1-888-539-3623]
          E-mail: tech@keyence.com
          Career Opportunities: KEYENCE Career Site